Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Can you put a 2 pin fan Hedder on the rasberry Pi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 703 subscribers
  • Views 676 views
  • Users 0 members are here
  • raspberry
  • raspberry_pi
  • raspberrypi
Related

Can you put a 2 pin fan Hedder on the rasberry Pi?

e14 Contributor
e14 Contributor over 13 years ago

hi sence im a VERY carefull person i was going to put a small computer fan inside my rasbery pi case to get some air moving arround and

i was wondering where you would mount one and if you even can mount one on to the bourd

 

(pictures and or digrams would be very helpful)

 

thanks!

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 13 years ago

    Most RasPi users don't need a fan.  There was a thermal issue with the 1.0 PC board which caused the USB/Ethernet chip to get very hot on some boards, but that's been fixed on the 2.0 PC board (the one with the alignment/mounting holes).

     

    You can find lots of discussion about fans at raspberrypi.org.  Enter "fan" in the Google search box on the home page.

     

    I have a RasPi 1.0 and I have found that mounting her vertically is a great way to keep her cool.  That way there's natural air flow (hot air rises) across both sides of the board.  There's a lot of heat conducted to the back side of the board, so if there's no air flow the back side gets warm.  Here are some photos: http://www.element14.com/community/thread/19162?start=16.  If the Broadcom SoC or USB/Ethernet chip are still getting hot, adding heat sinks is a good way to cool them down provided there's some natural air flow.  But that's usually only needed if RasPi is in an environment that's already warm or if you're overclocking and/or overvolting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi friend,

    I read many reviews about the temperature of the various chips of RPI, and in conclusion, I understand that there is no danger that can be damaged by heat, unless it is extreme (over ~75 ºC).

    But I decided to help my RPI to have "long life" and not take risks.

    I placed a fan as this: http://goo.gl/qUNQM

    The photos on the following links:

    http://goo.gl/fNZRJ

    http://goo.gl/VUM5E

    http://goo.gl/QAvSj

    http://goo.gl/I0z2Z

    http://goo.gl/1rD8B

     

    The results:

    Working temperature WITHOUT fan: 55ºC (131 ºF)

    Working temperature WITH fan: 34.2°C (93.5°F)

     

    I can monitor the temperature through SNMP:

    image

     

    Take your own conclusions please.

    Best Regards,

    Marcelo

     

     

    Argentinian RPi G+ Community

    http://goo.gl/vG0Ke