Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Utilization of re-purposed overhead LCD display modules from Ford WinStar, Freestar Vans etc
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 705 subscribers
  • Views 1750 views
  • Users 0 members are here
  • lcd
  • video
  • sharp
  • cheap
  • NTSC
  • raspberry_pi
  • display
Related

Utilization of re-purposed overhead LCD display modules from Ford WinStar, Freestar Vans etc

e14 Contributor
e14 Contributor over 13 years ago

The origin of this re-purposing post is CANADA and applies to the U.S.A. as well.


 

I discovered an overhead LCD cache of parts at the local U-Pull-It Automobile Junk Yard today

that can be re-purposed as a RPi COLOR LCD TN display.

 

While looking for a rear hatch replacement for my rusted out one, I happened to notice the vast numbers

of luxury type Ford Vans with AUTOVISION VCP Rear Seat Entertainment System .

 

The systems were implemented by Johnson controls in year 2000 and later models in a SHARP LCD 6.4 display

which had a TN LCD with 130 degree limited view filter and special polarization against Sunlight wash-out.

 

With the removal of just two phillips screws, the entire asembly drops down revealing just five wire connection

from any Ford Winstar/Freestar type vehicle although I noticed the feature in the WinStar Vans from 2000-2003 which are

now appearing in great quantities at these Auto-graveyards.

 

Only 5 wires of 20AWG stranded are in the harness!

Red = +12,

Black = Return,

Silvered = Signal Ground,

GREEN = NTSC 1V Video composite Input,

Blue: assumed to be a diming input with Headlamps active, but grounded to the Silvered connection.

 

Wow, this display can be obtained by paying a very low fee to the Scrap Yard keeper.

I do not expect yards to charge more than $20 

 

      The LCD is a Sharp LQ064A5CG01 and I found a technical manual from the Ford forum and here is the link

     which is still active (March 2013)

http://document.sharpsma.com/files/LQ064A5CG01_SP_041499.pdf

 

actual pinouts on the LCD (not the five wire):

1 wht DMO -o- voltage output for dimmer (note 5-1)

2 yel DM1 -i- return signal for dimmer (note 5-2)

3 blk HRVR -i- turns direction of horizontal and vertical scanning (note 5-3)

4 pnk VIN -i- voltage in 9-16v DC typical 13.8v 850ma bl/on 220ma bl/off

5 blk GND - Power Ground

6 grn VBS -i- Composite video signal (NTSC) 75ohm

7 blu GND - Signal GND

8 n/c BRT -i- Brightness adjusting terminal 0- 5v (note 5-4)

9 n/c TEST -i- generally, when using, connect to DM0 (note 5-5)

10 clr GND - Frame GND

 

Notes for above list

5-1 voltage output is 5.3v

5-2 backlight dimming 0 to 800kohms

5-3 low signal is normal high reverse video both vertically and horizontally

low is 0-1.5 hi is 3.5-5volts

5-4 brightness adjusted by voltage on this pin

5-5 when connected to ground, backlight is always on regardless of input signal (otherwise baclight is off with no signal)

 

spec

6.4" color LCD with 112,320 pixels

1440(480rgb)horiz by 234 vert .09 dph .417v mm rgb stripe configuration

viewing angle: 130 deg. horiz and 105 deg. vertical

100:1 contrast ratio

SHARP Color tft-lcd active matrix

SHARP Part LQ064A5CG01

controls: Brightness Pot 800K 270deg turn


I used the Red/Black for power,

Green for composite video,

and spliced the Blue/clear/Black shield for video ground.

Very Simple: I guessed this before I came across the Spec's and TFT Manual

The Video Cassette player was a unit between the seats

but because the windows are smashed and snow and rain just sit on the flying heads

the VCPlaye is ruined- just leave it-it is not worth recovery;

there is an interesting rear seat media control at the rear of the front center arm rest

but again, the controls I examined were smokey and dirty and not worth recovery...

 

The results (from two recovered, re-purposed) "rear seat entertainment system overhead 6.4" LCD's"

in pictorial essay

 

AutoVision shown in its case, with ceiling cavity removed:

image

DC power supply detail from the bench

12V power (from around 8.3 up to 16.0 but I wont go higher than that)

Brightness Pot was set at about 50%

down to 0 = about 250mA @ 12.0V

up to MAX bright = 730mA @ 12.0V

image

 

Raspberry Pi in booting up although the font is (admittedly) small

mostly readable but in color (for fruity low cost),

image

the second module stripped naked (!electronics porn!) of its shell

showing 5 wire harness ruthlessly ripped from the dead Luxury Van,

wires tortured and cut with a dull flat blade screwdriver

[yes I forgot my side cutters and the FORD section was some 1/2mile into the compound]

image

face side up on the Sharp LCD



image

 

Enjoy.

 

(1) Find a Pull-it-Yard

(2) wear sensible Work Boots with Steel Toes and Heel Sheath and comfortable gloves

(3) take Cross-Philips-Screwdriver(s) and Side-Cutter or knife

(4) Locate sad looking Van with most of its guts pulled out

 

and you are looking for this display on the rear seat roof facing rearwards

image

 

(5) Undo two cross-philips screws, pull down from rear, cut 5wires past harness connector

(6) pay for it (my yard classed this as RADIO-with CD because the Keeper recognized its high value)

(7) get it home to lab and clean it off (mine had years of Tobacco smog coated to every pore)

(8) wire it up and enjoy

 

Enhancements

I connectorized my project with coaxial 2.1mm for 12V Power

and

RCA for NTSC 1V Video input

 

Photo example of the U-pull yard I like to go to (showing Imports section I think) ;

Cars are propped up on old rims; sharps bits and broken glass everywhere,

take care please, use appropriate foot , eye, and hand protection.

image

 

Johnny (in Canada)

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    The link for the Sharp module is broken,

    I just searched for another one in Russia somewhere

     

    http://www.gaw.ru/pdf/Sharp/LQ064A5CG01.pdf

    or any search of "LQ064A5CG01.pdf"

     

    Johnny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    A Fry's store last week had a bunch of refurb 'Sylvania' 7-inch car dual-headrest LCD DVD player with integrated monitor and a separate monitor, and the separate monitor works well with PAL composite (so I guess it auto-detects and possibly works with NTSC too - I have not tried). I used it for an alternate purpose, but I suspect it works with the Rasp-Pi too. The cost was just over $60 from memory, so cheap, but not anywhere as near as low cost as you have managed to find. There are some of these models on ebay too. So, if you want a DVD player but don't need the second LCD, then you could retask it for any composite video purpose.

    Most of these small composite LCD monitors only have a few hundred lines resolution, so it's not ideal for text, but very ideal if you just intend to display video/animations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    I admit that 480x234 or less will not suffice for command line environments

    but the price was so very low for both monitors, that it was hard to resist in that moment.

     

    I suspect your Fry's LCD TFT aftermarket is 480x234 but with good contrast ratio and filter

     

    I found another u-pull-it yard, out of town by 1 hour,

    that charges $10 for "Radio with CD or any Rear Entertainment device".

    with MANY Freestars and Winstar LX's all propped up on wheelrims

    I suspect that all of this era LCD's are the same low resolution


    You bring up a good point that the RPi boot text is not readable.


    For the money, I found 9 more Ford/JohnsonControls screens

    but I hestitate to pull them because of lower resolution, despite the low prices.


    I am going to start looking for better resolutions on Automotive LCD

    but 480x234 is a re-occuring theme on the 2000-2004 era soccer mom vehicles

    in our throw-away society auto graveyards

     

    the target price (for this thread) would be $40 ? max for an LCD TFT

    pull capable of 720i/p in Sunlight (1280x720 or similar even if the color depth is only 8bit).

    this could be reasonable in 2015; all the current DIN size dashboard screens are 7-9" and

    720p capable, with "reverse gear NTSC and PAL auto-sensed" for the reversing camera option


    The search terms would be

    1280 and TFT and overhead or headrest,

    which are now in the $200-300 China aftermarket and mostly 9 to 14" in diagonal size

     

    so I appeal to all seasoned Electronics Technicians and Engineers to post repurposing LCD  "finds" here

    12V

    1280x720 or 720p/i,  

    TFT and overhead or headrest,

    and 7inch diagonal and up

    with NTSC

    for use with RPi

     

    remember the Sinclair Z80's , TRS80's and CBM machines;

    there was no 'electronic scrap' then.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    I admit that 480x234 or less will not suffice for command line environments

    but the price was so very low for both monitors, that it was hard to resist in that moment.

     

    I suspect your Fry's LCD TFT aftermarket is 480x234 but with good contrast ratio and filter

     

    I found another u-pull-it yard, out of town by 1 hour,

    that charges $10 for "Radio with CD or any Rear Entertainment device".

    with MANY Freestars and Winstar LX's all propped up on wheelrims

    I suspect that all of this era LCD's are the same low resolution


    You bring up a good point that the RPi boot text is not readable.


    For the money, I found 9 more Ford/JohnsonControls screens

    but I hestitate to pull them because of lower resolution, despite the low prices.


    I am going to start looking for better resolutions on Automotive LCD

    but 480x234 is a re-occuring theme on the 2000-2004 era soccer mom vehicles

    in our throw-away society auto graveyards

     

    the target price (for this thread) would be $40 ? max for an LCD TFT

    pull capable of 720i/p in Sunlight (1280x720 or similar even if the color depth is only 8bit).

    this could be reasonable in 2015; all the current DIN size dashboard screens are 7-9" and

    720p capable, with "reverse gear NTSC and PAL auto-sensed" for the reversing camera option


    The search terms would be

    1280 and TFT and overhead or headrest,

    which are now in the $200-300 China aftermarket and mostly 9 to 14" in diagonal size

     

    so I appeal to all seasoned Electronics Technicians and Engineers to post repurposing LCD  "finds" here

    12V

    1280x720 or 720p/i,  

    TFT and overhead or headrest,

    and 7inch diagonal and up

    with NTSC

    for use with RPi

     

    remember the Sinclair Z80's , TRS80's and CBM machines;

    there was no 'electronic scrap' then.