Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi Model A usage scenarios
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 709 subscribers
  • Views 1023 views
  • Users 0 members are here
Related

RPi Model A usage scenarios

e14 Contributor
e14 Contributor over 13 years ago

What are the anticipated Model A usage scenarios, given the single USB port

and no ethernet port?

 

Are there any keyboards with an embedded hub for a mouse that are known to work?

 

Would a PS/2 keyboard/mouse splitter cable with USB adapter work better?

 

If the single USB port is used for a WiFi dongle, can the Model A be used

headless over ssh?   How would you set the WiFi SSID/password?

 

An attempt by Simon on the RPi forum to ask these questions got locked for concern trolling.

Even adding smilies didn't prevent shooting the messenger.

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=24&t=39463

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi Coder27,

     

    RaspberryPi is probably an ideal platform for robotics and you don't really need an ethernet port for that. So Model A is just fine and totally wins here.

     

    For kids/teachers you mentioned in your post at RaspberryPi forums, I suppose the $35 version (B) is the way to go.

     

    More usages for Model A:

    1. http://www.southgatearc.org/news/march2013/turning_the_raspberry_pi_into_an_fm_transmitter.htm

    2. http://m0xpd.blogspot.co.uk/2013/01/raspberry-whispers.html

    3. small ftp/http server accessible via WiFi (data stored on SD card)

    4. home automation (via GPIO) with control via WiFi

    5. information desk display

    lots more....

     

    If you can't find usage for Model A - it's probably not for you (smile)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago

    Hi coder27,

    I'm not aware of many scenarios (except maybe simple data logging type stuff) that require the 1-USB port but no IP connectivity.

    Personally I always expect either a serial port, or IP connectivity on a development board (USB is not so useful to me unless it is one of those

    FTDI things, but even then I sometimes prefer 3.3V levels out of the board, because then I can interface to anything, not just devices with

    FTDI drivers.

    My home keyboard is a Sun (now Oracle) one which has a built-in hub, but it is slow USB not high speed,

    which is fine for a mouse, but I've not tried it with Rasp-Pi. I could try it if you'd like me to. I've only used Ethernet and serial

    on the original Rasp-Pi board (I don't have a model A) after initial config. The keyboard not cheap though, about $50+postage

    according to Oracle's website. The quality is ok.

    I suppose someone could adapt the firmware to read WiFi details from the SD card, but I think it may be hard to cater for all dongles,

    It all sounds messy, so probably configuring via serial port is easiest, but it does require a level converter board to get it into your PC of course.

    As an idea, someone could make device (from a Rasp-Pi, but cheaper still could be any simple AVR micro) that could be used to configure

    all other Model A's in the classroom. Basically it would be coded to log into the model A's via serial (no need for level converter since it is 3.3V to 3.3V levels) and configure the device and then issue shutdown. It could even be powered from the same supply. Then one could unplug, and move on to

    the next one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago

    Model A should work nicely with a Motorola Atrix Lapdock, which has an internal hub for its keyboard and mouse.  You can plug an Ethernet or WiFi dongle into one of the two Lapdock A ports.  The only problem with this scenario is that Model A only has 256MB RAM vs Model B's 512MB.  But then, maybe the Model A is only using up a supply of pre-ordered 256MB chips and once they're gone you'll be seeing 512MB Model As.  With RasPi, you never know and it's always a surprise -- part of the fun, I guess. image

     

    A big advantage of Model A is much lower power consumption, since the LAN9512 uses a lot of power on a board with linear regulators.  So if you've got a stand-alone embedded appliction that needs fairly low power, Model A is a much better bet.  That said, neither board is an ultra-low power board like some of the ARM Cortex-M0/0+/3/4 boards.  But it's pretty low power for a GNU/Linux board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago

    A wireless keyboard/mouse combo is another solution. The single USB port is a fairly serious limitation to me and so pretty much requires

    a hub. This is really not a big deal but it does add to the cost. I agree with John that stand alone applications is probably what it will do

    best.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    > A wireless keyboard/mouse combo is another solution

     

    Good point.  Even better would be a combination Bluetooth/WiFi dongle.

    I notice that this has already been tried on the Model B:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?t=27678&p=314994

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago

    I'm waiting to test it for couple of application where the Rpi will be headless and probably just with a WiFi dongle for remote access via ssh and/or tightvnc.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    I have this: Wireless Mouse/Keyboard combo...

     

    http://www.jaycar.com.au/productView.asp?ID=XC5174

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I've turned a Model A Raspberry Pi into a Piratebox using instructions at http://piratebox.aod-rpg.de/dokuwiki/doku.php?id=raspberry . Have a Dlink DWA-125 plugged into the only USB port.  Works a treat!.