Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi Model A usage scenarios
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 709 subscribers
  • Views 1030 views
  • Users 0 members are here
Related

RPi Model A usage scenarios

e14 Contributor
e14 Contributor over 13 years ago

What are the anticipated Model A usage scenarios, given the single USB port

and no ethernet port?

 

Are there any keyboards with an embedded hub for a mouse that are known to work?

 

Would a PS/2 keyboard/mouse splitter cable with USB adapter work better?

 

If the single USB port is used for a WiFi dongle, can the Model A be used

headless over ssh?   How would you set the WiFi SSID/password?

 

An attempt by Simon on the RPi forum to ask these questions got locked for concern trolling.

Even adding smilies didn't prevent shooting the messenger.

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=24&t=39463

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 13 years ago

    Hi coder27,

    I'm not aware of many scenarios (except maybe simple data logging type stuff) that require the 1-USB port but no IP connectivity.

    Personally I always expect either a serial port, or IP connectivity on a development board (USB is not so useful to me unless it is one of those

    FTDI things, but even then I sometimes prefer 3.3V levels out of the board, because then I can interface to anything, not just devices with

    FTDI drivers.

    My home keyboard is a Sun (now Oracle) one which has a built-in hub, but it is slow USB not high speed,

    which is fine for a mouse, but I've not tried it with Rasp-Pi. I could try it if you'd like me to. I've only used Ethernet and serial

    on the original Rasp-Pi board (I don't have a model A) after initial config. The keyboard not cheap though, about $50+postage

    according to Oracle's website. The quality is ok.

    I suppose someone could adapt the firmware to read WiFi details from the SD card, but I think it may be hard to cater for all dongles,

    It all sounds messy, so probably configuring via serial port is easiest, but it does require a level converter board to get it into your PC of course.

    As an idea, someone could make device (from a Rasp-Pi, but cheaper still could be any simple AVR micro) that could be used to configure

    all other Model A's in the classroom. Basically it would be coded to log into the model A's via serial (no need for level converter since it is 3.3V to 3.3V levels) and configure the device and then issue shutdown. It could even be powered from the same supply. Then one could unplug, and move on to

    the next one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago

    Hi coder27,

    I'm not aware of many scenarios (except maybe simple data logging type stuff) that require the 1-USB port but no IP connectivity.

    Personally I always expect either a serial port, or IP connectivity on a development board (USB is not so useful to me unless it is one of those

    FTDI things, but even then I sometimes prefer 3.3V levels out of the board, because then I can interface to anything, not just devices with

    FTDI drivers.

    My home keyboard is a Sun (now Oracle) one which has a built-in hub, but it is slow USB not high speed,

    which is fine for a mouse, but I've not tried it with Rasp-Pi. I could try it if you'd like me to. I've only used Ethernet and serial

    on the original Rasp-Pi board (I don't have a model A) after initial config. The keyboard not cheap though, about $50+postage

    according to Oracle's website. The quality is ok.

    I suppose someone could adapt the firmware to read WiFi details from the SD card, but I think it may be hard to cater for all dongles,

    It all sounds messy, so probably configuring via serial port is easiest, but it does require a level converter board to get it into your PC of course.

    As an idea, someone could make device (from a Rasp-Pi, but cheaper still could be any simple AVR micro) that could be used to configure

    all other Model A's in the classroom. Basically it would be coded to log into the model A's via serial (no need for level converter since it is 3.3V to 3.3V levels) and configure the device and then issue shutdown. It could even be powered from the same supply. Then one could unplug, and move on to

    the next one.