Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54260 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    Spring greetings to you all ...  this thread has brought me out of my forum sabatical, naughty naughty. image

     

    Seeing the Slashdot thread on BeagleBone Black made me warp over to here post haste, as I guessed you would all be talking about it ... and you were, hehe.  I agree with everything that's been said.

     

    Two additional bits of information that slightly change the picture:

     

    • Farnell UK says "18584 will be available for delivery on 3 May, 2013", so they're clearly taking this seriously and expect BB Black to sell in much higher volumes than the first BeagleBone.  No surprise of course, price is king.

     

    • The BeagleBone's TI Sitara AM3359 contains a pair of integer-only realtime processors running at 200MHz, the Programmable Realtime Unit Subsystem or "PRU".  These can provide waaaaaaay better hard realtime interfacing performance than any program running in Linux user-space, so for hardcore techies who aren't afraid of getting their hands dirty with some pretty simple assembler, the BeagleBone is lightyears ahead of the Pi in interfacing capability.

     

    Success has very little to do with engineering merit though, so I won't be making any guesses about how popular this new board will become.  However, for myself, the Pi Model B is now totally dead in the water since it lost its only advantage, which was price.

     

    Needless to say, BeagleBone Black is on my shopping list as soon as they're in stock. image

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Spring greetings to you all ...  this thread has brought me out of my forum sabatical, naughty naughty. image

     

    Was wondering where you'd been hiding recently image

    • Farnell UK says "18584 will be available for delivery on 3 May, 2013", so they're clearly taking this seriously and expect BB Black to sell in much higher volumes than the first BeagleBone.  No surprise of course, price is king.

     

    However after getting an 'in stock' notification from Newark (strange when I'm in the UK), Newark now show 0 in stock and more expected to ship on 28th June - no qty listed...

    So I'm not holding my breath just yet.

    Success has very little to do with engineering merit though, so I won't be making any guesses about how popular this new board will become.  However, for myself, the Pi Model B is now totally dead in the water since it lost its only advantage, which was price.

     

    I'd hoped to see something like this where the price difference (in the UK anyway) is approaching zero. Regardless of the merits of each device, it'll be interesting to see what happens next.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to gdstew

    Gary: Good, I'm glad to see that we both agree on the worthless contribution that fanbois make to technical discussion.  Let there be none here, for any board or device regardless of manufacturer.

     

    And that means being willing to point out the downsides and areas of improvement of everything we discuss, without fear of treading on irrelevant fanboi sensitivities.  Technology is technology, and discussing where it fails and suggesting how it can be improved is part of the engineering process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Is their 280 mA with or without USB (keyboard/mouse etc.) or Ethernet connections ? Is your 410 mA with or without USB or Ethernet connections ? I pull

    a fairly consistent 700 mA on mine with a full complement of I/O attached but given what the Pi was designed for and the major constraints used for that

    design (something people seem to lose track of or just plain ignore all the time) I don't have any problems with it using 3.5W. For one of the more mundane

    uses I have in mind for one of mine, a DNS/DHCP server, 3.5W would be about 30x less than doing it with a normal old "junk" PC. For the project I would

    probably use the BeagleBoard Black for (robot) the less power used the better.

     

    The previous argument about linear LDOs was simply that they were not the best solution (some even said they were a bad engineering solution which is silly)

    for  powering the Pi. There is some merit to the argument of using a switcher as far as allowing a wider selection of input voltages and efficiency goes however

    given the pricing and size contraints of what it was designed for (again) there really is not much choice. It would also have required either a multi-output

    switcher or the same number of LDOs (one for 3.3V and one for 1.8V) already on the Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    Is their 280 mA with or without USB (keyboard/mouse etc.) or Ethernet connections ? Is your 410 mA with or without USB or Ethernet connections ? I pull

     

    The SRM says their figures are with HDMI monitor, usb hub, 4G thumb drive, ethernet @100Mb, serial debug cable. I basically have Pi, ethernet, sdcard, max3232 and a few temperature sensors, no usb devices for 410mA. So a reasonably similar setup.

     

    I'm about 310mA with the switchers and a GPS receiver for an NTP clock. As single purpose devices I don't tend to have much running on them - ntp isn't exactly processor intensive.

     

    So I'm waiting impatiently for my BBB to arrive so I can swap out a Pi and compare it in the same environment.

     

    The previous argument about linear LDOs was simply that they were not the best solution (some even said they were a bad engineering solution which is silly)

    for  powering the Pi. There is some merit to the argument of using a switcher as far as allowing a wider selection of input voltages and efficiency goes however

    given the pricing and size contraints of what it was designed for (again) there really is not much choice. It would also have required either a multi-output

    switcher or the same number of LDOs (one for 3.3V and one for 1.8V) already on the Pi.

     

    I really don't have a problem with the LDO's (and my switchers cost way too much to use on the Pi), I'm just interested in the different design compromises. Especially when the costs are so similar.

    Yes time and technology marches on, but it does make you wonder that if the BBB can use a composite pmic (with some switchers and some LDO's) while being so close in cost, could the Pi have done so too ?  Or if it couldn't a year or more ago, could it do so today..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Gary Stewart wrote:

     

    Is their 280 mA with or without USB (keyboard/mouse etc.) or Ethernet connections ? Is your 410 mA with or without USB or Ethernet connections ? I pull

     

    The SRM says their figures are with HDMI monitor, usb hub, 4G thumb drive, ethernet @100Mb, serial debug cable. I basically have Pi, ethernet, sdcard, max3232 and a few temperature sensors, no usb devices for 410mA. So a reasonably similar setup.

     

    I'm about 310mA with the switchers and a GPS receiver for an NTP clock. As single purpose devices I don't tend to have much running on them - ntp isn't exactly processor intensive.

     

    So I'm waiting impatiently for my BBB to arrive so I can swap out a Pi and compare it in the same environment.

     

    The previous argument about linear LDOs was simply that they were not the best solution (some even said they were a bad engineering solution which is silly)

    for  powering the Pi. There is some merit to the argument of using a switcher as far as allowing a wider selection of input voltages and efficiency goes however

    given the pricing and size contraints of what it was designed for (again) there really is not much choice. It would also have required either a multi-output

    switcher or the same number of LDOs (one for 3.3V and one for 1.8V) already on the Pi.

     

    I really don't have a problem with the LDO's (and my switchers cost way too much to use on the Pi), I'm just interested in the different design compromises. Especially when the costs are so similar.

    Yes time and technology marches on, but it does make you wonder that if the BBB can use a composite pmic (with some switchers and some LDO's) while being so close in cost, could the Pi have done so too ?  Or if it couldn't a year or more ago, could it do so today..

     

    Yes the prices are close. However one of the major design considerations for the Pi was the $35 price point which they achieved. I'm sure there are more than one or two things

    they would have preferred to do differently but that is how engineering works when rubber meets road. I know, I've been there a few times. Although there is a good degree of crossover

    in what they both do I still feel that they are fundamentally aimed at different markets. The Pi market is much more narrowly focused. The BB Black is much more general purpose. That

    probably accounts for most of the price difference. Personally I'm very excited about the BB Black.

     

    One of the nice things RPF did do recently was to double the memory for the same price. So there is room for improvements as technology advances. It will be interesting to see

    what happens to both of them (and others to come ?) over the next couple of years.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    s ork wrote:

    Did you catch the table in the BBB SRM showing power consumption ?   I was very interested in the Kernel Idling Display Blank figures of 280mA @ 5v, my Pi shows ~410mA in the same condition. So something is doing a better job.

     

    BBB, with external 5V supply using the barrel connector, max3232 serial adapter and 100Mb network, no capes, sdcard, or usb devices

     

    ~230mA with kernel idle and ondemand cpu governor, cpu running at 300Mhz. Switch to performance governor, cpu at 1GHz, and ~300mA.

     

    If anything, the figures from the SRM are worst case - I don't seem to be able to reach them without adding a good number of extras.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Maybe it's the PMIC doing an awesome job of being very efficient.  It's the same TPS65217C as used on the white BeagleBone, and the more I read about its capabilities, the more it's clear that it's quite a little star in its own right.

     

    I suspect that the kernel isn't clever enough yet to control it dynamically through I2C, but in principle a board that uses this PMIC could be run very frugally when not all its subsystems need to be powered at the same time, and some parts put on standby.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    I suspect there's several factors contributing to the better power figures. There does appear to be some communication between kernel and PMIC, as I saw a reference in some of the kernel docs that enabling pwm mode causes problems for ethernet (or was it usb, I forget) and it does appear to be used for the power button and shutdown.

    I'm sure things will improve, it's still quite early in it's lifetime..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I suspect there's several factors contributing to the better power figures. There does appear to be some communication between kernel and PMIC, as I saw a reference in some of the kernel docs that enabling pwm mode causes problems for ethernet (or was it usb, I forget) and it does appear to be used for the power button and shutdown.

    I'm sure things will improve, it's still quite early in it's lifetime..

     

    It is not clear from your description, were you using the BB Black as stand alone (using HDMI video) or tethered to a PC (not using HDMI video) ? If you were not that

    would explain some of the difference.

     

    Morgaine wrote:

     

    I suspect that the kernel isn't clever enough yet to control it dynamically through I2C, ...

     

    I'm quite sure that the kernel is clever enough since it has been handling power for years on notebooks, netbooks, smart phones, and more recently tablets. It has

    been using the motherboard version of I2C (SMB) for years too so no problems there either. Whether the people who ported the kernel were clever enough is another

    story but since both the Linux C and header files for using the TP65217 exits I assume they were.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    It is not clear from your description, were you using the BB Black as stand alone (using HDMI video) or tethered to a PC (not using HDMI video) ? If you were not that

    would explain some of the difference.

     

    I was quite clear about what I had plugged in. Specifically so that others could duplicate the test.  Yes there will be differences, but unless both you and I have exactly the same things plugged it then the numbers can't be compared anyway. Although the SRM gives some general idea of what was connected there isn't enough detail - was their usb hub powered or not, what was the precise make and model of the thumbdrive etc.

     

    So, for avoidance of doubt, here's some photos of what's connected along with the current reading. this is with the default angstrom build which uses the ondemand cpufreq scaling

     

    root@beaglebone:~# cat /proc/version

    Linux version 3.8.6 (koen@rrMBP) (gcc version 4.7.3 20130205 (prerelease) (Linaro GCC 4.7-2013.02-01) ) #1 SMP Sat Apr 13 09:10:52 CEST 2013

     

    root@beaglebone:~# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

    ondemand

     

    root@beaglebone:~# cat /proc/cpuinfo

    processor       : 0

    model name      : ARMv7 Processor rev 2 (v7l)

    BogoMIPS        : 297.40

    Features        : swp half thumb fastmult vfp edsp thumbee neon vfpv3 tls

    CPU implementer : 0x41

    CPU architecture: 7

    CPU variant     : 0x3

    CPU part        : 0xc08

    CPU revision    : 2

     

    Hardware        : Generic AM33XX (Flattened Device Tree)

    Revision        : 0000

    Serial          : 0000000000000000

     


     

     

    image

    image

    image

     

    Whether the people who ported the kernel were clever enough is another

    story but since both the Linux C and header files for using the TP65217 exits I assume they were.

    The driver exists and is in use, what it's capable of is a different question. From https://github.com/beagleboard/kernel/tree/3.9

    • PMIC: working
    • PMIC PWM: working, kills ethernet

     

    so it should be clear that some of the drivers are still a work-in-progress at this point.

    It appears that as of 3.9 their external patch set is much reduced. As they get more into the upstream kernel we can expect improvements and better integration with the existing power management.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    There are substantial differences in your test set up and theirs so differences in current readings are to be expected. A couple of these differences stand

    out. Since they did not specifically say the hub was powered I assume it was not. And it makes more sense that for power testing purposes to not power

    the hub externally. They stated that the HDMI was connected so I assume the GPU was in use. Between the two port hub, the thumb drive and the GPU

    I'd be surprised if that didn't account for most if not all of the differences you are seeing.

     

    I did a little checking and with a 400 KHz I2C it would take ~ 840 uS to change all three voltages (~ 280 uS for one) due to level two password

    protection of all three registers which have to be individually unlocked before writing to them. This definitely limits just how "dynamic" it can be.

    Still within the limits this sets it can be used to provide a substantial power savings when used.

     

    I received my BeagleBoard Black yesterday and had just enough to power it up tethered and spent about an hour to check it out. Not really all that

    impressed with the tethered mode as you can already do everything it does with a PC and the beagleboard.org URL. Didn't have enough time (or the

    HDMI cable) to check out anything more than that. I do have an RS232 converter I could use to hook up to the serial port so I might try that today.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    There are substantial differences in your test set up and theirs so differences in current readings are to be expected. A couple of these differences stand

    out. Since they did not specifically say the hub was powered I assume it was not. And it makes more sense that for power testing purposes to not power

    the hub externally. They stated that the HDMI was connected so I assume the GPU was in use. Between the two port hub, the thumb drive and the GPU

    I'd be surprised if that didn't account for most if not all of the differences you are seeing.

     

    I did a little checking and with a 400 KHz I2C it would take ~ 840 uS to change all three voltages (~ 280 uS for one) due to level two password

    protection of all three registers which have to be individually unlocked before writing to them. This definitely limits just how "dynamic" it can be.

    Still within the limits this sets it can be used to provide a substantial power savings when used.

     

    I received my BeagleBoard Black yesterday and had just enough to power it up tethered and spent about an hour to check it out. Not really all that

    impressed with the tethered mode as you can already do everything it does with a PC and the beagleboard.org URL. Didn't have enough time (or the

    HDMI cable) to check out anything more than that. I do have an RS232 converter I could use to hook up to the serial port so I might try that today.