Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 714 subscribers
  • Views 55800 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player. It's pretty much a cubieboard without the gpio lines. It will cost more than a Pi, but it comes with a supply and a housing. It also has a vga output and connector fitted. It has wifi and ethernet embedded if I remember well. There even is the Mele A2000G with 1Gig of ram.

    For GPIO, I prefer to use a dedicated microcontroller connected to the linux board with an usb interface. This approach might be a bit more expensive, but it makes it possible to switch from one linux board to another without much hassle. It also makes the system responsive to io changes after a fraction of a second instead of several seconds needed to boot the system. Maybe it's just me being conservative and used to embedded design on 8 bit microcontrollers. Linux adds connectivity to it and makes easy in system programming possible.

    The Mele also uses the allwinner A10 soc, so booting linux is possible from the sd card. Placing it on the internal flash memory of the player should be possible as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player. It's pretty much a cubieboard without the gpio lines.

    At least for me, it's the GPIO that makes or breaks the device, without them I'm much less interested.

     

    It will cost more than a Pi,

    Approx 60 GBP, so around twice what the Pi costs. Sure it's not a straight comparison.

     

    The A10 looks like it should be a good SoC and so far the cubieboard looks to be the closest to the sort of board I'm interested in. The danger, as always, is that something better and cheaper may come along by the time they start appearing in volume.

     

    Either way, interesting times, and I'm really hoping we'll see more and more devices of this type.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    What the raspberry pi foundation lying ?

    Who would have thunk it ?

     

    Actualy its ridiculous, they want everyone to think its an open hardware project despite the fact that you cannot buy the processsor unless you sell your soul to Broadcomm.

    and wow they are going to release the gerbers, big deal, Ive got the schematic I could do my own layout if I wanted, only trouble is......its not open hardware and you cannot buy the processor.

     

    Seriously stay away from the raspberry pi, it started life as an educational toy, got hijacked by some very strange people who think every embedded system has to run linux and several of my clients have tried to use it as the basis of their projects only to regret it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    The article in wired was pretty tyipcal of how they work, don't talk to engineers who have any experience of designing embedded systems, talk to jouralists who have not the slightest idea and they will repeat any bullshit you tell them if you take them to lunch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Frippy Frippy wrote:

     

    got hijacked by some very strange people who think every embedded system has to run linux

    Lots of embedded devices do run linux (certainly not all), but what they run doesn't tend to resemble Debian, RedHat or any other 'full fat' distros.  It's my opinion that trying to force a full desktop distro onto the Pi was a mistake, it simply doesn't have the resources to handle all the crap in todays bloated distros.

     

    Still, it had to run something. Whatever they put on it couldn't be too alien to their supposed educational audience either. Seeing them try to put VxWorks or Windows onto it might have been entertaining, but I suspect they wouldn't have sold as many as they have.  What OS would you have chosen ?

     

    several of my clients have tried to use it as the basis of their projects only to regret it.

    I've built a few things around the Pi and while I don't know that I'd go so far as to say I regret it, suffice to say that some other, incomplete, projects are being reworked to use the BBB instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I noticed that they were advertising for a senior hardware guy recently, not exactly the job where you are going to be overloaded with projects given their stated position that changes to the hardware are going to scare off the user base.

    But yes it is difficult because your supposed education user base isnt going to be too keen on bare metal, but bare metal is what you need to teach if you are going to produce embedded engineers rather than software guys who  write C++ drivers for 8 bit processors or cannot write a driver for an RS232 port without it spilling bits all over the floor as I found recently.Embedded systems design is difficult and is quite different to normal software design, but teaching would be embedded systems engineers that its all the same isnt doing anyone any good.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Frippy Frippy wrote:

     

    ... raspberry pi, it started life as an educational toy, got hijacked by some very strange people who think every embedded system has to run linux and several of my clients have tried to use it as the basis of their projects only to regret it.

     

    From my recollection of the history of RasPi, it was not intended to be an embedded computer.  It was intended to be the cheapest possible desktop computer that could run GNU/Linux.  It only had to be powerful enough so that users could learn about programming.  It's not intended to be the world greatest Internet surfing engine or gaming platform or real-time controller.  IMO it's amazing how much it does so for US$35 with Ethernet, or US$25 without.

     

    My understanding is that the RasPi foundation itself does not produce its own OS -- it only redistributes the work of others.  The various GNU/Linux distros and other operating systems are the products of their own organizations.  You can run on RasPi anything you want, or even program it at the bare metal.

     

    Yes, some people have used Raspi for embedded applications and it can often be quite successful if they don't have real-time constraints.  But like any computer-based tool, you need to match the hardware and software to the problem and if it's a poor match you can expect poor results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to johnbeetem

    Yes John your recollection is correct. While I have no doubt RPF knew it could be used for embedded purposes and were happy to support that

    (in spirit at least) it was not designed specifically for it.

     

    According to the Rapsbian web site the RPF does produce its own "official" version of Raspbian and that distro is not the same as the one on their

    web site. The other distros on the RPF web site are as you say the work of others.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 13 years ago in reply to johnbeetem

    Yes John your recollection is correct. While I have no doubt RPF knew it could be used for embedded purposes and were happy to support that

    (in spirit at least) it was not designed specifically for it.

     

    According to the Rapsbian web site the RPF does produce its own "official" version of Raspbian and that distro is not the same as the one on their

    web site. The other distros on the RPF web site are as you say the work of others.