Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 714 subscribers
  • Views 55802 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player. It's pretty much a cubieboard without the gpio lines. It will cost more than a Pi, but it comes with a supply and a housing. It also has a vga output and connector fitted. It has wifi and ethernet embedded if I remember well. There even is the Mele A2000G with 1Gig of ram.

    For GPIO, I prefer to use a dedicated microcontroller connected to the linux board with an usb interface. This approach might be a bit more expensive, but it makes it possible to switch from one linux board to another without much hassle. It also makes the system responsive to io changes after a fraction of a second instead of several seconds needed to boot the system. Maybe it's just me being conservative and used to embedded design on 8 bit microcontrollers. Linux adds connectivity to it and makes easy in system programming possible.

    The Mele also uses the allwinner A10 soc, so booting linux is possible from the sd card. Placing it on the internal flash memory of the player should be possible as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player. It's pretty much a cubieboard without the gpio lines.

    At least for me, it's the GPIO that makes or breaks the device, without them I'm much less interested.

     

    It will cost more than a Pi,

    Approx 60 GBP, so around twice what the Pi costs. Sure it's not a straight comparison.

     

    The A10 looks like it should be a good SoC and so far the cubieboard looks to be the closest to the sort of board I'm interested in. The danger, as always, is that something better and cheaper may come along by the time they start appearing in volume.

     

    Either way, interesting times, and I'm really hoping we'll see more and more devices of this type.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Frippy Frippy wrote:

     

    ... raspberry pi, it started life as an educational toy, got hijacked by some very strange people who think every embedded system has to run linux and several of my clients have tried to use it as the basis of their projects only to regret it.

     

    From my recollection of the history of RasPi, it was not intended to be an embedded computer.  It was intended to be the cheapest possible desktop computer that could run GNU/Linux.  It only had to be powerful enough so that users could learn about programming.  It's not intended to be the world greatest Internet surfing engine or gaming platform or real-time controller.  IMO it's amazing how much it does so for US$35 with Ethernet, or US$25 without.

     

    My understanding is that the RasPi foundation itself does not produce its own OS -- it only redistributes the work of others.  The various GNU/Linux distros and other operating systems are the products of their own organizations.  You can run on RasPi anything you want, or even program it at the bare metal.

     

    Yes, some people have used Raspi for embedded applications and it can often be quite successful if they don't have real-time constraints.  But like any computer-based tool, you need to match the hardware and software to the problem and if it's a poor match you can expect poor results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to johnbeetem

    Yes John your recollection is correct. While I have no doubt RPF knew it could be used for embedded purposes and were happy to support that

    (in spirit at least) it was not designed specifically for it.

     

    According to the Rapsbian web site the RPF does produce its own "official" version of Raspbian and that distro is not the same as the one on their

    web site. The other distros on the RPF web site are as you say the work of others.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    Frippy Frippy wrote:

     

    several of my clients have tried to use it as the basis of their projects only to regret it.

     

    Would you mind to share some details about this and the reasons why your clients regret now using the R-Pi for their projects ?

     

    Thanks

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Still, it had to run something.

     

    BBB is one of the few ARM boards that can run a Linux distro to provide almost instant gratification to the *nix legions and at the same time offer very tight realtime response through its PRUs.  A dedicated RTOS wouldn't provide that instant gratification except to its  small community of adherents.

     

    This *nix host + RTcores approach seems to be the best of all worlds for embedded work.  There probably isn't an RTOS in existence that offers the breadth of languages, networking, UIs, APIs, and other facilities provided by Linux, and yet BBB can still be made to behave as tightly as a microcontroller.

     

    IMO, every SoC used for top-end embedding should provide something along these lines.  And before somebody answers "RT Linux", no, just no.  Use hardware, don't compromise.  A little RISC core requires very few gates to implement, an insignificant number compared to the gatecount on the entire SoC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    BBB is one of the few ARM boards that can run a Linux distro to provide almost instant gratification to the *nix legions and at the same time offer very tight realtime response through its PRUs. 

    ...

     

    IMO, every SoC used for top-end embedding should provide something along these lines.  And before somebody answers "RT Linux", no, just no.  Use hardware, don't compromise.  A little RISC core requires very few gates to implement, an insignificant number compared to the gatecount on the entire SoC.

    Hi Morgaine,

     

    That's spot on. I really hope TI focus in this area and come up with even more powerful PRUs as time progresses of course (although the current ones are pretty amazing!), but also equally importantly have lots of documented examples of the types of things one can do with them (for example, currently I'm struggling with getting high-speed input in the GPIO mode (not GPI mode) via the PRU simply because of a lack of examples - whereas high speed output is well understood now. I know the PRU is capable, it just needs some more understanding. I can't really complain since at least the documentation is intensive - just needs a few examples code.

    Also, in future revisions it should be extended to allow the ultra high-speed (i.e. GPI and GPO modes) on even more pins.In terms of instruction set, it is already excellent, it has a rich set of registers and no restrictions on what registers get manipulated with what instructions. Also, recently the PRU documentation was updated - apparently there is MAC capability too! - for fast FFT type calculations, plus additional register banks. (see here - plus debugger information from Michael Haberler is there too).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to morgaine

    @Morgaine

     

    A few problems you forgot to mention:

     

    1) Real time programming and real time program debugging in assembly language is a real pain. Any idea of "almost instant gratification" is not being realistic and it assumes that the

         person can actually program in assembly in the first place which is already highly unlikely and getting more unlikely every year. You actually need to know and understand the

         underlying hardware well to do this effectively and the PRUs are not simple hardware.

    2) The resources available to the PRUs in terms of code (8 KB that's only 2 K instructions, see 3 below), and data RAM (8 KB with another 12 KB shared between the PRUs) is extremely

         limited.

    3) It uses only 32 bit instructions which increases code size and further limits what a PRU can do with its limited code space. This is the reason for the 16 bit Thumb instruction set used

         in ARM CPUs.

    4) Given the resources avaiable you are at best talking about a process scheduler with a small queue, event handler, and some timer functions. This is about as primitive an "RTOS" as it gets.

     

    There are probably a few more but I've already wasted too much time pointing out the obvious.

     

    And before somebody answers "RT Linux", no, just no. Use hardware, don't compromise.

     

    But compromise and knowing how to make the right compromises is what real world engineering is all about. As you already know, but apparently fail (or as far as I can tell don't even attempt to)

    comprehend, it totally depends on what level of real time you need in terms of response times and what resources the real time application requires as far as code and data space goes. Very tight

    real time response is not always needed so why would you waste hardware (and money) to get something you don't need ? Your one size "use hardware, don't compromise" fits all is the epitome

    of bad engineering. Sometimes RT Linux will work, sometimes it won't. Why, in the face of lots of evidence to the contrary (it's being used every day in real world research and commercial applications,

    even NASA uses it) do you keep insisting that it won't ?

     

    And by the way, all RTOS's that I am aware of already run on hardware, no compromise needed for that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    1) Real time programming and real time program debugging in assembly language is a real pain. Any idea of "almost instant gratification" is not being realistic and it assumes that the

         person can actually program in assembly in the first place which is already highly unlikely and getting more unlikely every year. You actually need to know and understand the

         underlying hardware well to do this effectively and the PRUs are not simple hardware.

     

    I think you misread what I wrote.  The "instant gratification" referred to the use of Linux on the host application processor, not to the programming of its embedded cores.  Assembly language and realtime programming both require detailed understanding of what you're doing, so for that part of the job there are no shortcuts.  However, when the rest of the applications processor is running Linux, everything else you do becomes easy, and the embedded realtime core can make use of powerful and easily testable services it couldn't dream of harnessing otherwise.  That's the instant gratification part, the Linux part.

     

    2) The resources available to the PRUs in terms of code (8 KB that's only 2 K instructions, see 3 below), and data RAM (8 KB with another 12 KB shared between the PRUs) is extremely

         limited.

    3) It uses only 32 bit instructions which increases code size and further limits what a PRU can do with its limited code space. This is the reason for the 16 bit Thumb instruction set used

         in ARM CPUs.

    4) Given the resources avaiable you are at best talking about a process scheduler with a small queue, event handler, and some timer functions. This is about as primitive an "RTOS" as it gets.

     

     

    Sure, the PRUs are very restricted, but then they don't need to do much when the host is a full Linux, just handle input and close the loop with low-latency output in response, then pass a message to the host for the non-realtime part of the operation.  Doing any complex work on the PRUs is missing the point of there being an application processor available to work in tandem.  It would be a mistake even if the PRUs were large and as fast as the ARM.

     

    As you already know, but apparently fail (or as far as I can tell don't even attempt to)

    comprehend ...

     

    [the rest, all irrelevant as it slides downhill into a typical Stewart rant interlaced with attacks]

     

     

    You failed, completely, 1) to read what I wrote about "instant gratification", 2) to understand how PRUs are best used and instead are looking for a full RTOS, 3) to understand how poor the realtime behavior of realtime Linux is (we've had that discussion before and repeating it is pointless because you insisted on making an erroneous conclusion from known facts), and 4) you also fail by turning every engineering discussion into a personalized argument.

     

    It is always you who takes that first step, and I do not turn the other cheek.  You fail utterly, I reciprocate.  (Is this what you're looking for?)

     

    We're never going to  be able to hold a sensible engineering discussion if you always insist on personalizing your comments into attacks.  Make your choice next time.  Either technology, or brickbats.  They don't mix, they derail.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Link to benefit people if they want to read Stewart's opinion on RTOSs - and other's opinions.

    The fact that timing can be engineered down to 5nsec for critical timing with the PRU means that all of a suddent things like controlling custom displays and stepper motors while running Linux become possible on a single chip. RTLinux could not have done that. I'm talking about events of the order of tens of nanosec, because that's the space where lots of modern hardware operates.

     

    I think it's clear to see by simple google that many people are finding real-world use-cases for the high-speed that small processors like PRU offers in conjunction with Linux applications. I think people who try it will really adopt this method. So, possibly times have changed. Also, that was clear tens of years ago, when other RTOS's attempted at reducing latency down to tens of usec speed levels for the processors at that time.

     

    To summarize, for anyone who wants to be able to control signals at high speed (i.e. MHz, tens of MHZ approaching 100MHz), and even down to tens of kHz, while maintaining the benefits of being able to use Linux apps and existing libraries of code, it is highly worth considering the PRU i.e. separate core method - which integrates nicely with the application processor. With the RPI, a CPLD or add-on microcontroller is a suitable method.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to morgaine

    @Morgaine

     

    The "instant gratification" referred to the use of Linux on the host application processor, not to the programming of its embedded cores

     

    Must have been the at the same time part. As you yourself explain they must be programmed to use them with the "instant gratification" Linux part. And the "instant gratification" Linux part must be

    programmed too. None of this programming happens in an instant.


    I wrote:

     

    Very tight real time response is not always needed so why would you waste hardware (and money) to get something you don't need ? Your one size "use hardware, don't compromise" fits all is the epitome

    of bad engineering. Sometimes RT Linux will work, sometimes it won't. Why, in the face of lots of evidence to the contrary (it's being used every day in real world research and commercial applications,

    even NASA uses it) do you keep insisting that it won't ?

     

    No rant or irrelevancy here, just facts. Why won't you answer the questions (rhetorical) ? There was only one "attack" and it was on your failure on several occasions past and present to simply acknowledge that

    there are applications where RT Linux does work instead of "just say no". As always when you get questions you would rather not answer your response is to attack the message and the messanger. Fine.

     

     

    @ shabaz

     

    I wrote:

     

    Sometimes RT Linux will work, sometimes it won't.

     

    This is not an opinion and I have always framed my arguments around that. You always respond with cases where it won't. They do not in any way negate cases where it will.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to gdstew

     

    Gary Stewart wrote:

     

    This is not an opinion

    I didn't say it was. I said the link was to your opinion - and in fact your first sentence at that link is

    "You really need to get better acquainted with real time Linux." - That's your opinion.

     

    Gary Stewart wrote:

     

    You always respond with cases where it won't. They do not in any way negate cases where it will.

     

    I think you're right; because these are precisely the cases I'm hitting. If you're hitting cases that you can solve with 100usec latency, then this is great too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago in reply to gdstew

     

    Gary Stewart wrote:

     

    This is not an opinion

    I didn't say it was. I said the link was to your opinion - and in fact your first sentence at that link is

    "You really need to get better acquainted with real time Linux." - That's your opinion.

     

    Gary Stewart wrote:

     

    You always respond with cases where it won't. They do not in any way negate cases where it will.

     

    I think you're right; because these are precisely the cases I'm hitting. If you're hitting cases that you can solve with 100usec latency, then this is great too.