Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54235 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • gdstew
    gdstew over 13 years ago

    I'd like to add another pro for the BeagleBoard Black.

     

    With the exceptions of the integer real time processors PRU-ICSS (not sure at this point why that is), and the PowerVR GPU for

    well known reasons, the AM3359 technical documentation from TI is excellent to the point of overwhelming. The Technical Reference

    Manual is over 4000 pages. No I did not accidentally add any zeros !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    With the exceptions of the integer real time processors PRU-ICSS (not sure at this point why that is), and the PowerVR GPU for well known reasons, the AM3359 technical documentation from TI is excellent to the point of overwhelming.

     

    You're right about the proprietary GPU, that seems to be an endemic problem for open source in the industry.  It's not true for the PRU-ICSS though.

     

    The PRU-ICSS is fully documented in the Technical Reference Manual SPRUH73C, with the entirety of chapter 4 (250 pages) devoted to it.  Also, there is a full package of PRU-related materials on Github, including more documentation and source code of the PRU's PASM assembler, a Linux loader, demos, etc.  I've even checked that the assembler compiles and it does.

     

    The BeagleBone materials on Github are at https://github.com/beagleboard/am335x_pru_package

     

    The PRU has been used successfully in quite a number of projects as a quick web search shows, and this long predates the BeagleBone Black since the original BeagleBone uses a slightly different version of the same AM3359 SoC.

     

    Morgaine.

     

    Addendum: Repeating the link to TI's wiki pages on PRU which I gave in my first post on this thread, in case it was missed when looking for docs.  There is a developers' link at the bottom of that first page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    The KL25z apears to also fit

     

    While it fits in the tin, it doesn't fit in the group. image

     

    Just to clarify that the mention of KL25Z wasn't to rank the Freedom board alongside BB and Pi.  For the benefit of new readers ...

     

    Microcontrollers like the KL25Z/Cortex-M0+ are in a different category to application processors like the BCM2835/ARM11 or AM3359/Cortex-A8, which is why manufacturers use those two different terms as marketing slots.  ARM even formalizes the distinction in their naming now, Cortex-M (or R) series versus Cortex-A, which is much clearer than the terminology they used back in the days of ARM9 and ARM11.

     

    Boards like the Freescale Freedom KL25Z belong in the microcontroller group alongside ST's STM32F4-Discovery and the zillion forms of Arduino.  The SoCs in this group typically do not provide an MMU (at best they may provide an MPU with a small number of segments like 8), and so they cannot properly support full operating systems with strong process separation.  That's why they're nearly always programmed either as bare metal or running an RTOS designed for microcontrollers.  (The special uClinux variant can run on them, but its use has decreased markedly now that application processors are common.)

     

    Application processors have proper MMUs and so can run full Linux or other process-protected operating systems.  They're best considered separately, so your suggestion of "Pi A, Pi B, BB, BBB" is a cohesive set since they all employ application processors.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    Also can someone please explain the fascination with Antoids tins.

    The KL25z apears to also fit, although I'm not sure why you'd use a metal tin to house a bare pcb that needs external connections in order to function, and generally will have a display or leds that somehow need to get through to the outside world.

    I'll have a go.  Developer boards (almost) never have cases.  This is probably because while it's very cheap to manufacture cases in quantity, the tooling for the first one is expensive.  Plus, if your target audience is makers, those makers are perfectly capable of making their own cases.  Makers like to take objects they already have and re-purpose them.  Creative use of things that would be otherwise thrown out scores Karma points, or something like that.

     

    RasPi is frustrating because while its rectangular dimensions are the same as a credit card, its square corners prevent it from fitting in an Altoids tin.  Plus, even if you could fit it in, having connectors on five sides (if you include GPIO) makes an Altoids tin problematic.  RasPi only has two "mounting" holes (zero on the rev 1.0 board), which makes a metal case problematic.  BBone has rounded corners so it fits nicely in the case and the four mounting holes make sure you don't short to the metal case.  Having standard I/O jacks only on the ends is very nice.  OTOH, as soon as you plug in a cape it no longer fits.

     

    I far prefer a metal case to plastic.   While EMI shouldn't be a problem with well-designed boards, plastic is a thermal insulator and I'd rather have something that conducts heat and acts as a radiator.  The RasPi model B rev 1.0 sometimes ran quite hot before rev 2.0 fixed an electrical problem and improved the thermal design for the LAN9512.  IMO rev 1.0 is not something that you want to put in a closed plastic or wood case, and rev 2.0 still generates the same amount of heat overall and would get hot in a closed case.  It will work for a while, but excessive heat shortens the lifetime of any electronic device, particularly if you thermal cycle it.

     

    Now for BBone, one should use a YipYap box instead of Altoids.  I think they're the same size. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    Also can someone please explain the fascination with Antoids tins.

     

    Peergroup reinforcement among techies. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    This is a much better debate ...well done.

    Thanks for the responses re the comparisons/features.

     

    A new user looking to compare them still has to read through lots of discussions in order to draw a list.

    Epigram #48 from Epigrams in Programming by Alan J. Perlis is:

    The best book on programming for the layman is Alice in Wonderland; but that's because it's the best book on anything for the layman.

    Let's see what Alice's Adventures in Wonderland has to say on the topic.

    "Cheshire Puss," [Alice] began, rather timidly... "Would you tell me, please, which way I ought to go from here?"

     

    "That depends a good deal on where you want to get to," said the Cat.

     

    "I don't much care where--" said Alice.

     

    "Then it doesn't matter which way you go," said the Cat.

    Same with RasPi and BBone.  It does depend on what you want to do with it, though as Morgaine pointed out the difference has narrowed with BBone Black.

     

    One thing I would strongly recommend to anyone considering either board -- or any community-supported development board -- is to first spend some time at the forums available for that board.  See how active the forum is, and whether people are getting helpful responses to problems or are being told to RTFM (without providing link to said manual), or worse, "Google it" as if a newbie can tell which few of the 1000 Google results are actually useful.  If you have questions, these are the people who are going to help you -- or not.  Find out if people are having issues with the board and whether you want to face those same issues.  Also, check out the wiki for the board.  It will tell you if people are interested enough in the board to build up a good wiki and are therefore more likely to be interested in helping you when you get in trouble.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to morgaine

    Morgaine

    Yes thanks for explaining the KL25z wasn't part of the discussion of Pi v BB.

    It was just the size.

     

    John

    You have some good reasons ...obviously the Antoid tins are a household item on the other side of the world, hence the inital reason.

    I also like your advice on the forums/support.

     

    Morgaine

    I think your answer is probably what I expected.

    I had to ask though.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to mcb1

    Yay, more boards with rounded corners! And cheap too! image

     

    Not on topic though, except for the rounded corners and the Element 14 angle. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Yay, more boards with rounded corners! And cheap too! image

     

    Not on topic though, except for the rounded corners and the Element 14 angle. image

    I like the way the Farnell site shows availability as "Awaiting Delivery" -- sounds like we're expecting a "bundle of joy" image.  The USA Newark site just says "Availability: 0" -- no poetry at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I like the way the Farnell site shows availability as "Awaiting Delivery" -- sounds like we're expecting a "bundle of joy" image.

     

    Better not give Marketing ideas, I really don't want to have my boards delivered with nappies and baby powder. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to morgaine

    Here in NZ its 4 times the price of KL25z, but with less features.

     

    Maybe nappies and baby powder will help sell it.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to mcb1

    Hehe. image

     

    I don't know PSoC4, but a quick glance at Element 14's linked summary suggests that it's along the lines of PSoC5, which John has often described here (in CPLD/FPGA threads) as being a microcontroller SoC with partially documented programmable logic features.

     

    That makes this board rather eclectic and somewhat alienating to those who prefer traditional CPU software programming.  Perhaps the manufacturer is trying to dispell that image by releasing the board at prices that fall below the worry radar ... except in NZ, that is. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to mcb1

    Hehe. image

     

    I don't know PSoC4, but a quick glance at Element 14's linked summary suggests that it's along the lines of PSoC5, which John has often described here (in CPLD/FPGA threads) as being a microcontroller SoC with partially documented programmable logic features.

     

    That makes this board rather eclectic and somewhat alienating to those who prefer traditional CPU software programming.  Perhaps the manufacturer is trying to dispell that image by releasing the board at prices that fall below the worry radar ... except in NZ, that is. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I don't know PSoC4, but a quick glance at Element 14's linked summary suggests that it's along the lines of PSoC5, which John has often described here (in CPLD/FPGA threads) as being a microcontroller SoC with partially documented programmable logic features.

     

    That makes this board rather eclectic and somewhat alienating to those who prefer traditional CPU software programming.  Perhaps the manufacturer is trying to dispell that image by releasing the board at prices that fall below the worry radar ... except in NZ, that is. image

    PSoC4 is a low-cost version of PSoC5, replacing PSoC5's Cortex-M3 with a Cortex-M0.   The PSoC line is quite interesting: Cypress integrates a processor, various digital blocks, and analog blocks all onto the same chip with a programmable interconnect to tie everything together and route to the pins.  The idea is to have a single chip provide everything for an embedded product, including the analog circuits.  The functions of the blocks and the routing are all programmed by the CPU through addressable registers, almost all of which are documented.  Cypress has a Windows-based tool called PSoC Creator that lets you select and interconnect the blocks, and it generates a C program that does the register initializations for you so you don't have to read an 1800-page manual.

     

    My beef with the chip has been that I want to be able to use it for teaching logic design using my own tools.  Cypress almost provides enough data to do this, but as far as I can tell the routing control registers aren't documented well enough to use them.  It may be that I'm wrong and the information is now there -- please tell me if that's the case!

     

    PSoC has had limited success, largely because the chips have been rather expensive.  PSoC4 is supposed to change this by providing a highly capable SoC for US$1.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    PSoC has had limited success, largely because the chips have been rather expensive.  PSoC4 is supposed to change this by providing a highly capable SoC for US$1.

     

    Did you notice that the  CY8CKIT-042 PSoC4 Pioneer Kit board contains, in addition to the PSoC4 target device, a PSoC5 device that's used for board programming and debug?  (The intro video mentioned it.)  If PSoC4 is the cheap device, you'd think they'd use a second PSoC4 to provide that function on this cheap board.

     

    It seems a little bizarre, but I guess they already had PSoC5 code developed for the required function, and don't expect to sell enough boards to recoup additional development required to use the cheaper part instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    John Beetem wrote:

     

    PSoC has had limited success, largely because the chips have been rather expensive.  PSoC4 is supposed to change this by providing a highly capable SoC for US$1.

     

    Did you notice that the  CY8CKIT-042 PSoC4 Pioneer Kit board contains, in addition to the PSoC4 target device, a PSoC5 device that's used for board programming and debug?  (The intro video mentioned it.)  If PSoC4 is the cheap device, you'd think they'd use a second PSoC4 to provide that function on this cheap board.

     

    It seems a little bizarre, but I guess they already had PSoC5 code developed for the required function, and don't expect to sell enough boards to recoup additional development required to use the cheaper part instead.

    Yes, I saw that.  It's not at all unusual to have a much more capable part as the program/debug interface.  If I've read the data sheets correctly, the PSoC4 only has 32KB flash and 4KB SRAM, while the PSoC5 has 256KB flash and 64KB SRAM.  It's hard to squeeze much into 32K+4KB, particularly if the code is written by people who didn't grow up carrying around boxes of punched cards (2000 cards per box * one box per arm * two arms per human = 4000 lines of code that you can "comfortably" carry around if you have two arms).

     

    Reminds me of an LPXpresso board I have for the LPC1114FBD48/301,1LPC1114FBD48/301,1 -- a Cortex-M0 with 32KB flash and 4-8 KB RAM.  It's controlled by an LPC3154 -- an ARM9 with 192KB RAM.  I don't know how this compares to an mbed because my mbed has the controller's part number erased.

     

    It's often the case that the control SoC is the one to play with, provided that the vendor hasn't disabled access.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Reminds me of an LPXpresso board I have for the LPC1114FBD48/301,1LPC1114FBD48/301,1 -- a Cortex-M0 with 32KB flash and 4-8 KB RAM.  It's controlled by an LPC3154 -- an ARM9 with 192KB RAM.

     

    Haha.  That's a pretty severe case of an application processor in servitude to a microcontroller.  It can't be impressed. image

     

    I guess it's only a matter of time before Cortex-A series devices are given such roles too, particularly if a small realtime microcontroller needs a full-function IPv6 stack and comprehensive networking apps, and the simplest way of providing this is by giving it an entire Linux subsystem on a different SoC.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I guess it's only a matter of time before Cortex-A series devices are given such roles too, particularly if a small realtime microcontroller needs a full-function IPv6 stack and comprehensive networking apps, and the simplest way of providing this is by giving it an entire Linux subsystem on a different SoC.

    Actually, at some point it might be a good idea just to have the vendor's eval board be a BeagleBone cape.  That way they don't have to design their own controller hardware.  One problem with this is that the vendor has to worry about whether the user has a compatible operating system.  I don't have experience with Linux device drivers, but it may also be that it's a lot easier to write the whole debug controller on a bare chip than to write the Linux driver image  Note that I didn't mention RasPi -- the vendor needs an open hardware project so it's not stuck if the controller board is discontinued.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Note that I didn't mention RasPi -- the vendor needs an open hardware project so it's not stuck if the controller board is discontinued.

     

    How is any ARM SOC with a proprietary GPU considered to be open hardware ? Isn't that a contradiction of terms ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    John Beetem wrote:

     

    Note that I didn't mention RasPi -- the vendor needs an open hardware project so it's not stuck if the controller board is discontinued.

     

    How is any ARM SOC with a proprietary GPU considered to be open hardware ? Isn't that a contradiction of terms ?

    Well, technically you're right since open source hardware (OSH) requires that all chips be fully documented.  However, my example of using BeagleBone as the controller for a chip's demo board doesn't need the GPU so for this application BeagleBone is indeed OSH.  You have open schematics, everything documented except GPU (I personally believe the PRUSS omission in latest TRM is an oversight), Gerbers, BOM, and all chips can be purchased in low volumes.  This is very different from RasPi, where most of the SoC is undocumented and it cannot be purchased in low volumes, and there are no Gerbers.

     

    I don't know what discussion OSH advocates are having about GPUs.  I suspect some argue that if you provide a GPU + binary blob, then as long as the API interface is fully documented you can think of the GPU as an OpenGL black box that happens to be implemented with downloadable black-box microcode.  However, in that case I would say you can't call it a GPU -- it's an embedded OpenGL engine where the implementation is hidden the same way you don't expose the innards of the ARM implementation.  IMO if you call it a GPU, then you have to let me program it or it's not OSH.

     

    I find the fact that FPGA bit streams are undocumented is much more annoying.  Yet, OSH champions like FPGAs since it lets them design their own open CPU architectures.  So plenty of opportunities to argue about how many angels can dance on the head of a pin.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Well, technically you're right since open source hardware (OSH) requires that all chips be fully documented.  However, my example of using BeagleBone as the controller for a chip's demo board doesn't need the GPU so for this application BeagleBone is indeed OSH. 

    There's no argument that GPU's are a problem and are likely to remain locked up behind a wall of patents, cross licensing and whatnot. So regardless of other issues the Pi isn't on the same playing field here. Most other SoCs are an Arm core with an undocumented, propriatary, GPU along for the ride, you can ignore the GPU, probably even turn it off and still use the rest of the SoC. For the Pi, you have an undocumented, propriatary Videocore GPU, with an Arm along for the ride - you can't get to the Arm without the GPU as the SoC is first and foremost a GPU.

    Even if the interface into that black box was fully documented it doesn't matter. A patent or licensing dispute could render you unable to legally use the GPU firmware and so unable to access the Arm.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to johnbeetem

    Another advantage for the BeagleBone Black, beyond OSHW, is that the BeagleBoard.org development community (TI employees, Linux kernel maintainers & various individuals) have been working hard to get all remaining patches accepted by the mainline.  jkridner has told me that is an important goal for the project to be able to just git clone Linus's kernel and go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Well, technically you're right since open source hardware (OSH) requires that all chips be fully documented.  However, my example of using BeagleBone as the controller for a chip's demo board doesn't need the GPU so for this application BeagleBone is indeed OSH.  You have open schematics, everything documented except GPU (I personally believe the PRUSS omission in latest TRM is an oversight), Gerbers, BOM, and all chips can be purchased in low volumes.  This is very different from RasPi, where most of the SoC is undocumented and it cannot be purchased in low volumes, and there are no Gerbers.

     

    I'm not sure not using any particular piece of the hardware is an exemption since "technically" it is still proprietary. What if you decide to add an LCD display to the controller ? Certainly not an unusual possibility.

    As I am sure you are aware the Raspberry Pi also has schematics. I find I rarely need Gerbers. I find having schematics essential. I would prefer to have both but I can definately live without Gerbers The only parts

    of the BCM2835 that I know of that are not documented well enough to write drivers for are the GPU and the media engine (DSP?). Media engines are usually in the same boat as GPUs for the same reasons.

     

    I'm not sure the AM335x can be purchased in low volumes either, got a source ?

     

    Not talking about angels or pinheads, talking about proprietary hardware which can not by any definition be called open no matter which SOC it is on.

     

     

    silsinork wrote:

     

    Most other SoCs are an Arm core with an undocumented, propriatary, GPU along for the ride, you can ignore the GPU, probably even turn it off and still use the rest of the SoC. For the Pi, you have an undocumented, propriatary Videocore GPU, with an Arm along for the ride - you can't get to the Arm without the GPU as the SoC is first and foremost a GPU.

    Even if the interface into that black box was fully documented it doesn't matter. A patent or licensing dispute could render you unable to legally use the GPU firmware and so unable to access the Arm.

     

    No idea what you are talking about here, you can ignore the GPU on the Pi too. The GPU by itself is useless without the ARM core, the opposite is not true. It is first and foremost an application processor that

    expects to have a GPU, but it does not require that the one it has be used. It may require that it have a bare minimum initialization but that does not appear to be a problem since several Linux distros, a BSD,

    and RiscOS have been able to do it, and it is not unusual for other hardware to require some initialization as well before the core can get down to the real business at hand.

     

    Since the GPU is a Broadcom design a license dispute is probably not reasonable. As far as patents go any patent dispute on any SOC whether the item in question is being used or not would have exactly the

    same effect since the SOC physically contains the "patent". One could never guaranty that it would not be used unless it is removed and I'm sure that it can't be removed from any devices that already exists.

    Where you go from there is up to the lawyers, judge, or jury.