Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum One of my "Pi-compatible" HDMI/VGA Adaptors doesn't work to my display.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 707 subscribers
  • Views 779 views
  • Users 0 members are here
  • video
  • raspberry_pi
  • raspberrypi
Related

One of my "Pi-compatible" HDMI/VGA Adaptors doesn't work to my display.

mgt6910
mgt6910 over 13 years ago

I have 2 HDMI/VGA adaptors, both certified compatible with Raspberry Pi by their supplier, but only the second listed below works between my Pi and a Proview RV729/700P display.

 

I have used the parameter "hdmi_safe=1" in config.txt, but that is not sufficient with the first adaptor.  Any ideas what other config parameters might need changing for this to work ?

 

This one displays nothing:

http://www.minifo.com/en/hdmi-to-vga-adapter.html

 

This one works fine, displaying 28 lines of 74 characters:

https://www.modmypi.com/pi-vew-raspberry-pi-hdmi-to-vga-converter

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    my config has only the following "active" lines in it (the rest are comented out) without the "hdmi_mode=16" i was only getting a blank screen on my monitor using a china made adaptor try the below config and see what happens.

     

    framebuffer_width=1024

    framebuffer_height=768

    console-width=1024

    console-height=768

     

    # uncomment to force a specific HDMI mode (this will force VGA)

    hdmi_group=1

    hdmi_mode=16

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mgt6910
    mgt6910 over 13 years ago in reply to e14 Contributor

    I am having trouble with this.  I would like to confirm the use of underscore after framebuffer and minus after console

    (before I brick my configuration), but I can find no documentation of any options beginning with the keyword "console".

    Is there a definitive description somewhere of all the options supported in config.txt ?

     

    P.S.  I've found references to the framebuffer options in http://elinux.org/RPi_config.txt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mgt6910

    my running config is has exactly those lines and yes its odd but thats how it looks in the config for my XBMC and raspbian sd cards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mgt6910
    mgt6910 over 13 years ago in reply to e14 Contributor

    Tests completed.   The display shows a large alert box with the message "display mode not supported".  It then functions just as it did with my previous config.txt, apart from the alert box hiding the central part of the screen. I guess that it is falling back to some default mode.  This is with the "approved"  Pi-View converter from Element14, no reason to try the doubtful converter after that result.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mgt6910
    mgt6910 over 13 years ago in reply to e14 Contributor

    Tests completed.   The display shows a large alert box with the message "display mode not supported".  It then functions just as it did with my previous config.txt, apart from the alert box hiding the central part of the screen. I guess that it is falling back to some default mode.  This is with the "approved"  Pi-View converter from Element14, no reason to try the doubtful converter after that result.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mgt6910

    try reducing the resolution using the below

     

    framebuffer_width=640

    framebuffer_height=480

    console-width=640

    console-height=480

     

    # uncomment to force a specific HDMI mode (this will force VGA)

    hdmi_group=1

    hdmi_mode=16

    I suspect the monitor cant handle the higher resolutiions