Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pidora 18 (Raspberry Pi Fedora Remix) Released!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 706 subscribers
  • Views 5053 views
  • Users 0 members are here
  • raspberry_pi
Related

Pidora 18 (Raspberry Pi Fedora Remix) Released!

e14 Contributor
e14 Contributor over 13 years ago

Pidora 18 (Raspberry Pi Fedora Remix) Release

 

We're excited to announce the release of Pidora 18 --

an optimized Fedora Remix for the Raspberry Pi.

It is based on a brand new build of Fedora for the ARMv6

architecture with greater speed and includes packages

from the Fedora 18 package set.

 

* * *

 

There are some interesting new features we'd like to highlight:

* Almost all of the Fedora 18 package set available via yum

    (thousands of packages were built from the official Fedora

    repository and made available online)

* Compiled specifically to take advantage of the hardware already

    built into the Raspberry Pi

* Graphical firstboot configuration (with additional modules

    specifically made for the Raspberry Pi)

* Compact initial image size (for fast downloads) and auto-resize

    (for maximum storage afterwards)

* Auto swap creation available to allow for larger memory usage

* C, Python, & Perl programming languages available & included

    in the SD card image

* Initial release of headless mode can be used with setups

    lacking a monitor or display

* IP address information can be read over the speakers and

    flashed with the LED light

* For graphical operation, Gedit text editor can be used with

    plugins (python console, file manager, syntax highlighting)

    to serve as a mini-graphical IDE

* For console operation, easy-to-use text editors are included

    (nled, nano, vi) plus Midnight Commander for file management

* Includes libraries capable of supporting external hardware

    such as motors and robotics (via GPIO, I2C, SPI)

 

* * *

 

For further documentation, downloads, faq's, read-me's,

    how-to's, tutorials, or videos:

        http://pidora.ca/

 

* * *

 

Pidora 18 is a Fedora Remix -- a combination of software packages

from the Fedora Project with other software.

 

The Fedora Project is a global community of contributors working

to advance open source software. For more information or to join

the Fedora Project, see http://fedoraproject.org

 

Pidora is a project of the Seneca Centre for Development of Open

Technology (CDOT). To connect with CDOT, please visit

http://cdot.senecacollege.ca

 

The Raspberry Pi is a small, inexpensive computer board designed

to provoke curiosity and experimentation in programming and

computer electronics. For more information, see the Raspberry

Pi Foundation website at http://raspberrypi.org

 

* * *

 

 

- - -

The CDOT team at Seneca College

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Andrew,

       Thanks for showing up in this forum to make the announcement!

     

       Can you tell us if this release fixes the firmware problem that

    prevented the previous F18 release from working with Hynix memory?

    http://trac.proximity.on.ca/projects/rpfr/ticket/161

    https://fedorahosted.org/arm/ticket/65

     

      Will there be release notes showing what problem reports have been closed?

     

       Can you tell us if there are any plans to maintain this release,

    unlike the F14, F17, and F18 releases?

     

       Can you tell us if there are any plans to consolidate your two

    bug tracking systems into a single system (and remove the spam)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    The current firmware we are using is Version 20130415git1c339b1, this is the firmware that was last committed on May 14th.

     

    More information will be posted on pidora.ca or the pidora wiki when available. We will be maintaining this release.

     

    Bug tracking should be done with, as stated by the pidora wiki: http://trac.proximity.on.ca/projects/rpfr/

     

    The current process for tracking bugs will be updated in the wiki: http://zenit.senecac.on.ca/wiki/index.php/Pidora_18_Bug_Tracking

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       Thanks for the reply!

       I'm curious what's your role with the Pidora project?

    I don't see you mentioned at:

      http://blog.chris.tylers.info/index.php?/archives/268-The-OSTEP-Team.html

    but I see you now at:

      http://zenit.senecac.on.ca/wiki/index.php/User:Oatley

     

    > We will be maintaining this release.

     

    That's really good to hear.

    I hope you close the problem reports that the release fixes.

    Will you also be maintaining the soft-float F-18 release, such as

    updating its firmware to work with Hynix memory, or is it dead now?

     

    Will there be a link from your pidora web page to your meeting minutes?

     

    Will you be cleaning out the spam from your bug tracking site?

    I see 6 open problem reports at:

       http://trac.proximity.on.ca/projects/rpfr/report/1

    5 of which contain spam, and the remaining one (#161) shouldn't

    be on the Open list.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    I'm responsible for the infrastructure for the OSTEP team(not just pidora), though I am quite new, started in January. My responsibilities include making sure the network, servers, builders, and build system are running. Non-pidora related I work with unstable development boards and making sure services for the OSTEP team are working. I added myself to the list: http://zenit.senecac.on.ca/wiki/index.php/User:Oatley.

     

    Can't say on current plans for soft-float F-18.

     

    We are working on a solution for the spam(it may already be fixed), still need to clean out the existing spam. Not sure if our meetings will ever end up on the pidora page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

    >  Not sure if our meetings will ever end up on the pidora page.

     

    I'm not sure what you mean by that.  Where do you intend your minutes

    to be linked from?   I hope you're not wanting to keep them secret.

    Some OSTEP minutes are already published at:

       http://zenit.senecac.on.ca/wiki/index.php/Category:OSTEP_Meeting

    although these are very hard to find, and are somewhat in shambles.

    For example, the minutes labeled:

       OSTEP Meeting 2012-04-11 (note 2012)

    and

       OSTEP Meeting 2013-03-11 (note -03-)

    both appear to actually be minutes of 2013-04-11,

    and many meeting dates show no minutes at all.

     

    As far as I know, there's no OSTEP blog or public mailing list,

    so the minutes are all we have to go on besides the wiki which

    has been very poorly maintained.

     

    What are your plans for transfering your open problem reports from

    your bug tracker at https://fedorahosted.org/arm to your other tracker

    at http://trac.proximity.on.ca/projects/rpfr ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    I'm definitely not the person to answer all these questions, but I'll give it my best.

     

    We will not be keeping anything a secret. I don't think the OSTEP meetings will be placed on pidora.ca, since not everything is pidora related, though there may be some better ways to publish pidora information. That is mostly likely going to be decided by another member of the OSTEP team, I can't give information on that.

     

    We are currently looking over the two different tracking systems, and all the open tickets. Hopefully more information and progress on all of these things will be out soon.

     

    Thanks for your comments, it is good to know what people may be worried about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,
      Sorry to bombard you with a bunch of questions that you aren't

    the right person to answer, but you're the only person from Seneca who

    has dared to show his face in this forum since the first RPi release.

    We have been completely puzzled why F14 was released and then

    withdrawn with no replacement until F17, and then why F18 was

    released with no maintenance, and why your bug trackers are

    in shambles and why your meeting minutes are in shambles,

    and why your wiki is in shambles. 

     

    If this is a serious project, we would like to see a single bug tracker

    without spam, release notes with releases, plans for F19, plans for

    soft-float F18 maintenance, a maintained wiki, minutes of meetings, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    Noted. Thanks again for the input, we'll do our best. If you're interested look over the release material and give Pidora 18 a try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       I looked over the release material, and was distressed not to find any release notes

    saying which problem reports were fixed.  If there have been improvements in speed,

    I don't see any benchmarks to demonstrate that, either in comparison to the prior

    soft-float F18 or to the competing Raspian hard-float.

     

      I can't even find Pidora mentioned with the other releases at:

    http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/

     

    The F18 soft-float did have release notes, at:

    http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/18/images/RaspberryPi-Fedora-Remix-18-Release-Notes.txt

    but with sloppy mistakes:

      "Model A has been redesigned to have 512Mb RAM"

    but this should say 256, not 512, and MB, not Mb.

       "The Raspberry Pi Fedora Remix 17 will be the second version of the Remix released."

    but this should say 18, not 17, and third version, not second.

        "firmware version: raspberrypi-firmware-20120727git0d88fba-1"

    I don't really think it's quite that old.  I think it's dated Nov 23, 2012,

    rather than Jul 27, 2012.

       3 fixed problems are listed, but without problem tracking numbers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       Are you maintaining two separate wiki's now?

        

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix

    http://zenit.senecac.on.ca/wiki/index.php/Pidora

     

    There is a lot of obsolete information in the first wiki, and even some

    in the second, such as:

     

    "The Remix was produced at the Seneca Centre for Development of Open Technology, which hosts the Fedora ARM build system."

    I believe the Fedora ARM build system is hosted now in Phoenix, AZ, not Seneca.

     

    "For suggestions on packages to meet particular needs and which run well on the Raspberry Pi, see Raspberry Pi Fedora Remix 14 - Suggested Packages."

    I believe this Remix 14 link is no longer specifically applicable, since C is

    included now with Pidora.

     

    The FAQ at

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_FAQ#Why_is_the_Remix_slow.3F

    currently says:

     

    "The GUI in particular is slow, because the 2D graphics (the X Window System) are not yet connected to the 3D graphics processing unit on the SOC."

     

    Similarly, the Educational Pilot currently says:

    "At this time, regular 2D graphics do not use the 3D accelerator built into the Pi. Therefore, the regular graphical user interface is somewhat slow. The 2D graphics will be hooked up to the 3D accelerator at some point in the future."

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Educational_Pilot

     

    Are you still trying to accelerate X Windows using the 3D GPU? 

    Or have you given up on that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    >Are you maintaining two separate wiki's now?

    The Raspberry Pi Fedora Remix wiki is related to the soft-float version, while the pidora wiki is related to our new release.

     

    Checking out some of the errors you pointed out.

     

    Related to making windows faster using the GPU, you can check out http://en.wikipedia.org/wiki/Wayland_(display_server_protocol). I believe they have released support for the raspberry pi as well.

     

    Just to note, some stuff will be fixed and cleaned up regarding the wiki and other materials.

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       What are your plans with regard to the kernel?

     

    The kernel version is said to be 3.6.11.

    Do you have plans for 3.8.x?

     

    Do you know what is the date of the latest patch to 3.6.11

    that is included? 

    Does it include the recent USB fixes for keyboards

    missing and repeating keys?

     

    The wiki at

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_FAQ#What_are_the_Future_Plans_for_the_Raspberry_Pi_Fedora_Remix.3F

    currently says:

     

    "The number of packages in the Raspberry Pi-specific repositories is expected to diminish over time -- by the time that Fedora 19 is released (May 2012), the Raspberry Pi repositories should hopefully contain mot much more than the VideoCore libraries and headers. (If these were ever to become licensed these under an OSI-approved license then the need for a Remix will be eliminated, and the Raspberry Pi could be directly supported as a Fedora target)."

     

    Aside from the mistake in the date, May 2012 should be May 2013 (or later),

    has the number of Pi-specific packages diminished over time as expected?

    Do you still expect F19 to contain "mot [sic] much more than VideoCore libraries

    and headers"?

     

    With the opensourcing of the all the ARM-based libraries and headers,

    is there still a need for a Remix?

     

    The same wiki section also says:

     

    "The future of the Remix is closely tied to the plans of the Fedora ARM project. By the release of Fedora 20 in November 2013, the ARM architecture will hopefully be promoted to Primary Architecture status, meaning that the ARM release will be done in lock-step with the x86 PC release."

     

    How have the plans for the F19 RPi Remix been affected by Fedora ARM dropping

    support for pre-v7 versions of ARM?

    Are you still expecting Fedora 20 to include RPi as a primary architecture?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       What are your plans with regard to the kernel?

     

    The kernel version is said to be 3.6.11.

    Do you have plans for 3.8.x?

     

    Do you know what is the date of the latest patch to 3.6.11

    that is included? 

    Does it include the recent USB fixes for keyboards

    missing and repeating keys?

     

    The wiki at

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_FAQ#What_are_the_Future_Plans_for_the_Raspberry_Pi_Fedora_Remix.3F

    currently says:

     

    "The number of packages in the Raspberry Pi-specific repositories is expected to diminish over time -- by the time that Fedora 19 is released (May 2012), the Raspberry Pi repositories should hopefully contain mot much more than the VideoCore libraries and headers. (If these were ever to become licensed these under an OSI-approved license then the need for a Remix will be eliminated, and the Raspberry Pi could be directly supported as a Fedora target)."

     

    Aside from the mistake in the date, May 2012 should be May 2013 (or later),

    has the number of Pi-specific packages diminished over time as expected?

    Do you still expect F19 to contain "mot [sic] much more than VideoCore libraries

    and headers"?

     

    With the opensourcing of the all the ARM-based libraries and headers,

    is there still a need for a Remix?

     

    The same wiki section also says:

     

    "The future of the Remix is closely tied to the plans of the Fedora ARM project. By the release of Fedora 20 in November 2013, the ARM architecture will hopefully be promoted to Primary Architecture status, meaning that the ARM release will be done in lock-step with the x86 PC release."

     

    How have the plans for the F19 RPi Remix been affected by Fedora ARM dropping

    support for pre-v7 versions of ARM?

    Are you still expecting Fedora 20 to include RPi as a primary architecture?