Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Windows C/C++ Cross Compilation Toolchain for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 711 subscribers
  • Views 5815 views
  • Users 0 members are here
  • research
  • raspberry
  • raspberry_pi
  • raspberrypi
Related

Windows C/C++ Cross Compilation Toolchain for Raspberry Pi

e14 Contributor
e14 Contributor over 13 years ago

Hi everyone, I am trying to compile my C/C++ project from Windows 7 machine, and use Eclipse Juno GDB to remote debug the application on RPi. So far I do not have any luck on getting the Toolchains to work correctly. Appreciate if you can share any gnu ARM toolchain for Windows 7. Alternatively, you may suggest me of any good C/C++ development solution for RPi, which will work right-out-of-the-box. Thank you.

 

Cheers,

Bryan

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    I've had good luck with CodeSourcery's (now part of Mentor Graphics) "Sourcery C++ Lite 2011.03-41 for ARM GNU/Linux".  I think this is the current Sourcery Lite page, but it's been a while since I downloaded 2011.03-41.  The Lite edition is free-as-in-beer and liberates you from dealing with a GUI by sticking to the command line as Thompson and Ritchie intended.  image

     

    Some specifics:

     

    1.  I only use Sourcery Lite for BeagleBoard/Bone, but it ought to work for RasPi by specifying ARMv6 instead of ARMv7.

     

    2.  I currently run Sourcery Lite on an Ubuntu GNU/Linux machine, so there's no nonsense with having to deal with Windows file names and paths.

     

    3.  I have run Sourcery Lite on a Windows 2000 machine under Cygwin, which gives me "make" (not included with Sourcery Lite) and Unix tools such as "diff", "grep", and "sed".  However, I did have to play some tricks to make this work: BeagleBoard FAQs.

     

    You might also check the "ARM Compilers" page at eLinux.org.

     

    I've found it easiest to program RasPi in C on the machine itself.  I think this is called "happy compiling" instead of "cross compiling".  The standard Debian-based releases come with gcc (already configured for ARM) as well as the Unix command-line tools you need.  Sure, it's a little slow (probably mostly because I'm still running Debian "Squeeze" and I believe the SD card driver has improved a lot since then) but that encourages you to write small, efficient programs image

     

    [Edit: you might also try going to http://www.raspberrypi.org/ and entering "cross compiling" in the Google search box on the home page.]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Hi John,

     

      I have tried Sourcery Code Bench Lite for ARM EABI to create a simple C++ Hellow World program. The compiler complaint of not finding the _start and other symbols as well.

     

      Here is the compilation messages,

     

    make all

    Building file: ../src/hellow.cpp

    Invoking: Cross G++ Compiler

    arm-none-eabi-g++ -mfpu=vfp -mfloat-abi=hard -march=armv6zk -mtune=arm1176jzf-s -mfpu=vfp -mfloat-abi=softfp -O3 -g3 -Wall -c -fmessage-length=0 -MMD -MP -MF"src/hellow.d" -MT"src/hellow.d" -o "src/hellow.o" "../src/hellow.cpp"

    Finished building: ../src/hellow.cpp

     

    Building target: hellow

    Invoking: Cross G++ Linker

    arm-none-eabi-g++ --verbose  -o "hellow"  ./src/hellow.o  

    Using built-in specs.

    COLLECT_GCC=d:\tools\Sourcery_CodeBench_Lite_for_ARM_EABI\bin\arm-none-eabi-g++.exe

    COLLECT_LTO_WRAPPER=d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/arm-none-eabi/4.7.3/lto-wrapper.exe

    Target: arm-none-eabi

    Configured with: /scratch/jbrown/2013.05-arm-eabi-release/src/gcc-4.7-2013.05/configure --build=i686-pc-linux-gnu --host=i686-mingw32 --target=arm-none-eabi --enable-threads --disable-libmudflap --disable-libssp --disable-libstdcxx-pch --enable-extra-sgxxlite-multilibs --with-gnu-as --with-gnu-ld --with-specs='%{save-temps: -fverbose-asm} -D__CS_SOURCERYGXX_MAJ__=2013 -D__CS_SOURCERYGXX_MIN__=5 -D__CS_SOURCERYGXX_REV__=23 %{O2:%{!fno-remove-local-statics: -fremove-local-statics}} %{O*:%{O|O0|O1|O2|Os:;:%{!fno-remove-local-statics: -fremove-local-statics}}}' --enable-languages=c,c++ --disable-shared --enable-lto --with-newlib --with-pkgversion='Sourcery CodeBench Lite 2013.05-23' --with-bugurl=https://sourcery.mentor.com/GNUToolchain/ --disable-nls --prefix=/opt/codesourcery --with-headers=yes --with-sysroot=/opt/codesourcery/arm-none-eabi --with-build-sysroot=/scratch/jbrown/2013.05-arm-eabi-release/install/host-i686-mingw32/arm-none-eabi --with-libiconv-prefix=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-gmp=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-mpfr=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-mpc=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-ppl=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-host-libstdcxx='-static-libgcc -Wl,-Bstatic,-lstdc++,-Bdynamic -lm' --with-cloog=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-libelf=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --disable-libgomp --disable-libitm --enable-poison-system-directories --with-build-time-tools=/scratch/jbrown/2013.05-arm-eabi-release/obj/tools-i686-pc-linux-gnu-2013.05-23-arm-none-eabi-i686-mingw32/arm-none-eabi/bin --with-build-time-tools=/scratch/jbrown/2013.05-arm-eabi-release/obj/tools-i686-pc-linux-gnu-2013.05-23-arm-none-eabi-i686-mingw32/arm-none-eabi/bin

    Thread model: single

    gcc version 4.7.3 (Sourcery CodeBench Lite 2013.05-23)

    COMPILER_PATH=d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/arm-none-eabi/4.7.3/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/

    LIBRARY_PATH=d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../arm-none-eabi/lib/

    COLLECT_GCC_OPTIONS='-v' '-o' 'hellow' '-D' '__CS_SOURCERYGXX_MAJ__=2013' '-D' '__CS_SOURCERYGXX_MIN__=5' '-D' '__CS_SOURCERYGXX_REV__=23'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/arm-none-eabi/4.7.3/collect2.exe --sysroot=d:\tools\sourcery_codebench_lite_for_arm_eabi\bin\../arm-none-eabi -X -o hellow d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crti.o d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crtbegin.o -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3 -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../arm-none-eabi/lib ./src/hellow.o -lstdc++ -lm --start-group -lgcc -lc --end-group d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crtend.o d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crtn.o

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: warning: cannot find entry symbol _start; defaulting to 00008018

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-abort.o): In function `abort':

    abort.c:(.text+0x10): undefined reference to `_exit'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-fstatr.o): In function `_fstat_r':

    fstatr.c:(.text+0x1c): undefined reference to `_fstat'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-openr.o): In function `_open_r':

    openr.c:(.text+0x20): undefined reference to `_open'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-sbrkr.o): In function `_sbrk_r':

    sbrkr.c:(.text+0x18): undefined reference to `_sbrk'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-signalr.o): In function `_kill_r':

    signalr.c:(.text+0x1c): undefined reference to `_kill'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-signalr.o): In function `_getpid_r':

    signalr.c:(.text+0x44): undefined reference to `_getpid'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-writer.o): In function `_write_r':

    writer.c:(.text+0x20): undefined reference to `_write'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-closer.o): In function `_close_r':

    closer.c:(.text+0x18): undefined reference to `_close'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-isattyr.o): In function `_isatty_r':

    isattyr.c:(.text+0x18): undefined reference to `_isatty'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-lseekr.o): In function `_lseek_r':

    lseekr.c:(.text+0x20): undefined reference to `_lseek'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-readr.o): In function `_read_r':

    readr.c:(.text+0x20): undefined reference to `_read'

    collect2.exe: error: ld returned 1 exit status

    make: *** [hellow] Error 1

     

    09:06:10 Build Finished (took 3s.981ms)

     

       Similarly in building a C Hello World project.

     

       It would be helpful if you can give a pointer here. Thank you John.

     

    Cheers,

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Hi John,

     

      I have tried Sourcery Code Bench Lite for ARM EABI to create a simple C++ Hellow World program. The compiler complaint of not finding the _start and other symbols as well.

     

      Here is the compilation messages,

     

    make all

    Building file: ../src/hellow.cpp

    Invoking: Cross G++ Compiler

    arm-none-eabi-g++ -mfpu=vfp -mfloat-abi=hard -march=armv6zk -mtune=arm1176jzf-s -mfpu=vfp -mfloat-abi=softfp -O3 -g3 -Wall -c -fmessage-length=0 -MMD -MP -MF"src/hellow.d" -MT"src/hellow.d" -o "src/hellow.o" "../src/hellow.cpp"

    Finished building: ../src/hellow.cpp

     

    Building target: hellow

    Invoking: Cross G++ Linker

    arm-none-eabi-g++ --verbose  -o "hellow"  ./src/hellow.o  

    Using built-in specs.

    COLLECT_GCC=d:\tools\Sourcery_CodeBench_Lite_for_ARM_EABI\bin\arm-none-eabi-g++.exe

    COLLECT_LTO_WRAPPER=d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/arm-none-eabi/4.7.3/lto-wrapper.exe

    Target: arm-none-eabi

    Configured with: /scratch/jbrown/2013.05-arm-eabi-release/src/gcc-4.7-2013.05/configure --build=i686-pc-linux-gnu --host=i686-mingw32 --target=arm-none-eabi --enable-threads --disable-libmudflap --disable-libssp --disable-libstdcxx-pch --enable-extra-sgxxlite-multilibs --with-gnu-as --with-gnu-ld --with-specs='%{save-temps: -fverbose-asm} -D__CS_SOURCERYGXX_MAJ__=2013 -D__CS_SOURCERYGXX_MIN__=5 -D__CS_SOURCERYGXX_REV__=23 %{O2:%{!fno-remove-local-statics: -fremove-local-statics}} %{O*:%{O|O0|O1|O2|Os:;:%{!fno-remove-local-statics: -fremove-local-statics}}}' --enable-languages=c,c++ --disable-shared --enable-lto --with-newlib --with-pkgversion='Sourcery CodeBench Lite 2013.05-23' --with-bugurl=https://sourcery.mentor.com/GNUToolchain/ --disable-nls --prefix=/opt/codesourcery --with-headers=yes --with-sysroot=/opt/codesourcery/arm-none-eabi --with-build-sysroot=/scratch/jbrown/2013.05-arm-eabi-release/install/host-i686-mingw32/arm-none-eabi --with-libiconv-prefix=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-gmp=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-mpfr=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-mpc=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-ppl=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-host-libstdcxx='-static-libgcc -Wl,-Bstatic,-lstdc++,-Bdynamic -lm' --with-cloog=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --with-libelf=/scratch/jbrown/2013.05-arm-eabi-release/obj/pkg-2013.05-23-arm-none-eabi/arm-2013.05-23-arm-none-eabi.extras/host-libs-i686-mingw32/usr --disable-libgomp --disable-libitm --enable-poison-system-directories --with-build-time-tools=/scratch/jbrown/2013.05-arm-eabi-release/obj/tools-i686-pc-linux-gnu-2013.05-23-arm-none-eabi-i686-mingw32/arm-none-eabi/bin --with-build-time-tools=/scratch/jbrown/2013.05-arm-eabi-release/obj/tools-i686-pc-linux-gnu-2013.05-23-arm-none-eabi-i686-mingw32/arm-none-eabi/bin

    Thread model: single

    gcc version 4.7.3 (Sourcery CodeBench Lite 2013.05-23)

    COMPILER_PATH=d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/arm-none-eabi/4.7.3/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/

    LIBRARY_PATH=d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/;d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../arm-none-eabi/lib/

    COLLECT_GCC_OPTIONS='-v' '-o' 'hellow' '-D' '__CS_SOURCERYGXX_MAJ__=2013' '-D' '__CS_SOURCERYGXX_MIN__=5' '-D' '__CS_SOURCERYGXX_REV__=23'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../libexec/gcc/arm-none-eabi/4.7.3/collect2.exe --sysroot=d:\tools\sourcery_codebench_lite_for_arm_eabi\bin\../arm-none-eabi -X -o hellow d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crti.o d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crtbegin.o -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3 -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib -Ld:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../arm-none-eabi/lib ./src/hellow.o -lstdc++ -lm --start-group -lgcc -lc --end-group d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crtend.o d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/crtn.o

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: warning: cannot find entry symbol _start; defaulting to 00008018

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-abort.o): In function `abort':

    abort.c:(.text+0x10): undefined reference to `_exit'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-fstatr.o): In function `_fstat_r':

    fstatr.c:(.text+0x1c): undefined reference to `_fstat'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-openr.o): In function `_open_r':

    openr.c:(.text+0x20): undefined reference to `_open'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-sbrkr.o): In function `_sbrk_r':

    sbrkr.c:(.text+0x18): undefined reference to `_sbrk'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-signalr.o): In function `_kill_r':

    signalr.c:(.text+0x1c): undefined reference to `_kill'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-signalr.o): In function `_getpid_r':

    signalr.c:(.text+0x44): undefined reference to `_getpid'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-writer.o): In function `_write_r':

    writer.c:(.text+0x20): undefined reference to `_write'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-closer.o): In function `_close_r':

    closer.c:(.text+0x18): undefined reference to `_close'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-isattyr.o): In function `_isatty_r':

    isattyr.c:(.text+0x18): undefined reference to `_isatty'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-lseekr.o): In function `_lseek_r':

    lseekr.c:(.text+0x20): undefined reference to `_lseek'

    d:/tools/sourcery_codebench_lite_for_arm_eabi/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib\libc.a(lib_a-readr.o): In function `_read_r':

    readr.c:(.text+0x20): undefined reference to `_read'

    collect2.exe: error: ld returned 1 exit status

    make: *** [hellow] Error 1

     

    09:06:10 Build Finished (took 3s.981ms)

     

       Similarly in building a C Hello World project.

     

       It would be helpful if you can give a pointer here. Thank you John.

     

    Cheers,

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mconners
    mconners over 13 years ago in reply to e14 Contributor

    Part of your problem is that you are using the baremetal version of GCC. The arm-none- basically means that there is no os support.

     

    You probably want to find arm-linux-gnueabi or something like that.

     

    I haven't done it under windows, but I have under linux.

     

    When developing on the pi I use vi and the command line as John says like Thompson and Ritchie intended.

     

    Good luck, I'm sure you can get the arm-linux for windows, and get some version of eclipse to work for you if you really must compile on pi.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to mconners

    Michael Conners wrote:

     

    Part of your problem is that you are using the baremetal version of GCC. The arm-none- basically means that there is no os support.

     

    You probably want to find arm-linux-gnueabi or something like that.

    Yes, the CodeSourcery version I use is "arm-none-linux-gnueabi".  Its gcc command is "arm-none-linux-gnueabi-gcc".