Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Running indexedDB (or pouchDB, or couchDB) on the Raspberry Pi???
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 705 subscribers
  • Views 667 views
  • Users 0 members are here
  • webserver
  • help
  • pouchdb
  • raspberrypi
  • urgent
  • rpi
Related

Running indexedDB (or pouchDB, or couchDB) on the Raspberry Pi???

wallarug
wallarug over 13 years ago

Hey Guys!

 

I need some help with a project that I am trying to get up and running using HTML5 and Javascript as the main vehicle!

 

BUT, as always, there is a problem.

 

I have been following a tutorial on the official “pouchDB” documentation but without success.  http://pouchdb.com/getting-started.html

 

I can copy and paste code easily but there seems to be a problem with the whole thing. 

 

Step 1: Ok… NOTE: Instead of running the python server as they have I am running apache2 (which works).

 

Step 2: Ok… But I am using a local version (as suggested) of pouchdb-nightly.js

 

Steps 3 – 7:  Ok … they are just copying code.

 

Step 8: Installing CouchDB. For this step I ran (on the Pi) apt-get install couchdb  which worked fine and installed properly.

 

Step 9:  Enable CORS … This is where it seems to have fallen apart. I ran the command many times last night and it failed every time with either: “Curl error(7)” or “Server Error”.

 

 

This morning I decided to change the file /etc/couchdb/local.ini (as described by this link: http://bell-dev.blogspot.com.au/2012/12/installing-couchdb-on-raspberry-pi.html?q=couchdb) so that the

bind_address=192.168.*.* (stars replacing internal network IP address).  This worked and I managed to run all the commands except the last one:

'"accept, authorization, content-type, origin"'

 

This could just be me not knowing what to do.

 

Anyway, I have no idea why the app just does nothing.  Can someone please help me out?

 

The webserver is running here:  http://cmdlab.zapto.org:81/ with couch DB services running here:  http://cmdlab.zapto.org:5984/

  • Sign in to reply
  • Cancel
  • wallarug
    wallarug over 13 years ago

    Sorry,  Server is offline at the moment.  I will turn it on at 2:30pm AEST

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to wallarug

    Server back online!  Pi over-heated in Pibow!

     

    NOTE: Pi Overheats in the Pibow.  Do not run a webserver through the Pi while in the Pibow!