Hi There,
anybody knows where I can find the FCC Part 15 Test report and certification documents for the Raspberry Pi Model A and B ?
Thanks & Regards
Jorge
Hi There,
anybody knows where I can find the FCC Part 15 Test report and certification documents for the Raspberry Pi Model A and B ?
Thanks & Regards
Jorge
If so, can't we just ask, point blank?
Yes, I have asked. The answer was:
So, Class A is all that RPi were aiming for.
It passed quite comfortably and, add to that, FCC, C-tick, REACH SVHC and RoHS compliance testing
the board is in a much better place than it potentially was.
Best wishes
Gary
Nobody seems to be able or willing to confirm if the Raspberry Pi has passed a Class B certification with the FCC and provide access to the appropriate test reports and certification documents.
It is not a matter if it may interfere with your TV or radio but as I said before an issue of liabilities.
A school district will have a hard time to approve a non-certified device that may interfere with among others devices, for example a medical device like a pacemaker, even if there is no chance for anything wrong to happen.
Premier Farnell's answer to code27 appears to describe the situation very authoritatively:
Gary Nevison wrote:
The board underwent EMC testing which enables one to discern if it should be classed as A or B. From the RPi pre-compliance work it was evident that it would not meet Class B. It did not meet the Class B limit but did meet, and comply with Class A. It is legal to place Class A equipment on the market for use in a domestic environment in both the EU and U.S. and to affix the CE and FCC mark provided that there is a warning on the product that it may cause interference. In the case of RPi the warning is on the Safety Data Sheet (a copy of this can be found on the Raspberry Pi area of element14.
That seems totally clear. The Pi board in question (which revision?) was Class A certified only. That was in April 2012 and things may have changed since then, but at least there can be no doubt about that specific Model B.
This Raspberry Pi Safety Data Sheet is probably the one mentioned by Gary. Note that it's dated 19th April 2012.
A school district will have a hard time to approve a non-certified device ...
A school district doesn't actually need to worry too much about the reasons for
the laws, such as pacemaker or TV interference, because in addition to the
manufacture, import, or sales of non-compliant devices being prohibited,
the "use" of such devices is also prohibited. See for example paragraph 6 of
the Hobby Lobby citation:
http://hraunfoss.fcc.gov/edocs_public/attachmatch/DA-10-2220A1.pdf
That seems totally clear. The Pi board in question (which revision?) was Class A certified only. That was in April 2012 and things may have changed since then, but at least there can be no doubt about that specific Model B.
Actually this part is as clear as mud:
It is legal to place Class A equipment on the market for use in a domestic environment in both the EU and U.S. and to affix the CE and FCC mark provided that there is a warning on the product that it may cause interference. In the case of RPi the warning is on the Safety Data Sheet (a copy of this can be found on the Raspberry Pi area of element14.
How could it possibly be true that simply supplying a warning that the product may cause interference
would be of any value whatsoever in eliminating the requirement that Class B devices be tested to
Class B standards. That warning is required of all devices, whether Class A or B, and there is no
reason to believe it has magic powers in eliminating the need for Class B certification.
Gary said he would provide some authorities for that claim, but he never did, and I'm not
holding my breath.
That FCC document that coder27 linked, "UNDERSTANDING THE FCC REGULATIONS FOR COMPUTERS AND OTHER DIGITAL DEVICES", is certainly explicit:
On pages 8-9, FCC writes:
What is the difference between a Class A and Class B digital device?
If a digital device will be sold to anyone who is likely to use it in a residential
environment then it is a Class B digital device. When determining whether a particular
device should be classified as Class A or Class B, the Commission normally considers
the following three questions, in this order:
Is the marketing of the device restricted in such a manner that it is not sold to residential users?
If a digital device is sold or offered for sale to any residential users (including
commercial or industrial companies that could employ the equipment in a residential
environment) then it is a Class B digital device regardless of its price or application.
Marketing through a general retail outlet or by mail order to the general public with a
simple disclaimer, such as "For Business Use Only," is not sufficient to qualify as
Class A. Instead, all marketing (advertising, sale and distribution) must be restricted
by the marketer to users in a commercial, industrial, or business environment.
Does the application for which the device is designed generally preclude operation in residential areas?
For example, mainframe computer systems have generally been considered Class A
digital devices because it is highly unlikely that they would be used in residential
environments.
Is the price of the device high enough that there is little likelihood that it would be used in a residential environment, including a home business?
The merits of classifying a digital device as Class A based on its price are reviewed on
a case-by-case basis. This is because, for example, the price threshold for an I/O card
will be different than the price threshold for a computer system configuration.
Portable computers, because they are designed to be used anywhere, are considered
Class B devices regardless of their price or restrictions placed on marketing. Only in
those cases where the designed application precludes the possibility of operation in a
residential environment may portable computers be qualified as Class A devices.
What happens if one sells or imports non-compliant digital devices?
As explained earlier, the form of authorization that is required for a digital device
depends on how the device will be marketed. The FCC rules are designed to control
the marketing of digital devices and, to a lesser extent, their use. If someone purchases
a non-compliant digital device, uses it, causes interference to authorized radio
communications, and is the subject of an FCC interference investigation, the user will
be told to stop operating the device until the interference problem is corrected.
However, the person (or company) that sold this non-compliant digital device to the
user has violated the FCC marketing rules in Part 2 as well as federal law and may be
subject to an enforcement action by the Commission's Field Operations Bureau that
could result in one or more of the following:
-- forfeiture of all non-compliant equipment
-- $100,000/$200,000 criminal penalty for an individual/organization
-- a criminal fine totalling twice the gross gain obtained from sales of the non-compliant equipment
-- an administrative fine totalling $10,000/day per violation.
It is the act of selling or leasing, offering to sell or lease, or importing a digital device
that has not gone through the appropriate FCC equipment authorization procedure that
is a violation of the Commission's rules and federal law.
Yikes!
If I understand the above correctly, product classification into class A or B is not a vendor option. A product falls into one class or another depending on who is expected to buy it, and the duty then falls upon the vendor to obtain the appropriate certification, otherwise apparently it's in violation of FCC rules and federal law. Is there any other way of understanding the above FCC statements?
NOTES and REFERENCES.
I think you unintentionally removed the emphasis on "any" and "portable computers".
Morgaine Dinova wrote:
That seems totally clear. The Pi board in question (which revision?) was Class A certified only. That was in April 2012 and things may have changed since then, but at least there can be no doubt about that specific Model B.
This Raspberry Pi Safety Data Sheet is probably the one mentioned by Gary. Note that it's dated 19th April 2012.
Then they should have no problem telling who, how, when, what, where made the tests and post publically as the Beaglebone guys did, the test reports.
There is no tops secret or trade information on those reports, just a detail of what test have been performed and if the device passed or failed the test.
Thanks for the headsup. All emphases in the original were lost because I imported those paragraphs via a text file to avoid direct pasting into the forum editor, since that causes all kinds of literary fireworks. I'd better go back and reinsert them manually, since it's an official document.
DONE, I've put the missing emphases back. I see why you mentioned it --- the paragraph about Portable computers is very specific:
Portable computers, because they are designed to be used anywhere, are considered
Class B devices regardless of their price or restrictions placed on marketing. Only in
those cases where the designed application precludes the possibility of operation in a
residential environment may portable computers be qualified as Class A devices.
Based on the above FCC document, the situation doesn't look too good, to put it mildly.
There's not much that can be done on the weekend, but perhaps good advice for Monday morning at Element14 is to begin the first steps towards Class B certification. If that requires Pi board redesign, so be it, the result will be a better board.