http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=53410&start=84
The prosecution rests. For now.
is there a thread or source why it failed compliance, and what standards were used to determine?
i would like to look into this a little more.
See Pete Lomas's blog here:
we have some definite options for ripping 10db or more off the key gremlin frequencies. Before you ask, yes, this should be enough.
and my unanswered question:
Are you trying to meet the Class A industrial standard, or Class B residential?
Similarly:
http://www.element14.com/community/people/PeteL/blog/2012/04/07/certification-testing--update
Jonathan Garrish wrote:
The prosecution rests. For now.
I sure hope that the message Element14 received was not about prosecution but about preventing bad things from happening before they happen. After all this analysis of the regulatory situation perhaps we can rest, but Element14 cannot. They have an official group-wide Code of Ethics to adhere to, so I'm sure they are taking the matter seriously now that they have been alerted to the problem.
Every single stakeholder in the Pi ecosystem is at risk (in different ways) because of this certification error, from suppliers to importers, distributors, retailers, users operating unintentionally radiating devices without knowing it, and other people in the residential vicinity of those devices who could be affected by them. There is a very good reason for requiring residential certification, it's not just a pointless burden on manufacturing. It's to prevent bad things from happening, a part of engineering and social responsibility.
Alas, there is still no acknowledgement of this week's advice in Feedback & Support on this matter.
There are some bits here and there but nothing conclusive or detailed ...
This is one of the classic ones were we get but don't get some information ...
http://www.raspberrypi.org/archives/978
Pay attention that at that time they realize the even when "at the Foundation call the computer a Raspberry Pi in conversation" "This thing’s called a Raspberry Pi, not a Raspberry Pi computer"
So we (they) call it a computer but is it not.... ohhh right now is a "linux box"
But first line on "About us" ...
"The idea behind a tiny and cheap computer for kids came in 2006"
So it is or it is not a computer ? ... perhaps Shakespeare can provide some light into this identity crisis.
On thing that they really missed big on the entire strategy and inspiration, is the context in the days of the BBC Micro and such.
-J
jamodio wrote:
There are some bits here and there but nothing conclusive or detailed ...
This is one of the classic ones were we get but don't get some information ...
http://www.raspberrypi.org/archives/978
Pay attention that at that time they realize the even when "at the Foundation call the computer a Raspberry Pi in conversation" "This thing’s called a Raspberry Pi, not a Raspberry Pi computer"
So we (they) call it a computer but is it not.... ohhh right now is a "linux box"
But first line on "About us" ...
"The idea behind a tiny and cheap computer for kids came in 2006"
So it is or it is not a computer ? ... perhaps Shakespeare can provide some light into this identity crisis.
On thing that they really missed big on the entire strategy and inspiration, is the context in the days of the BBC Micro and such.
-J
Indeed - the road to a lucrative career in Law is paved with semantics.
Regarding Pete Lomas' blog - I see he's not even logged into his account here since October 2012.
Morgaine - obviously "getting the paperwork done right" is a given - especially considering the inordinate amount of time that the RPF have spent promoting their product Stateside. It all just makes no sense as there is absolutely nothing to be gained, but a lot to be lost by not getting the relevant certifications
Indeed - the road to a lucrative career in Law is paved with semantics.
So how many semantic issues do you detect in the opening line of
Eben's March 2013 pycon keynote speach:
[Eben]: Thankyou guys. So, my name is Eben Upton, I run a thing based in the UK called the Raspberry Pi Foundation. Ah, we make little computers for kids.
coder27 wrote:
Indeed - the road to a lucrative career in Law is paved with semantics.
So how many semantic issues do you detect in the opening line of
Eben's March 2013 pycon keynote speach:
[Eben]: Thankyou guys. So, my name is Eben Upton, I run a thing based in the UK called the Raspberry Pi Foundation. Ah, we make little computers for kids.
I'd say that in my opinion that opening sentence was explicit and not open to misinterpretation by any reasonable person.
#1) He's still leaning on the Foundation for promotional purposes, rather than on Raspberry Pi (Trading) Ltd - of which he is listed as a director.
#2) He's promoting his organisation's consumer product. Computers, if I'm not mistaken.
Being a portable computer by the FCC definition would automatically define Pi as a Class B device.
Note however that it's captured as a Class B device anyway, even without the above, because if falls foul of the FCC's three key questions that distinguish between devices of the two classes:
Since it fails to be excluded from the residential environment through restricted marketing and sales (point 1), and it cannot avail itself of the exemptions in points 2 and 3, by FCC rules it is a Class B device anyway, even if someone could retrospectively wish away the fact that it is clearly a portable computer.
A Class B device without Class B certification is uncertified for its expected use, and cannot be marketed or offered for sale to residential users. If it has Class A certification then it can be marketed or offered for sale as a restricted commercial or industrial device, but that is not how Pi has been marketed and offered for sale, as anyone can plainly see.
So you would say "I run a thing based in the UK called the RPF, but not officially; we make little computers, but officially just motherboards; it's for kids, but not officially for kids in residential areas."
The 2013 Premier Farnell annual report shows the target audience as "engineers and hobbyists".
Raspberry Pi
The element14 Community played a key role in another very successful
product launch this year. The Raspberry Pi, the credit card sized computer
developed to put computer programming back at the heart of engineers,
launched to phenomenal interest from engineers and hobbyists alike. In the
first 15 minutes after launch our websites received over ½ million hits as
customers flocked to order from us and by January 2013, Premier Farnell
had sold 600,000 Raspberry Pi units.
The "educational focus" appears to have come at least in part, from David Braben. Liz wrote:
David was one of the people Eben brought the original idea to, along with the other trustees and a few others who aren't trustees. He's helped us develop the educational focus behind it, ...
http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=319&start=20