Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum My lovely RaspberryPi is dead...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 57 replies
  • Subscribers 716 subscribers
  • Views 7752 views
  • Users 0 members are here
  • raspberry_pi
  • no_tv_image
  • not
  • booting
Related

My lovely RaspberryPi is dead...

e14 Contributor
e14 Contributor over 12 years ago

I was so looking forward to it and I was pleasantly surprised how the  RaspBMC from the NOOBS package worked, I have even bought a wireless  keyboard for it ( http://www.totalhtpc.com/logitech-k400r-wireless-touch-keyboard-review/ ) but...

 

The problem started about a week ago, when I had to unplug  everything to get the image going, as it was all stuck. Several reboots  and it started working again but all that unplugging and plugging it  back again - maybe it was the electricity somehow damaging some of the  HDMI/composite circuitry?

 

I can see  that it is powered up (there is red light inside) but neither HDMI, not  Composite cables give me any image whatsoever, on the TV.

 

I  have reformatted and copied the NOOBS files to the SD card, as  described on your pages - but I get no system booting in any way. Not a  flicker of an image on my TV.

 

The SD card seems OK, as I have dealt with it in my laptop without a problem.

 

I also tried other OSs, like RaspBMC alone, as well as OpenELEC. Alas, to no avail. The same applies.

 

I have tried different ports and different cables. Not a squeak.

 

Therefore, I must conclude it is the HW that is faulty.

 

Please, instruct me how to return the Pi to you.

 

A refund is preferable to "repair and return", at this point. No response from "sales" at Fernell, sadly... Just forwarded it to the other email...

 

========================================

 

In addition, I hope this might help a bit...

 

I  have read that Pi  might be susceptible to varying voltage/electricity problems. I have a  Belkin safety multiple extension cord, with serious protection against  electricity surges. So, can it still be an electrical mishap?

 

Or is it simply the power supply issue, as some here have suggested, in which case we would need a really good one, properly advertised here and on sales website...

 

May  I also suggest a ON/OFF switch, as a good idea, which may go  a certain  way towards preventing this from occurring. I understand that it only  uses very little electricity but I think this is beside the point.  Sometimes my NAS would not go to "Standby" mode after 10 minutes as I  set it up because it seems that RaspBMC could have been queering it?

 

Not  sure what exactly went wrong but I can see quite clearly that both HW  and SW improvements are possible. I would urge you to contact the patent  holders ASAP, in order to make the Mark III...

 

Best regards,

 

gorski

 

P.S. Anyone with multiple HDMI switches experience? I have this one in my mind: http://www.amazon.it/Ligawo-%C2%AE-switch-attivo-automaticamente/dp/B002I9LH2Q/ref=sr_1_1?ie=UTF8&qid=1382270091&sr=8-1&keywords=ligawo+5x1

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    D_Hersey over 12 years ago

                      X                            X  

    X  X         X   X                        X   X                                                             XXXXXXXXX          X  X

      X  X       X     X                     X      X                                                            X            X            X  X

    XXXXXXXX        X       XXXXXXXX       X        XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

      X  X               X     X                     X     X           X                        X              X            X            X  X

    X  X                  X   X                       X   X            X                        X              XXXXXXXXX          X  X

                             X                            X               X                        X

                                                                            X      X          X    X  

                                                                            X     X         X      X   

                                                                       XXXXXXX           XXXXXXXXX

                                                                      X   X X                    X X      X

                                                                     X   X   X                  X   X   X

                                                                        X      X                X     X

                                                                       X        X              X       X

                                                                     XXXXXXXXX          XXXXXXXX

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                       XXXXXXX            XXXXXXX

                                                                          XXX                    XXX

     

    image

    This is a super-Zener.  The industry hasn't been marketing power Zeners since my son was born.  I'm a grandpa.  Obviously this only apes the Zener in reverse breakdown mode, so this must be paralleled by the power Shottky.  BV(breakdown potential) is Vz+c. 0.6V, 1.2 for Darlington.

    Not all rpi setups are the same.  3.5W seems to be a max for the board alone, we could use 10W for our design-point, implying a flow of 2 Amperes.

    In an extreme stress event, this device only has to be robust (must be?) enough to live 'til the fuse rides to the rescue.  Moderate situations could have it warming up some without blowing (activating?) the fuse.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 12 years ago

                      X                            X  

    X  X         X   X                        X   X                                                             XXXXXXXXX          X  X

      X  X       X     X                     X      X                                                            X            X            X  X

    XXXXXXXX        X       XXXXXXXX       X        XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

      X  X               X     X                     X     X           X                        X              X            X            X  X

    X  X                  X   X                       X   X            X                        X              XXXXXXXXX          X  X

                             X                            X               X                        X

                                                                            X      X          X    X  

                                                                            X     X         X      X   

                                                                       XXXXXXX           XXXXXXXXX

                                                                      X   X X                    X X      X

                                                                     X   X   X                  X   X   X

                                                                        X      X                X     X

                                                                       X        X              X       X

                                                                     XXXXXXXXX          XXXXXXXX

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                            X                       X

                                                                       XXXXXXX            XXXXXXX

                                                                          XXX                    XXX

     

    image

    This is a super-Zener.  The industry hasn't been marketing power Zeners since my son was born.  I'm a grandpa.  Obviously this only apes the Zener in reverse breakdown mode, so this must be paralleled by the power Shottky.  BV(breakdown potential) is Vz+c. 0.6V, 1.2 for Darlington.

    Not all rpi setups are the same.  3.5W seems to be a max for the board alone, we could use 10W for our design-point, implying a flow of 2 Amperes.

    In an extreme stress event, this device only has to be robust (must be?) enough to live 'til the fuse rides to the rescue.  Moderate situations could have it warming up some without blowing (activating?) the fuse.