Raspberry Pi Forum I'd be giving the patents away...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 691 subscribers
  • Views 2489 views
  • Users 0 members are here
  • raspberry_pi
  • patents
Related

I'd be giving the patents away...

packetgeek
packetgeek over 12 years ago

A recent discussion, which appears to have (thankfully) been removed, involved a technology which was doubted by many.  Ignoring that it was inappropriate to advertise the thing an off-topic post, the thing that made me think that the tool was just more snake oil was the vendor's statement: "If I tell you everything you want to know,'I'd be giving the patents away!! and I cannot afford to do that."  If the author of that statement has a patent, then the information is already publicly available.  His statement makes me believe there is no patent and no actual working technology.

  • Sign in to reply
  • Cancel
Parents
  • R_Phoenix
    R_Phoenix over 12 years ago

    Thanks e14 for pulling those articles.

    I was able to read it when it was first posted and I had a good chuckle. While we have yet to understand all forms of energy exchange and the efficiency of most applications can be much improved on - there is no such thing as "free energy".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to R_Phoenix

    I believed that the Sun and Wind are "Free Energy"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to packetgeek

    Of course you are allowed to have an opinion - no-one (as far as I know)  disputes that.

    What I was trying to point out is that it is better to discuss (and disprove) things rather than to pull posts.

    If the OP won't provide  a dongle for actual measurement it's hard to take his device at all seriously.

    I'm interested that many of the arguments presented against the device working rely on assertions rather than evidence or fact.

    For example - the device only has two connections, power and ground (which is clear from a photo) so it can't be affecting the laptop settings via USB.

     

    You suggest that there is some limit to conversion efficiency

     

    any energy conversion (mechanical to electrical, electrical to RF,

    electrical to chemical, etc.) is at best 80% efficient.

     

    but this just isn't true and there is no physical reason why it should be. (and in the spirit of scientific reasoning which I am defending, here is some evidence to back up my assertion : http://www.csiro.au/solutions/psz7)

     

    Just for the record I don't think, (on the basis of casual application of 2nd Law of Thermodynamics and some of the circumstantial evidence) that it will work.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Guessing: the comparison involves different loads on the motor (i.e.,

    comparing one output to the other).  My statement applied to conversions

    between different forms of energy.  I'll withhold any further comment on

    the topic as we're just chasing each others tails with this discussion.

    I'd rather get back to experimenting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to packetgeek

    Sometimes it's hard to let the other guy have the last word image

     

    But motor efficiency (in the context of the link I provided) is mechanical power out/ electrical power in.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett

    But motor efficiency (in the context of the link I provided) is mechanical power out/ electrical power in.

    Funny I was thinking the same thing.

     

    In the case of this device, it isn't converting energy from its electrical state, and I do know of DC to DC converts in the high 90's% of efficiency.

     

    Test challenge

    I still haven't heard back, and obviously there would be no cost to the testers, otherwise its not fair.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to mcb1

    DC/DC is still from electrical to electrical; although applicable in the context of the product discussed, I think packetgeek meant conversion from one domain to the other.  Anyway, he's wrong as ThinGap claims 95% efficiency: http://www.thingap.com/efficiency-and-smoothness/ and the CSIRO motors have way more efficiency than 80%.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to mcb1

    mcb1 wrote:

    ... and I do know of DC to DC converts in the high 90's% of efficiency.

     

    Right. That's marketing-speak. In general DCDC converters convert at "around 80%" efficiency. Then when you sweep the output current along the whole range, at one point you may measure "above 90%" efficiency. The marketing guys jump on this number and prominently place it everywhere they can. In reality, count on 80% and let yourself be surprised if possible.

     

    The "80%" mentioned is a good ballpark figure. There are exceptions. Gas-powered central heating installations here in the Netherlands apparently achieve 107% efficiency according to the official efficiency-calculating-rules. If you WANT to go from electrical power to heat, that can easily be done with 100% efficiency.

     

    On the other hand, going from chemical (gas) to mechanical power (moving car), you are lucky if you hit the 30%.

     

    As another example of how "ballpark figures" work I use "0.8" as the density of "organic materials". Wood, gasonline, etc. I know there are woods that are so dense that they sink (i.e. >1.0). But as a ballpark figure this 0.8 still works quite well. (e.g. when they say an airplane had XXX kg of fuel on board).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to rew

    Gas-powered central heating installations here in the Netherlands apparently achieve 107% efficiency according to the official efficiency-calculating-rules. If you WANT to go from electrical power to heat, that can easily be done with 100% efficiency.

    That's because in the official rules (when efficinecy was much, much lower) they thought that the heat going through the chimney was neglectabe..... Now that that heat loss is reduced, you get more than 100% efficiency. It's more an calculation / definition error. 107% efficiency would mean you'd be generating energy more heat than is available in caloric energy in the gas...

     

    Then when you sweep the output current along the whole range, at one point you may measure "above 90%" efficiency

    Yes. And when your application permits, you can design to be in that sweet spot. So it's a marketing-overused, but not a lie.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to vsluiter

    It's not the "heat going through the chimney" that they neglected in the definition at first.

     

    It's the energy that is contained in the water-vapour that goes up the chimney that they neglected. That can be recovered if you make sure the water condenses and you can leave the resulting water somewhere (a drain).

     

    If you build a heat-pump, powered either by gas or by electricity, you can get even higher efficiency figures, well above 100%.

     

     

    P.S; I fully agree with you to call the 107% situation a "definition error".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to rew

    "I know there are woods that are so dense that they sink (i.e. >1.0). But as a ballpark figure this 0.8 still works quite well."

     

    More common than you might think - as is well known to my poor dog. In the woods where we walk about half the sticks I throw in the river for her to fetch turn out to be sinkers. I'm trying to improve my manual density measurement skills but so far to little avail.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Recommend doing the power conversion math using the cars specs

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Recommend doing the power conversion math using the cars specs

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 12 years ago in reply to packetgeek

    Perhaps you would like to explain your rather crytpic comment a little more - I can't see how the car spec would lead me to the efficiency of one of its components but I may have misunderstood you. From the link I gave you it is possible to get to the "motor information pack" which quotes the motor spec in some detail, extract follows:

     

    RMS phase current (A) 13.9

    Copper loss (W) 43.9

    Eddy current loss (W) 2.6

    Windage (W) 2.1

    Total loss (W) 48.6

    Output power (W) 1800

    Efficiency (%) 97.4

    Winding, temperature, rise (K) 22

     

    I offered this as evidence that practical devices can achieve conversion efficiencies from electrical to mechanical energy well in excess of 80%. If you doubt this source then Victor offered another one.

     

    MK