Raspberry Pi Forum Raspberry Pi NoIR camera board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 687 subscribers
  • Views 4158 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi NoIR camera board

Former Member
Former Member over 12 years ago

Hi,

 

This is my second attempt to get a PI camera working. After the first attempt I returned the camera on the assumption that it’s faulty. However I get the same results with this newly acquired camera.

Basically I get the following when I run the command:-

  pi@raspberrypi ~ $ raspistill -o image.jpg

   

          mmal: mmal_vc_component_create: failed to create component 'vc.ril.camera' (1:ENOMEM)

           mmal: mmal_component_create_core: could not create component 'vc.ril.camera' (1)

          mmal: Failed to create camera component

          mmal: main: Failed to create camera component

          mmal: Camera is not detected. Please check carefully the camera module is installed correctly

 

I have updated and upgraded the system. Set the raspi-config. Check and re-inserted the cables but to no avail.  I have run out of options and not sure what to do next.  Any suggestions?

 

PS: I have tried a new RPi mother board to eliminate the RPi unit but I get the same results.

Regards

 

AW

 

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • dkelley810
    dkelley810 over 10 years ago

    I was wondering if anyone knows. Does the NoIR camera work in the UV spectrum? Can I use UV LEDs. I have it working in IR.

     

    Thanks in Advance for any positive feedback.

     

    Dennis Kelley

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to dkelley810

    Most silicon cameras are sensitive to UV but much less than IR which is why they have IR cut filters and not UV ones.

    So you could use the LEDs, you'll probably need something in front that will block the optical and IR to give the UV a chance to dominate.

     

    Should make some cool pictures!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dkelley810
    dkelley810 over 10 years ago in reply to Problemchild

    I was thinking that I could build a full spectrum camera. Like what is used on ghost adventures. Does the NoIR camera have any filters?

    Thanks

     

    Sent from my iPhone

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dkelley810
    dkelley810 over 10 years ago in reply to Problemchild

    I was thinking that I could build a full spectrum camera. Like what is used on ghost adventures. Does the NoIR camera have any filters?

    Thanks

     

    Sent from my iPhone