Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum wifi direct on raspberrypi by using wipi adapter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 706 subscribers
  • Views 1147 views
  • Users 0 members are here
Related

wifi direct on raspberrypi by using wipi adapter

e14 Contributor
e14 Contributor over 11 years ago

hi ,

 

I have Raspberry pi 2 board and wi-pi adapter is with me. by using wipi adapter i can connect with wifi network.

now i need to do wi-fi direct feature.

i need to communicate  board by using wifi direct feature with another android phone.

how it is possible .It is an urgent query please help me.

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    balearicdynamics over 11 years ago

    Hello,

     

    first of all, about your query I suggest that you simply set Android WiFi as a WiFI access point then you connect the Raspberry to it. Then, if your Android has also the Bluetooth or 3G/4G connection active your Raspberry PI can also access to Internet, depending on the settings of your Android WiFi Direct.

     

    Second, please consider that the users that can answer to a query do this happily as a favour in a harmonised collaborative situation. So, if your query is urgent, be patient and wait that users give you a suggestion.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics

    I am trying to do something very similar to this, making wifi-direct work between a RPi and any wifi-direct enabled android device. I have tried to achieve this using  EDIMAX EW-7811Un and TP Link tl-wn725n on a RPi 2 model B but have had no luck by far. First problem I face is that I am not finding the device everytime, and when I do I am unable to discover services on the device found. I have been trying to develop this using Ubuntu 14.04 which has wpa_supplicant built in. I am running the utility wpa_cli to run all the commands. When I check the log, I get a timeout message everytime and the timeout period is 0.2 seconds by default, when I hacked into the code and changed the timeout interval, it resulted into erroneous outcome I could not comprehend.

    Seems like a dead-end to me but I believe that can't be. Would welcome any help/suggestion/insight/direction. I am neither experienced with networking nor with hardware and this is my first time working on the combination. So I am not sure that its a hardware/driver/configuration limitation or what. Everything I do is pure trial in the dark by following links and trying out stuff.

    Also, I tried to run the test suit for hostap. No luck there too.

    Please help if anyone can.

    Thanks..!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics

    I am trying to do something very similar to this, making wifi-direct work between a RPi and any wifi-direct enabled android device. I have tried to achieve this using  EDIMAX EW-7811Un and TP Link tl-wn725n on a RPi 2 model B but have had no luck by far. First problem I face is that I am not finding the device everytime, and when I do I am unable to discover services on the device found. I have been trying to develop this using Ubuntu 14.04 which has wpa_supplicant built in. I am running the utility wpa_cli to run all the commands. When I check the log, I get a timeout message everytime and the timeout period is 0.2 seconds by default, when I hacked into the code and changed the timeout interval, it resulted into erroneous outcome I could not comprehend.

    Seems like a dead-end to me but I believe that can't be. Would welcome any help/suggestion/insight/direction. I am neither experienced with networking nor with hardware and this is my first time working on the combination. So I am not sure that its a hardware/driver/configuration limitation or what. Everything I do is pure trial in the dark by following links and trying out stuff.

    Also, I tried to run the test suit for hostap. No luck there too.

    Please help if anyone can.

    Thanks..!