Help!!!! I have my pi up and running, but when it came to power off i thought it would be like a regular computer in which i selected the shut down option. now my pi will not turn on. how can i fix this?
Help!!!! I have my pi up and running, but when it came to power off i thought it would be like a regular computer in which i selected the shut down option. now my pi will not turn on. how can i fix this?
it should power back on by simply un-plugging the power wait a few seconds and re apply the power
Thank you for the prompt reply peter, i tried that and no dice. i waited a couple of minutes with the power plugged in to see if something would display to the screen, all to no avail. All that was displayed was the message, "Hold shift for secure boot." tried that and nothing happened as well. any ideas as to what is can be?
Thanks
Amando
Well, the good news is that if you see a message, then the Pi isn't broken.
It sounds like you have somehow corrupted the operating system on the SD card. Did you maybe pull it out before the Pi had fully powered down? They do take a long time to power down after clicking the icon on the GUI screen, and the red light stays on even after fully powered down.
My suggestion would be to try again with a different SD card (if you have another one that you know worked ... try it first). Or else you will need to either buy a new one (maybe with NOOBS pre-installed) or reinstall the operating system on the SD card you have. Lucky this happened early before you had written your own programs etc!
Yeap it sounds like you need to reinstall the OS, I suggest you try the newest version of weeze from the pi website, its worked like a charm for me.
Hope you solve the issue man and best of luck with your projects, I know I have had a lot of fun with it.
Gary- to power off the rpi, you log out first and then the command?? im,such a noob, but thats one of the reasons i bought the pi. another question where do you go to find information about the raspbian os and commands like the one you mentioned? @Gary Stewart
i agree, i was beginning to believe it was damaged. Going to try and re-install the os. thank you sir
Like the cowboy I'am I just unplug the power lead, can't say I've ever had any issues thereafter. Although a proper shutdown is obviously highly recommended :)
So i reformatted and downloaded the raspberry pi. it installed successfully, but nothing seems to happen after i confirmed instillation