Raspberry Pi Forum NEW: RPI MODEL B+ -> Q&A
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 693 subscribers
  • Views 3874 views
  • Users 0 members are here
  • b+
  • pi
  • modelb+
  • raspberry_pi
  • raspberrypi
  • b_plus
  • rpi
Related

NEW: RPI MODEL B+ -> Q&A

wallarug
wallarug over 11 years ago

Source:  Blog | Raspberry Pi

 

Enjoy!

  • Sign in to reply
  • Cancel
Parents
  • bodgy
    bodgy over 11 years ago

    I thought the BCM chip only had two USB ports with a shared Ethernet (can't find the original schematics on my desk top at the moment). If that is correct, is there an extra hub chip to provide the additional USB?

     

    I like the new form factor, but I have to say as far as the USB is concerned, I'm considering investing in the Raspiado Kickstarter project.

     

    Colin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to bodgy

    The BCM only has ONE USB port. If it has two, the (pins for the) second one is(are) used for something else.

     

    The two USB ports on the original B are from the LAN9512, which is an ethernet chip  with built-in 2-port USB hub.

     

    There is also the LAN9513 which is exactly the same, except for a 3-port USB hub... And the 9514 with a four-port USB hub........

     

    I've tried reading the numbers on the chip in the pictures, but failed, after researching the likely candidates I now know it's the 9514, and knowing that you can decipher the numbers on the chip in the published photos. (I used a picture on hackaday).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bodgy
    bodgy over 11 years ago in reply to rew

    Yes, just found the E14 splurge, I'm sure it wasn't there earlier today (Aus time), yup I see they are now using the LAN9514 - datasheet at Microchip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to bodgy

    and you can order them

    part Number 2431426

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to rew

    image here that might help

    http://www.raspberrypi.org/wp-content/uploads/2014/07/rsz_b-.jpg

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 11 years ago in reply to mcb1

    I just bought two from MCM, Newark Element14 shows "Awaiting Delivery" and list price is $50.59 instead of $35.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 11 years ago in reply to rew

    The new chip is the LAN9514 from SMSC/Microchip, 1xEthernet 4xUSB Hub downstream

    LAN9514 - USB to Ethernet

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 11 years ago in reply to rew

    The new chip is the LAN9514 from SMSC/Microchip, 1xEthernet 4xUSB Hub downstream

    LAN9514 - USB to Ethernet

     

    -J