Raspberry Pi Forum NEW: RPI MODEL B+ -> Q&A
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 694 subscribers
  • Views 3896 views
  • Users 0 members are here
  • b+
  • pi
  • modelb+
  • raspberry_pi
  • raspberrypi
  • b_plus
  • rpi
Related

NEW: RPI MODEL B+ -> Q&A

wallarug
wallarug over 11 years ago

Source:  Blog | Raspberry Pi

 

Enjoy!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 11 years ago

    Sorry, I an extreme novice in regards to a lot of this stuff. I might just not understand, but on the B+ are the USB and Ethernet bandwidth still tied together then?

     

    I currently have my entire DVD/Blu-ray collection ripped onto a hard drive that's connected to a PC, but I don't like leaving the computer running all the time or dedicating system resources to media streaming.  I was thinking about using the RPI with external HD to make a micro-NAS to create a media server for my home network. My biggest concern is that streaming high definition content that the connection would cannibalize itself and either the ethernet or USB would be affected by the shared bandwidth.

     

    Or is the bandwidth great enough that I'm just over thinking it and it shouldn't be an issue.

     

    Thanks in advance for the great answers and patience with a new-comer image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago

    Sorry, I an extreme novice in regards to a lot of this stuff. I might just not understand, but on the B+ are the USB and Ethernet bandwidth still tied together then?

     

    I currently have my entire DVD/Blu-ray collection ripped onto a hard drive that's connected to a PC, but I don't like leaving the computer running all the time or dedicating system resources to media streaming.  I was thinking about using the RPI with external HD to make a micro-NAS to create a media server for my home network. My biggest concern is that streaming high definition content that the connection would cannibalize itself and either the ethernet or USB would be affected by the shared bandwidth.

     

    Or is the bandwidth great enough that I'm just over thinking it and it shouldn't be an issue.

     

    Thanks in advance for the great answers and patience with a new-comer image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Former Member

    The Ethernet is still connected to the ARM via the USB 2.0 interface

     

    the difference is the Ethernet chip now has a 4 port hub on it vs a 2 port, see included diagram

     

    image

     

    for full details see the PDF here: http://ww1.microchip.com/downloads/en/DeviceDoc/9514.pdf

     

    So ultimately all data from the USB HUB connected devices and the Ethernet share the same USB2 upstream channel