Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Model B HDMI issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 686 subscribers
  • Views 4318 views
  • Users 0 members are here
  • frontpage
  • hdmi
  • rasp
  • rasp-pi
  • rasberry
  • rasp-berry
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
  • raspbian
Related

Raspberry Pi Model B HDMI issue

robobosan
robobosan over 11 years ago

HI, I have a Raspberry Pi Model below with some issue on the HDMI. I followed the troubleshooting steps, but with no luck. It's still not displaying anything on the screen.
The hdmi cable seems to be fine, i tried connecting it with a different device and that worked.

Look like there is something wrong with the raspberry pi/hdmi port on the device. Is it?


Below is the troubleshooting step:

http://elinux.org/R-Pi_Troubleshooting#No_HDMI_output_at_all


Thanks!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 11 years ago

    That troubleshooting should help you if you follow it all. What bits did you do?

    Is your RPi running if you access using SSH for a terminal? Can you get it to output via composite video?

    How are you editing config.txt? Can you post a copy of the file for us to see?

     

    My own experience is that if the TV/monitor is modern, known to be working and has the right input selected then the most common cause is the HDMI cable not plugging into the RPi properly - this is a frequent problem if the RPi is in a case, as many cases tend to obstruct the HDMI socket just enough to stop it connecting (but you think it's plugged in OK). If RPi doesn't find an HDMI monitor during boot, it stops looking thereafter so pushing the plug later will not work. If in any doubt, take the RPi out of the case while you test

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago

    That troubleshooting should help you if you follow it all. What bits did you do?

    Is your RPi running if you access using SSH for a terminal? Can you get it to output via composite video?

    How are you editing config.txt? Can you post a copy of the file for us to see?

     

    My own experience is that if the TV/monitor is modern, known to be working and has the right input selected then the most common cause is the HDMI cable not plugging into the RPi properly - this is a frequent problem if the RPi is in a case, as many cases tend to obstruct the HDMI socket just enough to stop it connecting (but you think it's plugged in OK). If RPi doesn't find an HDMI monitor during boot, it stops looking thereafter so pushing the plug later will not work. If in any doubt, take the RPi out of the case while you test

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • robobosan
    robobosan over 11 years ago in reply to Former Member

    Hi, i took the RPi out of the case and booted it up. At first it looked like it was working but then it started to flicker constantly.
    Check this video: https://www.dropbox.com/sh/15pn6wi1q2nnd4y/AACSHsizY7tpYOoKEpnerK6Pa?dl=0

    I was able to start the (default) OS installation, but the screen just went black after a while; with a message displaying "Check Video Cable". (screenshot)
    Now when i turn it on, i only get the message "Check Video Cable", the flickering stopped.

    This is what i have for my config file:
    config_hdmi_boost=4
    hdmi_force_hotplug=1
    hdmi_safe=1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to robobosan

    Did you check +5V voltage level between TP1 and TP2?  I'm the guy who added the low voltage cause to the RasPi Troubleshooting Wiki.  When I was first powering my Model B my power supply had an iffy connection, and whenever the voltage dropped below a certain level (I'd have to look it up) my monitor would first show random green dots and then blank out totally.  It would depend on what RasPi was doing.  Sometimes it worked fine until I did something compute-intensive like compiling, and then return to normal after the compiling ended.  The +5V voltage wasn't low enough to affect anything else.

     

    Nowadays I back-power RasPi from a Motorola Atrix Lapdock using a very short USB cable, so I get nearly 5V at TP1-TP2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to robobosan

    There is also this blog on the E14 web site on the same ting John is describing, more focused on the cables (USB) used when providing power Raspberry PI:- USB power cables, crashing and other problems

     

    Also I note from your screen view, that the screen may not be full HDMI, and not compatible with the output from the PI, what is the spec of the screen ? is it 720P or SD, Or something else

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to robobosan

    First, I can't see your video ('Page not found' error from Dropbox), so I'm a bit in the dark; others obviously have seen it though!

     

    Second, I'm going to ignore the 'check the 5v power' dialogue - I'm not saying it is wrong, just it is a completely different possiblity and I am not the expert!

     

    If your screen showed the OS selection dialogue, it tells us the conections are working. That will be a low resolution screen though, and maybe your monitor will not cope with higher or different resolutuions?

    A point of HDMI is that during startup, the monitor tells the RPi what resolutions it can show, and RPi chooses the 'best' amongst these. When you add those lines into config.txt, RPi ignores that dialogue (that's what the 'hdmi_force_hotplug=1' does) and RPi chooses a low resolution instead (I think it's 1024x768 60 Hz). 'hdmi_safe=1' does something similar, but difference between the 2 commands is that 'hdmi_force_hotplug=1' doesn't even need a monitor plugged in at all - just forces it to send low resolution down the wire, ignoring whether there is any feedback.

     

    So, what might be going on? Your monitor obviously works at some resolution or other. But it might not work at the default low resolutions (unusual, but possible). I would try the following with the physical setup that you know can display something (ie, RPi uncased). Also, use a direct cable - no 3:1 HDMI switch box or similar.

     

    1. Remove those lines from config.txt and see if it now works if the RPi can negotiate with the monitor.

     

    2. If not, look up the monitor manual for a list of resolutions it is capable of. Need to know both the reolutions (eg 1024x768) and the refresh rate (eg 60 Hz). Or they may be specified TV-style (720i, 720p, 1080i, 1080p etc). If you post those lists here, we can look up some extra parameters to add into config.txt alongside hdmi_force_hotplug=1, to force the RPi into one of the acceptable modes.

     

    We will get there!!

    • Cancel
    • Vote Up 0 Vote Down