Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Uses for a Raspberry Pi supercomputer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 711 subscribers
  • Views 4197 views
  • Users 0 members are here
  • cluster
  • raspberry
  • pi
  • beowulf
  • supercomputer
Related

Uses for a Raspberry Pi supercomputer

e14 Contributor
e14 Contributor over 11 years ago

Hey, this is my first post to Element14!

I came here from The Ben Heck Show, so naturally, like other semi-geeks, I decided to embark on a bunch of Raspberry Pi projects.

 

One of these projects is actually inspired from various other sources, and that's to build a small Beowulf Cluster out of Raspberry Pis. I'll start with a 16 node and upgrade to 32 afterwards.

The reasoning? Nothing more than to tinker and cross "Make a supercomputer" off of the bucket list. I am happy to spend that money and literally have it sat at home looking good until I can finally get a use out of it.

 

My question: As a general computer user and keen video editor, are there any uses I could get from the supercomputer? What could someone like me actually use this for? How would I go about doing so?

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    Problemchild over 11 years ago

    AS a bit of fun then it's OK you are learning something good on you for actually doing something!

     

    How ever as a practical cluster it's totally useless as 32-64 of them is about as powerful as a normal PC image !

    Also since there are currently no video editors for the Pi and also that you would need to have one that was cluster aware there are no applications available for your  Cluster as is.

     

    Either accept it as a learning toy or maybe get some PC hardware  use Linux +KVM then create some VMs then Cluster  them to get the same learning experience with out the difficulties of using the RPI and having a network switch  32++ PSUs etc etc

     

    Obviously creating VMs then clustering them will not improve performance but will give you the learning experience!

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Problemchild

    I wasn't expecting there to be any video editing capabilities, but it's good to have confirmation image

     

    I like Dale's idea of making a smaller one, now that I know that there really isn't much of a practical use for is. A simple little thing that could sit in my office would be cool.

     

    Beyond that of video editing, etc, what are the possibilities of hosting a Minecraft server for my ICT class? I'm an ICT teacher at a primary school near me, so it'd be cool to have something along them lines for them to be able to interact when we do redstone projects, etc. I understand that it's entirely possible with just the 1 Pi, but would I hit two birds with one stone if I built the "not-so-supercomputer" and hosted a server off of it?

    EDIT: Preferably with a GUI. I'm not very tuned when it comes to Linux, yet. I feel like I'm asking the impossible here, for some reason haha

     

    My other idea would just use the damned thing as an NAS image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to e14 Contributor

    Obviously you could use these as a Minecraft server or in fact a server for almost anything else. However the whole point of a "Beowulf Cluster" or similar HPC clusters is not to run individual tasks such as servers but a single distributed task communicating over a standard messaging protocol for example MPI or PVM. Otherwise it's not a supercomputer but a bunch of normal computers stuck on a network.

     

    For a single threaded app you may find that a mini ITX mobo is much more powerful, however if learning about message passing is the issue then you need to run that set of tasks not conventional server instances that do not use that method of comunications

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Problemchild

    Quite a few words and phrases being thrown around that I've not yet been introduced to haha

     

    I speak from the perspective of a person who has never approached anything of this caliber before. Heck, I've never used Linux or anything before buying my Pi about 2 years ago! So you will have to bear with me on alot of this.

     

    So I understand that a Minecraft server would be a poor use for such a construction, but am I right in saying I could configure them to run together in a manner which allows a server to be ran, and if (In the odd circumstance) a Pi should fail or disconnect, the others could keep it running?

     

    Remember, alot of this is for learning, not so much getting the best results. I'm going to build this cluster, regardless of what other options I have, but I also want to learn what uses it has in the average person's life image For instance, what sort of tasks in an average computer users life could be distributed amongst this system?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to e14 Contributor

    Andy Moor wrote:

     

    ... I also want to learn what uses it has in the average person's life For instance, what sort of tasks in an average computer users life could be distributed amongst this system?

    The short answer is that average computer users don't need a supercomputer.  This is why there are billions of PCs and tablets and smart phones, but few supercomputers.  The longer answer is that most of those billions of computers do have very powerful parallel GPUs which have the power of supercomputers from decades ago.

     

    Supercomputers are best suited to "embarrassingly parallel" applications than can easily be split up into small tasks that can efficiently run in parallel.  Graphics is well-suited, as is weather prediction, finite-element modeling to replace wind tunnels, and quantum chromodynamics.  Most users don't do any of this except graphics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to e14 Contributor


    So in the case of minecraft servers they would all be running there own environments so they wouldn't easily operate in a manner where they  offered one common environment.

     

    Webservers would be trivial you could do this either via an Apache Module or a load balancer

     

    Clustering for resilience is not HPC (a Beowulf or any other type of such cluster) so an active passive arrangement for a database is not an HPC cluster

     

    HPC is clustering for performance and has specific protocols such as MPI/PVM to do it..

     

    Problem here is that for either type of cluster your software needs to be written to be aware of the clustering solution.

     

    Prepare for brain pain image  the above issues and many more consume the working life of many !!!

     

    Try something like Blender which I believe as an HPC configuration to demonstrate rendering of frames across many nodes.

     

    Again good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 11 years ago in reply to e14 Contributor


    So in the case of minecraft servers they would all be running there own environments so they wouldn't easily operate in a manner where they  offered one common environment.

     

    Webservers would be trivial you could do this either via an Apache Module or a load balancer

     

    Clustering for resilience is not HPC (a Beowulf or any other type of such cluster) so an active passive arrangement for a database is not an HPC cluster

     

    HPC is clustering for performance and has specific protocols such as MPI/PVM to do it..

     

    Problem here is that for either type of cluster your software needs to be written to be aware of the clustering solution.

     

    Prepare for brain pain image  the above issues and many more consume the working life of many !!!

     

    Try something like Blender which I believe as an HPC configuration to demonstrate rendering of frames across many nodes.

     

    Again good luck!