Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Model A+ > Specs Released
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 709 subscribers
  • Views 2788 views
  • Users 0 members are here
  • raspbmc
  • raspi
  • raspberry_pi
  • a+
Related

Raspberry Pi Model A+ > Specs Released

wallarug
wallarug over 11 years ago

See this article:  http://www.i-programmer.info/news/91-hardware/7956-new-raspberry-pi-a.html

 

They found a page on Element14's site that was later taken down. 

 

What do you guys think?

  • Sign in to reply
  • Cancel
  • wallarug
    wallarug over 11 years ago

    specs breakdown:

     

    700MHz Broadcom BCM2835 CPU
    256MB RAM
    40pin extended GPIO
    1 x USB 2 port
    4 pole Stereo output and Composite video port
    Full size HDMI
    CSI camera port
    DSI display port (Raspberry Pi touch screen display)
    4 mounting holes
    Micro SD port
    Micro USB power connector
    Size : 65mm x 56mm

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago

    There's a list of specifications here: Raspberry Pi Model B+ and Model B Boards and Accessories | MCM Electronics

    and here: Raspberry Pi Model A+ Board Features a 40-pin GPIO Connector, a micro SD slot, and Improved Power Management

     

    A+ looks like a nice board.  I like the size: it finally fits in an Altoids box image  US$20 price is very impressive.  With the 40-pin GPIO connector it becomes a good candidate for projects that would otherwise need BeagleBone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem

    Best thing about it is that it can fit in those smaller enclosures Altoids included !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to wallarug

    It's all over the net now so no more point in hiding it ... I suppose the very existence of this thread means they think the same ..So far!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to Problemchild

    It's a shame that it still has connectors poking out all over the place and is using micro USB for power.

    If it really sells for £12.50 it is very cheap.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to michaelkellett

    Hard to slag it off too much when it's cheaper than a genuine Arduino image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kidiccurus
    kidiccurus over 11 years ago in reply to wallarug

    Noooo.... It only has 256mb of ram. I don't want to have to use a full model b just so I can get the extra ram. I hope they add an option to order a 512mb version for slightly more ram intensive applications. Apart from that it looks very nice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to kidiccurus

    Alas, that won't happen.

    The units are quite cheap and that is achieved by doing mass-production with lots-of-the-same-units. Having all sorts of options no-tv-out for me, extra ram for you is going to make things more expensive. So if you need more ram, I'm afraid you'll have to get the bigger B+....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 11 years ago in reply to rew

    glad someone knows how economics works.

     

    if you really really want 512 mb ram, desoldier the components off the b+. It is the same device. If you want to go to the extreme, disconnect the power from the usb chip. Then you (technically) have a model a+.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to wallarug

    Haha! If you try moving the RAM chip, or CPU+RAM from the B (*) to the model A, and you make a nice write-up of what you did you'll get featured on "hackaday.com".... Either as "fail-of-the-week" or as a regular article... :-)

     

    (wallarug: you're not completely clear: There are three ways about it that you're suggesting: 1) move the RAM chip off a "B" to an "A", 2) move CPU+RAM from a model B to a model A, 3) downgrade the "B" to an A by disconnecting the USB chip. (#)

     

    (*) note: where I'm saying "model B", this includes the "B+", same goes for "A".

    (#) This might no longer be possible with the B+: The PCB has (probably) not been designed to be "downgradable" to a model-A+. The "designed as downgradable" means that there is a "jumper" that allows you to connect the CPU-USB to the connector instead of to the ethernet chip. So disconnecting the usb-hub/ethernet chip will probably leave you without any USB on the B+.

     

    Oh... On hackaday they predicted that it would take a week for someone to come up with power-measurements for the model A+...

    I measured it on Tuesday but don't think it warrants a fully writeup for a hackaday article. My model A+  uses just under 100mA (about 95-97) when idling, but with a full-HD monitor connected. There are short peaks when the "SD active" led flashes, The peaks are around 150mA, so it seems as if my SD card (a trancend) uses about 50mA. Note that the current consumption depends on the exact voltage that you provide. By providing closer to 5.5V than 5.0V, the current consumption should also go down by about 10%.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>