Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum LiPo battery questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 673 views
  • Users 0 members are here
  • raspberry
  • pi
  • raspberry_pi
  • lipo
  • fona
  • adafruit
  • heck
  • ben
Related

LiPo battery questions

e14 Contributor
e14 Contributor over 11 years ago

I'm currently building a raspberry pi based phone similar to that of Dave Hunt (PiPhone – A Raspberry Pi based Smartphone) and also like Ben Heck's DIY Cell Phone. Using the Adafruit FONA ben used and the Pi with the Pi TFT I was wondering if the Pi could be powered by the same battery as the FONA.

 

Currently the FONA uses a 3.7v battery and contains its own charging circuit which is perfect. However I can't tell if it can provide power out to power the Pi. Therefore I was wondering if and how it would be possible to split a LiPo output to go to the Pi and also the FONA. I know I would need to convert the voltage to 5V for the Pi but I know how to do that. So I just need some help on the splitting battery output and also if anyone knows if the current charge circuit would still charge the battery?

 

Thanks in advance for any information.

  • Sign in to reply
  • Cancel
Parents
  • toxxn
    toxxn over 11 years ago

    What amperage does the LiPo battery provide and how much does the FONA require?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to toxxn

    This is taken from a fact sheet on the FONA

     

    "How long can FONA last on my battery?

    We haven't done extensive testing with FONA but from preliminary reports, the FONA

    draws about 20-25mA while running, up to 200mA+ while actually making a

    call/sending/receiving data, and has very small spikes of up to 2A. The spikes are short

    and are absorbed by the onboard capacitors.

    A 1200mAh battery can run the FONA on 'standby' for a day or two."

     

    I have a 500mAh, 1200mAh and would be willing to get when they are back in stock a 2500mAh.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to e14 Contributor

    The battery-use of a 'pi is MUCH more than that of your FONA. A factor ten or twenty.

     

    The CPU on the rasbperry pi is designed to draw its power from a LIPO battery! Perfect!

     

    So... If you hook up the "what-is-supposed-to-be-5V" on the 'pi directly to the LIPO then the CPU will work just fine.

     

    What doesn't work is:
    * The 5V output on the USB side. Your USB peripherals won't work.

    * The 5V output on the HDMI. It is meant to power for example the in-cable HDMI to VGA converters.

    * The SD card and ethernet/usb chip on the model B(+) will work as long as its 3.3V is "reasonable".

     

    That "reasonable" depends on a few things. I've measured the ethernet chip as "working" with the 3.3V rails

    as low as 3.0V. I recommend not going below 3.3, and keep some margin. I have not tested SD cards, besides there are many of those.

     

    On the model B the "recommend not going below 3.3V" means that your 5V line has to be above about 4.3V: Not possible by the "direct connection to a LIPO". On the B+, I expect (but have not measured) that the voltage converter will keep the 3.3V operational down to a source voltage of about 3.4V.

     

    At that voltage you have less than 5% of your battery capacity remaining. You need to SHUT DOWN NOW to prevent damage to your battery. Just leaving your 'pi connected to the battery at that point in time will drain the battery into unrecoverable damage within a few hours, even if you halt the 'pi. So a discharge protection circuit is a must. If your FONA has this already I don't know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 11 years ago in reply to e14 Contributor

    The battery-use of a 'pi is MUCH more than that of your FONA. A factor ten or twenty.

     

    The CPU on the rasbperry pi is designed to draw its power from a LIPO battery! Perfect!

     

    So... If you hook up the "what-is-supposed-to-be-5V" on the 'pi directly to the LIPO then the CPU will work just fine.

     

    What doesn't work is:
    * The 5V output on the USB side. Your USB peripherals won't work.

    * The 5V output on the HDMI. It is meant to power for example the in-cable HDMI to VGA converters.

    * The SD card and ethernet/usb chip on the model B(+) will work as long as its 3.3V is "reasonable".

     

    That "reasonable" depends on a few things. I've measured the ethernet chip as "working" with the 3.3V rails

    as low as 3.0V. I recommend not going below 3.3, and keep some margin. I have not tested SD cards, besides there are many of those.

     

    On the model B the "recommend not going below 3.3V" means that your 5V line has to be above about 4.3V: Not possible by the "direct connection to a LIPO". On the B+, I expect (but have not measured) that the voltage converter will keep the 3.3V operational down to a source voltage of about 3.4V.

     

    At that voltage you have less than 5% of your battery capacity remaining. You need to SHUT DOWN NOW to prevent damage to your battery. Just leaving your 'pi connected to the battery at that point in time will drain the battery into unrecoverable damage within a few hours, even if you halt the 'pi. So a discharge protection circuit is a must. If your FONA has this already I don't know.