Raspberry Pi Forum 3.8 Inch LCD Touchscreen Connection Help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 684 subscribers
  • Views 1854 views
  • Users 0 members are here
  • raspberry
  • lcd
  • help
  • pi
  • raspberry_pi
  • touchscreen
  • screen
Related

3.8 Inch LCD Touchscreen Connection Help

Former Member
Former Member over 11 years ago

Hi, I was wondering as I can't seem to find any pinout matching my Touchscreen does anyone know which wires I should connect?

My screen has 34 Pins:

 

 

1: CS                   18: RS

2: WR                  19: RD

3: RST                 20: DO

4: D1                   21: D2

5: D3                   22: D4

6: D5                   23: D6

7: D7                   24: D8

8: D9                   25: D10

9: D11                 26: D12

10: D13               27: D14

11: D15               28: GND

12: BL                 29: VDD

13: CDD              30: GND

14: GND              31: 5v

15: MI                  32: M0

16: PEN              33: NC

17: TCS              34: CLK

 

 

 

 

Many thanks

  • Sign in to reply
  • Cancel
Parents
  • mconners
    mconners over 11 years ago

    You might want to research this, I think it is similar to what you posted, beware, it's not for the faint of heart image

    http://www.sainsmart.com/arduino/arduino-shields/lcd-shields/sainsmart-3-2-tft-lcd-display-touch-panel-pcb-adapter-sd-slot-for-arduino-2560.html

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 11 years ago in reply to mconners

    They swear it works with a ras pi, I found the info once, but I can't find it at the moment.

     

    There is an adapter card that can be purchased/built highlighted here

    http://ozzmaker.com/2013/05/23/raspberry-pi-with-a-3-2-tft-with-touch-control/

     

    But that requires additional hardware/work

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mconners
    mconners over 11 years ago in reply to mconners

    They swear it works with a ras pi, I found the info once, but I can't find it at the moment.

     

    There is an adapter card that can be purchased/built highlighted here

    http://ozzmaker.com/2013/05/23/raspberry-pi-with-a-3-2-tft-with-touch-control/

     

    But that requires additional hardware/work

     

    Mike