Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is the Raspberry B+ GPIO passed through with the Cirrus Audio card?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 709 subscribers
  • Views 5325 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Is the Raspberry B+ GPIO passed through with the Cirrus Audio card?

gkzsolt
gkzsolt over 11 years ago

The previous Wolfson card has a 26 pin header with male pins to connect to the Raspberry GPIO header after pushed on top of it. Does the new audio card do the same for the 40 pin header? Sorry, but I cannot discern from the card images I have.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Sorry, I mean 7 GPIOs, of course...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tonyhansen
    tonyhansen over 11 years ago in reply to e14 Contributor

    If what you say is correct, that means I count 9 GPIO pins that are passed through from the RPi, the 7 GPIOs (not 6) you list (Pins 09, 11, 14, 17, 18, 19, 20) that are passed through the Expansion header, and 2 more that are passed through the J8 header.

     

    I put together this table for my own notes and figured I'd share it:

     

        


    Cirrus Logic

    Audio Board

    Pin

    RPi GPIO

    Description

    RPI Alternate

    Description

    RPi pin

    1

    EX 9

    GPIO 3

    SCL I2C

    5

    2

    EX 11

    GPIO 2

    SDA1 I2C

    3

    3

    EX 14

    GPIO 5

     

    29

    4

    EX 17

    GPIO 6

     

    31

    5

    EX 18

    GPIO 12

     

    32

    6

    EX 19

    GPIO 16

     

    36

    7

    EX 20

    GPIO 26

     

    37

    8

    J8-1

    GPIO 14

    UART TX

    8

    9

    J8-2

    GPIO 15

    UART RX

    10

     

     

    Of course, this doesn't match the number 8 that is mentioned in the Cirrus Logic Audio Card Comparison Table. No reconciling that yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gkzsolt
    gkzsolt over 11 years ago in reply to tonyhansen

    Sorry to ask, what do you mean by GPIO pins that are passed through from the RPi? How can I access those? (I don't have a Cirrus card yet).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tonyhansen
    tonyhansen over 11 years ago in reply to gkzsolt

    The Cirrus Logic Audio Card (and the Wolfson Audio Card before) have a few headers sticking up. In particular, the Cirrus Logic Audio Card has a header known as the J2 Expand (or Expansion) Header and another header known as J8 (marked UART on the CL), some of whose pins are direct connections to (i.e., pass-throughs of) the GPIO pins on the Raspberry Pi itself. The other pins are instead connected to various features of the Audio Board itself.

     

    For more information, see

    • the table in previous posts for which CL header pins are hooked to which RPi pins,
    • the user manual (which currently has some typos in it), or
    • the schematic.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gkzsolt
    gkzsolt over 11 years ago in reply to tonyhansen

    Thank you again. I am sorry, I've misread your previous comment (and not looked at the schematic and table attentively.) Now I've done this.

    The user manual definitively needs major corrections. What is not clear now is what are pins 15 and 16 on the expansion header, if they are not GPIO4 and GPIO3.

    9 GPIO pins passed through from the RPi doesn't sound very bad, but what worries me very much is that the SPI bus pins (GPIO9, 10 and 11, not counting CE0 and CE1) are not between them. So how can I use any SPI device then?

     

    Another note. According to the Cirrus Logic Audio Card Comparison Table, the previous Wolfson Audio Card had only 3 available Pi GPIO pins, including UART. Is that true? It follows that using the new one would be a better choice. But on the old card and RPi I could access the general protocol pins, in particular the SPI bus because the whole RPi P1 header was available. Am I right?

     

    The pdf user manual I downloaded is not text searchable, at least I cannot search it with Linux evince. Is this my fault?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tonyhansen
    tonyhansen over 11 years ago in reply to gkzsolt

    Correct, pins 15&16 are marked GPIO4&3. But if you look at the schematic, you will see that those are GPIO connections from the AUDIO chip, and NOT the RPi. And I haven't seen any reports of anyone finding an interface for controlling those audio chip pins.

     

    You cannot directly use an SPI device when the audio board is mounted. But you can use UART and I2C.  If you >really< need SPI, you'll need to use a bridging device between I2C or UART and SPI.

     

    The older Wolfson Audio card has the same architecture as the newer board: it plugs into the RPi J8 header AND has contact pins to the P5 interface, then uses most of the available RPi GPIO pins for its own purposes, including the P5 GPIO pins. Your choices are limited.

     

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gkzsolt
    gkzsolt over 11 years ago in reply to tonyhansen

    Thanks for looking up the 15 & 16 pins.

     

    "You cannot directly use an SPI device when the audio board is mounted."

     

    Why? To my knowledge, the SPI control pins are general: the clock, MOSI and MISO are shared between all SPI devices (like on the I2C). There is one pin dedicated to each slave, a CHIP SELECT (and maybe some other pins too, depending on the device). I have an nRF24 device connected to my Raspberry now, what seems that I should abandon if I enter the Wolfson/Cirrus world. Do you see any reason for not using the SPI bus for several devices?

     

    "But you can use UART and I2C.  If you >really< need SPI, you'll need to use a bridging device between I2C or UART and SPI."

     

    I am not sure what kind of bridging device you mean, but if it would be a protocol translator chip, for ex. from SPI to I2C I would definitely avoid this. The I2C interface implementation on the Raspberry PI is quite (I would say "very") limited. It does not allow repeated starts (by the software driver), which already hinders the use of some devices. It also supports only single-master setups (by hardware), so you should carefully design your network. But you may understand if I would stay clear from translating other (and quicker) protocols to I2C.

     

    Regarding the UART, it's fine but allows a connection with only one device and you should decide to disable or not the kernel console on it. If you leave it enabled, you have a "single master" only operation (commands only from the connected device). If you disable it, you can implement a duplex communication (where each device can initiate write), but you loose the kernel messages.

     

    I am thinking of connecting the RPi to a controller (an Arduino), but even this has issues, knowing the mentioned limitations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tonyhansen
    tonyhansen over 11 years ago in reply to gkzsolt

    For SPI, you're making a few assumptions:

     

    • that you can get at the pins for CLK, MOSI and MISO. They are not passed through to the audio card expansion header.
    • that they haven't been reassigned to other uses by the audio card. We don't know the answer to this.

     

    Some people have played around with resoldering some of the audio card connectors to gain access to hidden pins like CLK, MOSI, and MISO. Feel free to try that and let us know how it goes.

     

    With the Wolfson card, because of the P5 spring-loaded connector, there was little leeway to access the pins >from below< the audio card. But with the Cirrus Logic card, I don't see any reason that something like Element 14's RTC shim board wouldn't work.

     

    So you MIGHT be able to do something similar to the shim board to access the CLK/MISO/MOSI pins. They MAY or may NOT work for you as SPI access. Go go for it and let us know what happens.

     

    The thing to remember with the Wolfson and Cirrus Logic audio cards is that they were designed to take advantage of the RPi's capabilities to provide high-quality audio features. To do that, those cards use a LOT of the RPi's resources. Anything else we get to do with the RPi after that is a bonus. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gkzsolt
    gkzsolt over 11 years ago in reply to tonyhansen

    Hi Tony,

     

    No, I am not making the assumption that the SPI bus pins are exposed. I know they are not, and that is what makes me wonder: why have the designers decided to hide them? In general, there should be no reason for that, except in some (unusual) cases.

    In the schematics I see these 4 pins (MIS, MOSI, SCLK, SS) routed to the corresponding CIF2XX on the WM5102 chip (the RPI pins enter into IC U8, what seems to be a level shifter). From this I conclude that they are used for their purpose, in an SPI protocol and not been "reassigned to other uses", if you meant that. This also means that they can be used for other devices too (except SS). All SPI devices in a module share the same bus pins, ignoring them if their SS slave select pin is not active. So the question remains.

    (I could go and try this with some experiments, but I don't have a Cirrus card yet. I am trying to figure out if it is worth buying one.)

    May I ask if you could search through the "Cirrus Logic Audio Card User Manual.pdf"?

    I agree very much with you in that a Cirrus card takes a lot of RPi's resources. But what worries me more, is the quality of documentation (very poor) and the lack of support. Is somebody at Cirrus reading and taking notice of these discussions? Or is there a place we can show some of these to a competent personnel (thinking of your table, etc.) ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gkzsolt

    In Windows the pdf CLAC user manual also not text searchable (it searches only in small parts of text like tables and command examples).

    Yes, and looks like there is nothing relevant to your question in the manual, any way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>