Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 - does it hit the mark?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 713 subscribers
  • Views 7234 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 - does it hit the mark?

tekmeister
tekmeister over 11 years ago

While previous articles had the release slated for 2017, it seems the next-gen Raspberry Pi is being released today:

 

http://www.theregister.co.uk/2015/02/02/raspberry_pi_model_2/

 

Pi v2 will come with a quad-core 900MHz processor and 1GB RAM (an upgrade from the single-core 700MHz and 512MB RAM of the original). Also the price will be the same ($35). It looks like the footprint is the same as the B+.

 

As I mentioned in November How to make a better Pi, the two main things in the Pi's favour are cost and community, but I have run into a number of limitations with the original Pi. I'm hoping this new version addresses most of them, but time will tell, as full details aren't available yet.

 

Aside: I'm wondering if this is what the upcoming "Enchanted Objects" challenge is about.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    Very interesting.  I'll be interested in seeing how much cache it has.  The BCM2835 is hobbled by having just 128KB level-2 cache shared between CPU and GPU, and I don't know how much individual I and D cache the CPU has.

     

    From what I see, for my intended use I'm better off with an ODROID-C1 ODroid - Oh Boy! which has gigabit Ethernet through dedicated MAC pins instead of USB, UHS-1 SD card or eMMC for mass storage, and quad 1.5 GHz ARMv7 processors.  Each processor has 32KB I and D caches, and a shared 512KB level-2 cache.  It has a separate 160KB level-2 cache for the GPUs.

     

    Update: according to this Make interview with Eben Upton, the BCM2836 has 512KB of level-2 cache like ODROID's AmS805.  Dr. Upton didn't say how much level-1 cache each ARM Cortex-A7 core has.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 11 years ago

    Very interesting.  I'll be interested in seeing how much cache it has.  The BCM2835 is hobbled by having just 128KB level-2 cache shared between CPU and GPU, and I don't know how much individual I and D cache the CPU has.

     

    From what I see, for my intended use I'm better off with an ODROID-C1 ODroid - Oh Boy! which has gigabit Ethernet through dedicated MAC pins instead of USB, UHS-1 SD card or eMMC for mass storage, and quad 1.5 GHz ARMv7 processors.  Each processor has 32KB I and D caches, and a shared 512KB level-2 cache.  It has a separate 160KB level-2 cache for the GPUs.

     

    Update: according to this Make interview with Eben Upton, the BCM2836 has 512KB of level-2 cache like ODROID's AmS805.  Dr. Upton didn't say how much level-1 cache each ARM Cortex-A7 core has.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to johnbeetem

    It's not showing on the AUS/NZ website ...so how do I order one?

     

    Considering all the controversy around the B+ and details leaked ...this one has been quietly slipped in and the suppliers aren't there yet.

    The UK site is also non existant.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tekmeister
    tekmeister over 11 years ago in reply to mcb1

    I think The Register might have jumped the gun slightly - my guess is the official announcement will hit later today (it's only 5am in England atm)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tekmeister
    tekmeister over 11 years ago in reply to johnbeetem

    Yeah the ODROID-C1 is a great little board. Don't rule out the RPi 2 just yet though, it will likely succeed due to sheer momentum. Remember the Pi is quite popular in education.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 11 years ago in reply to johnbeetem

    I like the ODROID-C1 (I have one) but at this time there are a few problems with them:

     

    1.  No documents on the ARM SOC. In one of the wiki threads it said it was going to be released Jan. 15 but I have been back several times since then and I am still waiting.

    2.  No documents on the GPU, and there is not likely to be any in the future because it is not their IP.

    3.  This one is just for you John, no PCB layout information. In one of the FAQs they state that this is NOT an open hardware platform and they will only release the schematics.

         As I have said several times in Raspberry Pi forums schematics are all I really need to find most problems so I have no problem with this as long as the schematics are accurate.

         There are a couple of problems with the current schematics however. There are two page 21s and two page 22s, both sets are for the USB1 - USB4 circuits. Both are related to

         the same issue, copying pages where the schematic is virtually the same, but not changing the signal net/bus names. All the nets/buses are labeled USB1 and USB2 on both

         pages so it is difficult to tell which is 1/2 and which is 3/4. There are different reference designators on the pages using A/B to differentiate between them which is carried over to

         the PCB silk screen so by it can determined which is which on the schematic, it's just better to have accurate schematics to start with.

     

    Other than the above I also like that:

     

    1.  You can use eMMC for the OS which is much faster (and much more expensive) than the micro-SDHC card.

    2.  It has an optional reasonable priced battery backup for the RTC,

    3.  A dedicated serial port for the console, although they use a "non-standard" connector that will not work with most RS232 level converters. They do offer a serial to USB converter.

    4.  Several interesting reasonably priced add-ons and according to them, more to come.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 11 years ago in reply to gdstew

    Hey Gary,

     

    Here is the link the the SOC:

    http://dn.odroid.com/S805/Datasheet/S805_Datasheet%20V0.8%2020150126.pdf

     

    I found it here:

     

    http://hardkernel.com/main/products/prdt_info.php?g_code=G141578608433&tab_idx=2

     

    On the technical details tab. It's been there for a while IIRC.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to gdstew

    Gary Stewart wrote:

     

    I like the ODROID-C1 (I have one) but at this time there are a few problems with them:

     

    1.  No documents on the ARM SOC. In one of the wiki threads it said it was going to be released Jan. 15 but I have been back several times since then and I am still waiting.

     

    AmS805 data sheet link is on this page: http://hardkernel.com/main/products/prdt_info.php?g_code=G141578608433&tab_idx=2

    2.  No documents on the GPU, and there is not likely to be any in the future because it is not their IP.

    It's a MALI GPU.  There's an open-source project called LIMA that's trying to produce open-source documentation and drivers.  I don't know how far they've gotten.  I'm delighted that RasPi opened up the VideoCore 4 last year and hope that starts a trend toward open documentation.  I've read that it's mostly USA patent law that preventing Progress in Science and Useful Arts in the GPU arena.

    As I have said several times in Raspberry Pi forums schematics are all I really need to find most problems so I have no problem with this as long as the schematics are accurate.

     

         There are a couple of problems with the current ODROID-C1 schematics however. There are two page 21s and two page 22s, both sets are for the USB1 - USB4 circuits. Both are related to the same issue, copying pages where the schematic is virtually the same, but not changing the signal net/bus names. All the nets/buses are labeled USB1 and USB2 on both pages so it is difficult to tell which is 1/2 and which is 3/4. There are different reference designators on the pages using A/B to differentiate between them which is carried over to the PCB silk screen so by it can determined which is which on the schematic, it's just better to have accurate schematics to start with.

    We're still waiting for the RasPi B+ schematics.  The RasPi page only has a single-pager with interfaces: http://www.raspberrypi.org/documentation/hardware/raspberrypi/schematics/

     

    There's no A+ schematic at all.  Who knows when the RasPi 2 schematics will be released.  It took a long time for the RasPi Model A/B schematics to come out.

     

    The ODROID schematics are a bit hard to follow since they're hierarchical instead of flat.  There is only one page 21 and one page 22 in the design, but the printout has two instances of each with different component names.  You have to go back to the root schematic on page 1 to make sense of it and see how the signal names map.  It's a pain: I far prefer flat schematics for a board this size, but schematic styles vary.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • nlarson
    nlarson over 11 years ago in reply to mcb1

    Hi Mark - if you are having a hard time finding the product on New Zealand's site - try this link here: http://nz.element14.com/raspberry-pi/raspberrypi-2-modb-1gb/sbc-raspberry-pi-2-model-b-1gb/dp/2461030?ost=2461030

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to nlarson

    Nicole

    Thanks very much

    Someone gave a link to the design centre, and that gave me an inside to be able to order it.

     

    I note the numbers have dropped since I first ordered ....

     

    The one good thing about element14 is the product code number stays constant (well except for MCM) ....

    Thanks

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 11 years ago in reply to mconners

    Thanks Mike (and John) !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 11 years ago in reply to johnbeetem

    "It's a MALI GPU.  There's an open-source project called LIMA that's trying to produce open-source documentation and drivers.  I don't know how far they've gotten.  I'm delighted that RasPi opened up the VideoCore 4 last year and hope that starts a trend toward open documentation.  I've read that it's mostly USA patent law that preventing Progress in Science and Useful Arts in the GPU arena."

     

    Yes I am aware of this project and trying is exactly the right way to put it. GPUs are very complicated devices and open documentation is really the only way to get it right . Like you I hope the others follow suit however I would not hold my breath,

    there have been rumors but they are at least a couple of years old now and nothing has changed.

     

     

    "We're still waiting for the RasPi B+ schematics.  The RasPi page only has a single-pager with interfaces:"

     

    Yes I know, I have brought up my displeasure with this several times in these forums. As far as I can tell the one page details all of the changes made between the B and B+ EXCEPT the new USB IC  and USB interface circuits. I have no idea why they

    have suddenly gotten secretive about this and it does not sit well with me that they have. Plus my attempts to get this changed have to date been ignored. I may wait until the schematics are(?) published before buying a Pi 2.

     

     

    "The ODROID schematics are a bit hard to follow since they're hierarchical instead of flat.  There is only one page 21 and one page 22 in the design, but the printout has two instances of each with different component names.  You have to go back to the root schematic

    on page 1 to make sense of it and see how the signal names map.  It's a pain: I far prefer flat schematics for a board this size, but schematic styles vary."

     

    My explanation pretty much describes exactly what they are. The part of page one you describe is just a block description that does not give any details that are useful when trying to trace a problem back to the source (pins). Not differentiating

    between which circuits on the schematics are for USB ports 1/2 and which are for USB ports 3/4 is just not the right "style" period. In my 30+ years in electronics I have never seen another schematic (other than maybe a bad preliminary one) that

    used this "style".