Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 is unstable.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 711 subscribers
  • Views 3965 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 is unstable.

e14 Contributor
e14 Contributor over 11 years ago

Today has received the Pi2 and was totally disappointed. Is very unstable. I do not even managed to set up the system. After a minute or two system is down. Then apparently fray fs continue after any issues downloading the same message "End Kernel panic - not syncing: VFS Unable to mount root fs on unknown-block(0,0)". That's all.image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Actually you guys right - this is power supply issue. I tried next steps. Connect Pi2 to Li-Ion battery with USB. See pic. And all working perfect. No one faults over 2 hours. Ok. That is good. I made update and upgrade for apt-get. And further. Get short USB cable with ferrites and connect to another power supply. And whole day Pi2 works very good. No faults and much stable.
    Thanks everyone for advices and help!

     


    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • hawkeyethehacker
    hawkeyethehacker over 11 years ago in reply to e14 Contributor

    Noooooooooooo!

     

    Don't run those on top of those anti-static bags - while the inside is nice and protective the outside is a farmhouse for static charges.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to hawkeyethehacker

    Your advice was appropriate for some bags.

    It just happens that these are a very good quality bag  .... better than I thought.

     

    Static builds up and unless it is discharged or dissapated it can cause issues where a pin is raised to a potential higher than the others.

    Discharging one's self by making contact with an earthed surface BEFORE touching the electronics is preferable.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 11 years ago in reply to hawkeyethehacker

    Hang on a moment though... surely if the outer layer is actually 'conductive' (as stated above) that surely implies that it will conduct electricity, and could therefore connect, and possibly 'short out' some of the exposed components on the underside of an otherwise protected board?

     

    Personally I would NOT advise placing a 'live' RasPi on on of these. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Montala

    surely if the outer layer is actually 'conductive'

    Did you actually read the pdf I referenced above.?

    10 ^8 to 10^11 ohms is 100M ohms to 100 G ohms

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 11 years ago in reply to mcb1

    Yes I did, thank you Mark, but just having a high resistance, doesn't necessarily make it non-conductive.

     

    It is obviously up to each individual to make up his own mind on what to use, but I will stick by my comments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to Montala

    Well. Just having a high resistance is exactly what makes things non-conductive.

     

    Everything conducts electricity to some point. Above some arbitrary threshold you call things "non contductive" because for all practical purposes no electrical current is conducted. In this case "10^8 ohms" is for all practical purposes "non conductive". Put a 5V over this and you'll get a "short" that carries about 2*10^-7 A. or about 0.02 micro amps. THAT will be difficult to measure, let alone influence the raspberry pi. (the influence of "at some time in the past few years you've touched the 'pi with your bare hands" is on the same order of magnitude. You don't worry about that, do you?).

     

    A friend of mine works with voltages of around 3MV. Megavolts. A current of 0.03A at 3MV represents 100kW and that is something that could be quite deadly if overlooked....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Montala

    It is obviously up to each individual to make up his own mind on what to use, but I will stick by my comments.

    You are entitled to make up your own mind.

    Sometimes when the facts don't support your theory, you have to decide if your theory is still correct.

     

    If you cannot confirm the bags design then your comment   Personally I would NOT advise placing a 'live' RasPi on on of these.  is perfectly valid.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • konakcc
    konakcc over 10 years ago in reply to hawkeyethehacker

    Actually, Anti-static bags are conductive on both sides, so they will short out your board.  Doesnt use any plastic either.  Purchase an ESD mat if you are going to work on table top.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to konakcc

    Actually, Anti-static bags are conductive on both sides

    Sorry but that statement isn't true.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to mcb1

    The datasheet of the anti-static bags (*) mentions some resistance. We tried measuring it, but were unable to make a connection or measure a resistance. 

     

    So.... the bags will NOT short your pi if you put the pi on top of the bag.

     

    (*) The ones that the 'pi comes in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to konakcc

    as Everyone else is saying... there not a short.


    The bags are dissapative or simply resist the build up of a static charge, mostly there to stop a static zap on the outside traveling to the inside and damaging the component within

     

    Dave Jones of the EEVBlog has done a few videos on this subject if your interested in finding out

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to konakcc

    as Everyone else is saying... there not a short.


    The bags are dissapative or simply resist the build up of a static charge, mostly there to stop a static zap on the outside traveling to the inside and damaging the component within

     

    Dave Jones of the EEVBlog has done a few videos on this subject if your interested in finding out

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • konakcc
    konakcc over 10 years ago in reply to Robert Peter Oakes

    According to a major static bag manufacturer, Anti-static bags contain conductive material.  I would never place any electronics in a powered up state on or in an Anti-static bag.

     

    Before You Buy: Comparing Anti Static and Static Shielding Bags

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to konakcc

    Hi!

     

    There are different kinds of bags. There may be a confusion between anti-static bags, conductive bags, and exactly what part

    of anti-static bags is conductive.

     

    The anti-static bags may have conductive layers, or conductive material, but often it is part of an internal layer.

    For example, this manufacturer states 10^8 to 10^11 ohm surface resistance, which is quite high, beyond my handheld Fluke measurement capability (I have tried it).

    That would be safe from a conductivity point of view. The layers do not split on the bag mentioned. They may with other bags. No idea.

     

    There are very conductive bags too, they are called (unsurprisingly) conductive bags, but they are usually black in colour. They have a very low surface resistance (less than 1kohm is

    possible!), definitely not suitable for placing powered circuits on top of. They are fantastic for storing MOSFETs though. They are easily measurable with any handheld multimeter.