Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi and Existing Accenta Gen 4 Alarm
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 710 subscribers
  • Views 7278 views
  • Users 0 members are here
  • pi
  • raspberry_pi
  • accenta
  • alarm
Related

Raspberry Pi and Existing Accenta Gen 4 Alarm

e14 Contributor
e14 Contributor over 11 years ago

Hi All,

 

I'd like to connect my existing alarm (HONEYWELL ADE ACCENTA MINI LCD BURGLAR ALARM PANEL: Amazon.co.uk: Kitchen & Home) to my pi, so that I can monitor the alarm remotely.  The panel has a connection for a "dialler" so im thinking of connecting the pi via that.

 

As well as the status of the alarm, I'd like to make use of the PIRs so that I can integrate them with my home automation. 

 

Thanks in advanced.

  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    I have found a Service Manual that may be appropriate for your panel: http://www.wavertreeelec.co.uk/skin/frontend/target/target/pdfs/Optima_Compact_Accenta_Panels.pdf

    It would seem from reading the manual that there are 5 active-low outputs switched between 0 and 13V depending on the status of the panel, namely:

    • FIRE: The fire output operates when the fire zone is triggered.
    • PA: The PA output operates when a PA alarm is triggered or a duress code is used.
    • INT: The intruder output is operated when an intruder condition is triggered whilst the system is set.
    • SET: The Set output operates whenever the system becomes set and is used to indicate opening and closing.
    • ABORT: Operates if the panel is unset within 90 seconds of the alarm condition starting. It is cleared when the panel is reset by the user or engineer.

     

    Connecting to this interface could be achieved to 5 GPIOs of the Raspberry Pi (NOT DIRECTLY - RPi's don't like 13V on the GPIO header.)

    It seems that interfacing with individual PIRs cant be achieved with this connector, and while you could in theory connect to the zone inputs for monitoring purposes, the panel may not appreciate the interference.

     

    Also worth noting is wether the panel is maintained under a service contract with a third party company. Modifying the panel wiring is very likely to upset such a company.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Thanks Paul!

     

    How would you recommend connecting those outputs to the PI?  I've got some knowledge with electronics but not enough to figure out how to connect it to the PI.

    Interesting thoughts about tapping in to the zone inputs, how would I go about doing this?  The PIRs I use are Active8 and a couple of door contacts.

     

    There's no service agreements as the alarm was installed by myself and my father.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    You could use a simple voltage divider to bring the voltage down: http://en.wikipedia.org/wiki/Voltage_divider

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Cheers!

     

    So I've found exactly what i was looking for: https://github.com/sidb/PiAlarm/blob/master/README.md

     

    BUT would you be able to help me convert that image in to a shopping list? and help to make sense of the connection on the breadboard?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    The photo on that page should give you a good idea about the wiring. It is essentially the same as the schematic above. (Please note the board in the photo has been turned upside down. Flip it through 180º and it should make a whole lot more sense. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Thanks for the tip!

     

    Sorry for being such a pain...could you point me to the correct 2k2, 330r and the isolators

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Thanks for the tip!

     

    Sorry for being such a pain...could you point me to the correct 2k2, 330r and the isolators