Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic Audio Card working on the Raspberry Pi 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 165 replies
  • Subscribers 715 subscribers
  • Views 26810 views
  • Users 0 members are here
  • wolfson
  • raspberry
  • audio
  • pi
  • cirrus
  • raspberry_pi
  • rpi2
  • raspeberry_pi_accessories
  • pi2
Related

Cirrus Logic Audio Card working on the Raspberry Pi 2

e14 Contributor
e14 Contributor over 11 years ago

Hi all!

 

As you might know, Cirrus Logic's main kernel source branch recently switched to 3.18.

My first thought was "Hmm, that means the Cirrus Logic card could finally work on the RPi2..."

I have built a couple of 3.18 kernels for my B+ and RPi2 and I have managed to get both models to produce sound image

 

It's still early days, i.e. there are possibly bugs and glitches to fix, but for those of you who would like to try it out I've made an image file that you can download here:

https://drive.google.com/file/d/0BzIaxMH3N5O1cmJ1bFhMcG1hc0E/view?usp=sharing

The file is a 1.3 GB zip. Uncompressed size is 3.1 GB, so it fits comfortably on a 4 GB card.


The image is based on the standard 2015-02-16-raspbian-wheezy image from the Foundation that you flash to a SD card for a fresh install.

I have only added my kernels and set up the configuration files to get the card going.

It should work on the older B model  with a Wolfson Audio Card too, but I haven't tested that yet.

 

Have fun!

--

Ragnar

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    For good measure, I've put together a tar archive of the 3.18 kernels with Cirrus Logic drivers, that can be installed on top of an existing Raspbian 3.18 installation.

    Download the archive file kernel_3_18_9_W_CL.tgz from here: https://drive.google.com/file/d/0BzIaxMH3N5O1S1FfSGpqYjEwaVk/view?usp=sharing

     

    To install:
    Become root: sudo -s
    Go to root directory: cd /
    Untar the archive: tar xvzf /path/to/where/you/saved/kernel_3_18_9_W_CL.tgz
    Add these lines

    dtparam=spi=on
    dtparam=i2c_arm=on
    dtoverlay=rpi-cirrus-wm5102-overlay

    to the file /boot/config.txt

    On a RPi2B, also add

    kernel=kernel7_CL.img

    or, on all others, add

    kernel=kernel_CL.img

    to /boot/config.txt

     

    Put these lines into /etc/modprobe.d/raspi-blacklist.conf  (create the file if it doesn't exist.)

    softdep arizona-spi pre: arizona-ldo1
    softdep spi-bcm2708 pre: fixed

    Reboot.

     

    If it doesn't work, you can revert to your original kernel by just removing the "kernel=kernel_CL.img" line from /boot/config.txt

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Ragnar:

    Thank you so much for putting this together.  I am up and running with the new kernel.  I am no luck however with the sound and I am putting that on my setup for now.  I have a local install of kodi on RPI2 to be controlled by BubbleUPnp android app, as well a as rpi2 install of BubbleUPnp, which allows to designate kodi as an openhome rendered and then drive the sound to the Onkyo Amp.  This setup worked only with HDMI before.  I am using the Sound configuration on Raspberry Pi with ALSA | Stephen C Phillips to troubleshoot, why I am not getting any sound. 

    Ahmed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    I know nothing about Kodi image

    Have you run any of the "Playback.." scripts to select which output(s) the card should use?

     

    I've noticed there's an experimental build of OpenELEC for the RPi2/Cirrus. Maybe some clues in there...

    http://www.horus.com/~hias/tmp/openelec-wolfson/

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    I have not run the play back scripts.  Thanks for pointing those out.  I think I need to go simple and use the 3.5 mm audio out instead of the digital out and work backwards.  I wish I did not have have to use kodi either.  I just needed a simple media player. I started looking at mpd and somehow ended up with kodi!  Kodi has an audio output area which I need to check again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • marcelheijkoop
    marcelheijkoop over 11 years ago in reply to e14 Contributor

    Hi Ahmed,

    If you use HDMI to your Onkyo receiver,  you do not need to follow any of the CLAC specific setups, nor the card.

    I recommend you look at ready to run image for Kodi, : Xbian. It allowed me to use HDMI sound output withouth too much work

    If you want a headless music player look at TUTORIAL: Installing Squeezelite player on Raspbian | Squeezing a Raspberry Pi

    if you read gerrelts tutorials you will be able to set the output of Squeezelite to the 1) Standard Raspi Analogue port ( fair but not hifi ) 2) HDMI ( but not together with Kodi running )

    or the CLAC as discussed in this forum. Hint:  SL_SOUNDCARD="sysdefault:CARD=sndrpiwsp" in /usr/local/bin/squeezelite_settings.sh

     

    I might experiment on Xbian and this Raspi 2B CLAC kernel later. But for me Kodi is not the preferred Audio renderer.

    Regards Marcel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to marcelheijkoop

    Marcel:

    I did not like the sound out of the box on the HDMI and Onkyo, but I have not done any kind of optimization either.  The sound was kind of boomy and did not have any body to it  I will look at your suggestion for another RPI2 iplmementation, that I will do for another Denon AVR-X2000.  I am not advanced user of Linux, so I had issues using Kodi, when I do remote desktop using XRDP.  So my current setup is MPD/MediaPlayer/BubbleUpnp on RPI2, BubbleUPnP on Notes 2 and then SPDIF connection from CLAC to Onkyo.  The sound is richer.  It still is lacking compared to my 2.1 audiophile setup that I have using a win2012r2/AO/Foorbar2k -> Cambridge Audio Dac Magic Plus -> Adcom.  But I think Raspberry PI can be further improved as I get to learn more from you advanced folks.  Thanks for your note.

     

    Ahmed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • marcelheijkoop
    marcelheijkoop over 11 years ago in reply to e14 Contributor

    Hi Ahmed,

    The HDMI output to the DAC in your receivers should be OK. If this does not sound right to you, I can only think of 2 causes.

    1) The receiver is not up to your specs.

    2) Kodi might to translations to the digital stream that does not preserve the full quality of your audio source.

    But I am not an audiophile, I just need good clear sound and an afordable system.

     

    If you like MPD, you can look at volumio, there might be support for the CLAC by now. At least there a a lot of audiophiles there.

    An other quick start would be squeezeplug, but to my knowledge this had no CLAC support up to about 6 weeks ago.

    Anyway I had bought 2 of the CLACs and have plans with the onboard class-d amp and the proper headset driver.

    While volumio did not deliver on the  multi room promise and has a lagging  user interface....,

    Gerrelt showed me the way to slap a squeeze lite client onto a Pi, and use the LMS on a laptop, and have many setup options to fit almost any wish. ( Read his site )

    Now with the the Pi2 power, running the LMS on the Pi itself becomes more resonable, and this is my direction.

     

    The fine kernel work done here by Regnar and others could be picked up to create easy to start sets.

    I am working on a script that builds Gerrelts examples on Regnars initial image and updates it too with the corrected kernel.

    I might present the script later, but currently it is not at beta stage, and I do not want to share the clumbsy code.

    It fits my purpose to remember and document the steps, and brings back a working setup in 7 minutes.

     

    Marcel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • marcelheijkoop
    marcelheijkoop over 11 years ago in reply to e14 Contributor

    Hi Ahmed,

    The HDMI output to the DAC in your receivers should be OK. If this does not sound right to you, I can only think of 2 causes.

    1) The receiver is not up to your specs.

    2) Kodi might to translations to the digital stream that does not preserve the full quality of your audio source.

    But I am not an audiophile, I just need good clear sound and an afordable system.

     

    If you like MPD, you can look at volumio, there might be support for the CLAC by now. At least there a a lot of audiophiles there.

    An other quick start would be squeezeplug, but to my knowledge this had no CLAC support up to about 6 weeks ago.

    Anyway I had bought 2 of the CLACs and have plans with the onboard class-d amp and the proper headset driver.

    While volumio did not deliver on the  multi room promise and has a lagging  user interface....,

    Gerrelt showed me the way to slap a squeeze lite client onto a Pi, and use the LMS on a laptop, and have many setup options to fit almost any wish. ( Read his site )

    Now with the the Pi2 power, running the LMS on the Pi itself becomes more resonable, and this is my direction.

     

    The fine kernel work done here by Regnar and others could be picked up to create easy to start sets.

    I am working on a script that builds Gerrelts examples on Regnars initial image and updates it too with the corrected kernel.

    I might present the script later, but currently it is not at beta stage, and I do not want to share the clumbsy code.

    It fits my purpose to remember and document the steps, and brings back a working setup in 7 minutes.

     

    Marcel