Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic Audio Card working on the Raspberry Pi 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 165 replies
  • Subscribers 715 subscribers
  • Views 26827 views
  • Users 0 members are here
  • wolfson
  • raspberry
  • audio
  • pi
  • cirrus
  • raspberry_pi
  • rpi2
  • raspeberry_pi_accessories
  • pi2
Related

Cirrus Logic Audio Card working on the Raspberry Pi 2

e14 Contributor
e14 Contributor over 11 years ago

Hi all!

 

As you might know, Cirrus Logic's main kernel source branch recently switched to 3.18.

My first thought was "Hmm, that means the Cirrus Logic card could finally work on the RPi2..."

I have built a couple of 3.18 kernels for my B+ and RPi2 and I have managed to get both models to produce sound image

 

It's still early days, i.e. there are possibly bugs and glitches to fix, but for those of you who would like to try it out I've made an image file that you can download here:

https://drive.google.com/file/d/0BzIaxMH3N5O1cmJ1bFhMcG1hc0E/view?usp=sharing

The file is a 1.3 GB zip. Uncompressed size is 3.1 GB, so it fits comfortably on a 4 GB card.


The image is based on the standard 2015-02-16-raspbian-wheezy image from the Foundation that you flash to a SD card for a fresh install.

I have only added my kernels and set up the configuration files to get the card going.

It should work on the older B model  with a Wolfson Audio Card too, but I haven't tested that yet.

 

Have fun!

--

Ragnar

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    For good measure, I've put together a tar archive of the 3.18 kernels with Cirrus Logic drivers, that can be installed on top of an existing Raspbian 3.18 installation.

    Download the archive file kernel_3_18_9_W_CL.tgz from here: https://drive.google.com/file/d/0BzIaxMH3N5O1S1FfSGpqYjEwaVk/view?usp=sharing

     

    To install:
    Become root: sudo -s
    Go to root directory: cd /
    Untar the archive: tar xvzf /path/to/where/you/saved/kernel_3_18_9_W_CL.tgz
    Add these lines

    dtparam=spi=on
    dtparam=i2c_arm=on
    dtoverlay=rpi-cirrus-wm5102-overlay

    to the file /boot/config.txt

    On a RPi2B, also add

    kernel=kernel7_CL.img

    or, on all others, add

    kernel=kernel_CL.img

    to /boot/config.txt

     

    Put these lines into /etc/modprobe.d/raspi-blacklist.conf  (create the file if it doesn't exist.)

    softdep arizona-spi pre: arizona-ldo1
    softdep spi-bcm2708 pre: fixed

    Reboot.

     

    If it doesn't work, you can revert to your original kernel by just removing the "kernel=kernel_CL.img" line from /boot/config.txt

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    I cant put lines into /etc/modprobe.d/raspi-blacklist.conf 

    When I try to put lines into this directory I open a (only read) and I cant save it. Or it adds a textfile extesion

    Who can give me a guideline to add lines to this directory?

    And can you add to the  /boot/ config.text in the same way?l


    Hugo50


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Hugo

    It sounds as if you do not have write permission of these files.

    Are you new to working with Linux?  If so, let me help.  If not, then ignore me.

     

    If I run the long version of the file list command on the /etc/modprobe.d directory I get ...

     

    pi@raspberrypi ~ $ ls -l /etc/modprobe.d

    total 24

    -rw-r--r-- 1 root root  229 May  8  2013 alsa-base-blacklist.conf

    -rw-r--r-- 1 root root 1186 May  8  2013 alsa-base.conf

    -rw-r--r-- 1 root root  456 Apr 29  2013 fbdev-blacklist.conf

    -rw-r--r-- 1 root root   65 Feb 15  2015 ipv6.conf

    -rw-r--r-- 1 root root  357 Mar 27  2015 oss-compat.conf

    -rw-r--r-- 1 root root   70 Mar 27  2015 raspi-blacklist.conf

    pi@raspberrypi ~ $

     

    This shows that these files are owned by the user 'root'  (The second 'root' tells you that they are also in group root.)

    The -rw-r--r-- tells you the permissions on these files.  Ignore the first dash for now.  The remaining nine characters form three groups of three.  Each group is Read, Write  , eXecute.

    The groups are Owner, group, others in that order.

     

    So the pattern on all these files tells us that the owner, that is root, has read and write permission on the files, but not execute permission.  (rw-)

    Both the group and others only have read permission (r--).

     

    In order to change these files you therefore need to be user root.  You can use the 'su' command to change which user you are - providing that you know root's password, or you can use the sudo command to temporally change who you are while running the command.

     

    So to edit the raspi-blacklist.conf file you could run the command :-

    sudo nano /etc/modprobe.d/raspi-blacklist.conf

     

    OK?

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Hugo

    It sounds as if you do not have write permission of these files.

    Are you new to working with Linux?  If so, let me help.  If not, then ignore me.

     

    If I run the long version of the file list command on the /etc/modprobe.d directory I get ...

     

    pi@raspberrypi ~ $ ls -l /etc/modprobe.d

    total 24

    -rw-r--r-- 1 root root  229 May  8  2013 alsa-base-blacklist.conf

    -rw-r--r-- 1 root root 1186 May  8  2013 alsa-base.conf

    -rw-r--r-- 1 root root  456 Apr 29  2013 fbdev-blacklist.conf

    -rw-r--r-- 1 root root   65 Feb 15  2015 ipv6.conf

    -rw-r--r-- 1 root root  357 Mar 27  2015 oss-compat.conf

    -rw-r--r-- 1 root root   70 Mar 27  2015 raspi-blacklist.conf

    pi@raspberrypi ~ $

     

    This shows that these files are owned by the user 'root'  (The second 'root' tells you that they are also in group root.)

    The -rw-r--r-- tells you the permissions on these files.  Ignore the first dash for now.  The remaining nine characters form three groups of three.  Each group is Read, Write  , eXecute.

    The groups are Owner, group, others in that order.

     

    So the pattern on all these files tells us that the owner, that is root, has read and write permission on the files, but not execute permission.  (rw-)

    Both the group and others only have read permission (r--).

     

    In order to change these files you therefore need to be user root.  You can use the 'su' command to change which user you are - providing that you know root's password, or you can use the sudo command to temporally change who you are while running the command.

     

    So to edit the raspi-blacklist.conf file you could run the command :-

    sudo nano /etc/modprobe.d/raspi-blacklist.conf

     

    OK?

     

    David