Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic Audio Card working on the Raspberry Pi 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 165 replies
  • Subscribers 715 subscribers
  • Views 27004 views
  • Users 0 members are here
  • wolfson
  • raspberry
  • audio
  • pi
  • cirrus
  • raspberry_pi
  • rpi2
  • raspeberry_pi_accessories
  • pi2
Related

Cirrus Logic Audio Card working on the Raspberry Pi 2

e14 Contributor
e14 Contributor over 11 years ago

Hi all!

 

As you might know, Cirrus Logic's main kernel source branch recently switched to 3.18.

My first thought was "Hmm, that means the Cirrus Logic card could finally work on the RPi2..."

I have built a couple of 3.18 kernels for my B+ and RPi2 and I have managed to get both models to produce sound image

 

It's still early days, i.e. there are possibly bugs and glitches to fix, but for those of you who would like to try it out I've made an image file that you can download here:

https://drive.google.com/file/d/0BzIaxMH3N5O1cmJ1bFhMcG1hc0E/view?usp=sharing

The file is a 1.3 GB zip. Uncompressed size is 3.1 GB, so it fits comfortably on a 4 GB card.


The image is based on the standard 2015-02-16-raspbian-wheezy image from the Foundation that you flash to a SD card for a fresh install.

I have only added my kernels and set up the configuration files to get the card going.

It should work on the older B model  with a Wolfson Audio Card too, but I haven't tested that yet.

 

Have fun!

--

Ragnar

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    For those interested I've uploaded the following packages to my Raspbian repository (http://rpi.autostatic.com/):

    • linux-image-cirrus: meta package that installs a kernel with Wolfson/Cirrus Logic audio interface support
    • cirrus-config-overlay: package that installs the device tree overlay file for the Wolfson/Cirrus Logic audio interface
    • cirrus-config-modprobe: package that installs the modprobe config file for the Wolfson/Cirrus Logic audio interface
    • cirrus-config-scripts: package that installs the playback, record and reset scripts for use with the Wolfson/Cirrus Logic audio interface
    • cirrus-config: meta package that installs all the above packages

    If anyone is interested in testing these packages, go ahead, feedback is greatly appreciated. On a clean Raspbian install adding my repo, installing the cirrus-config package and rebooting your RPi should enable the Wolfson/Cirrus Logic audio interface. No need to edit any config files.

     

    Jeremy

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    I tried, jeremy. it rendered my pi (temporarily) unusable after reboot. something must have gone wrong, I figure. this was a (quite fresh) 2015-05-05 image on a pi2.

    fortunately I have a spare sd card where I will put the clean image onto and see where I can find a difference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Markus, sorry about that. I already know what the cause is, working on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    jeremy, no problem. any quick hint for me to fix that manually while you prepare new debs? don't have access to the file system right now, though (I could, of course, boot the spare card and access the other via usb card reader).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    You will need to comment the

    kernel=vmlinuz-3.18.9-cirrus

    line in /boot/config.txt so that your RPi loads kernel7.img again. So you will need to access the file system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    well, that part was easy. you can access it via the fat32 partition even in windows and modify that file. I was afraid I had to fiddle with the ext3 (or 4).

    it's up again (could have figure myself, of course image ), but thanks anyway! awaiting the updated packages now...

     

    -greetings, markus-

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Markus, I've updated the packages. Thanks a lot for testing and providing feedback!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    the update went fine until it reached the point where the hardlink to the initrd bak file is supposed to be created. then it bails out.it booted fine after that, but I realized that this is the standard 3.18.11 kernel.

    the package update does not comment the alternate kernel and overlay back in, so I did. but after that it doesn't boot again. any helping information I should provide?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    the update went fine until it reached the point where the hardlink to the initrd bak file is supposed to be created. then it bails out.it booted fine after that, but I realized that this is the standard 3.18.11 kernel.

    the package update does not comment the alternate kernel and overlay back in, so I did. but after that it doesn't boot again. any helping information I should provide?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    That shouldn't happen, I probably made a mistake somewhere. The problem

    is that /boot lives on a FAT32 partition and apt/dpkg doesn't really

    like that. I have to work a bit around that limitation and the solution

    I'm using now is a bit hacky and apparently it doesn't work flawlessly

    yet. If you could provide me with the warnings/error messages that'd be

    great.

     

    Jeremy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    the hardlink creation fails with "permission denied" - it happens in /boot where the fat32 is mapped into, then. while the alternate kernel is commented in, you'll see colour gradient screen only. it doesn't even try to boot that kernel.

    either there is some additional magic used to tell the pi to boot that specific kernel, or it just doesn't find it (as it recognises the vanilla kernel that obviously doesn't even have to be referenced in the config.txt).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Found the problem and I'll fix it. The linux-cirrus-image package merrily does a rm -f *3.18.9*cirrus on install but should only do that on upgrade. Thanks again for the feedback.