Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic Audio Card working on the Raspberry Pi 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 165 replies
  • Subscribers 715 subscribers
  • Views 26929 views
  • Users 0 members are here
  • wolfson
  • raspberry
  • audio
  • pi
  • cirrus
  • raspberry_pi
  • rpi2
  • raspeberry_pi_accessories
  • pi2
Related

Cirrus Logic Audio Card working on the Raspberry Pi 2

e14 Contributor
e14 Contributor over 11 years ago

Hi all!

 

As you might know, Cirrus Logic's main kernel source branch recently switched to 3.18.

My first thought was "Hmm, that means the Cirrus Logic card could finally work on the RPi2..."

I have built a couple of 3.18 kernels for my B+ and RPi2 and I have managed to get both models to produce sound image

 

It's still early days, i.e. there are possibly bugs and glitches to fix, but for those of you who would like to try it out I've made an image file that you can download here:

https://drive.google.com/file/d/0BzIaxMH3N5O1cmJ1bFhMcG1hc0E/view?usp=sharing

The file is a 1.3 GB zip. Uncompressed size is 3.1 GB, so it fits comfortably on a 4 GB card.


The image is based on the standard 2015-02-16-raspbian-wheezy image from the Foundation that you flash to a SD card for a fresh install.

I have only added my kernels and set up the configuration files to get the card going.

It should work on the older B model  with a Wolfson Audio Card too, but I haven't tested that yet.

 

Have fun!

--

Ragnar

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi, I followed the building instructions on github and replaced the kernel in Ubuntu https://ubuntu-mate.community/t/ubuntu-mate-15-04-for-raspberry-pi-2/517/101

     

    Now I would like to stream the spdif input directly to my speakers (analog or via USB sound card)

     

    I tried to test spdif capturing with the sh skript, but only got a mute audio file.

    Is it normal that pulseaudio only recognizes the analog output but not the inputs of the cirrus card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi, I followed the building instructions on github and replaced the kernel in Ubuntu https://ubuntu-mate.community/t/ubuntu-mate-15-04-for-raspberry-pi-2/517/101

     

    Now I would like to stream the spdif input directly to my speakers (analog or via USB sound card)

     

    I tried to test spdif capturing with the sh skript, but only got a mute audio file.

    Is it normal that pulseaudio only recognizes the analog output but not the inputs of the cirrus card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • marcelheijkoop
    marcelheijkoop over 11 years ago in reply to e14 Contributor

    Hi Some One.

     

    Perhaps stating the obvious, but have you run the 'wolfson' scripts to setup the recording paths?

    SPDIF_record.sh should be in /home/pi if you use the ragnar image.

    The Cirrus logic image contained something similar If I remember correct.

    Edit : OOPS you did use the script , ...sorry

     

    BTW If you would be able to compile the Cirrus Logic patches into a tinycore kernel.... :-) I would love to test it for you.

    A headless player with the CLAC that can not corrupt its card is the next level for me.

    MH

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    kickass

    Now I would like to stream the spdif input directly to my speakers (analog or via USB sound card)

    I made a couple of scripts to route sound directly on the Wolfson card. I think they work on the Cirrus card too.

    http://www.element14.com/community/message/114756/l/re-read-in-from-the-headset-jack-and-read-out-to-the-amplifier#11475…

    One of them connects S/PDIF In to Line Out.

     

    Is it normal that pulseaudio only recognizes the analog output but not the inputs of the cirrus card?

    No idea at all, I've never used pulseaudio. Have you tried recording without using pulse?

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Ragnar,

    I'm a bit confused I'm afraid! I saw your .deb files and tried to install the drivers with these .deb file. The package was installed, but thats obviously not enough to get the card working. So could you tell us the steps to follow to get the card working? Do i also need the .tar files? Please forgive me if this is a stupid question. The method with the .tar files only worked for me perfectly.

     

    Thanks for your great work!

     

    Thomas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Thomas!

     

    No, you don't need the .tar file, but you have to make the same kind of changes to the configuration files.

    After you have installed  the .deb package, add these lines

     

    dtparam=spi=on
    dtparam=i2c_arm=on
    dtoverlay=rpi-cirrus-wm5102-overlay

    to the file /boot/config.txt

     

    On a RPi2B, also add

    kernel=vmlinuz-3.18.9-v7cludlmmapfll

     

    or, on all others, add

     

    kernel=vmlinuz-3.18.9cludlmmapfll

    to /boot/config.txt

     

    Put these lines into /etc/modprobe.d/raspi-blacklist.conf  (create the file if it doesn't exist.)

    softdep arizona-spi pre: arizona-ldo1
    softdep spi-bcm2708 pre: fixed

     

    EDIT to add: You  also need the overlay file rpi-cirrus-wm5102-overlay.dtb if you don't already have it in /boot/overlays. You can extract the tar file in some temporary location and then copy the overlay file from it to /boot/overlays.

    --

    Ragnar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Ragnar,

    that was the missing part! It's running now!

     

    Thanks for the good work and your kind support!

     

    Thomas