Raspberry Pi Forum Raspi 2 sure is a finicky bit of tech.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 681 subscribers
  • Views 1118 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Raspi 2 sure is a finicky bit of tech.

Former Member
Former Member over 10 years ago

Boy, a few of my microSDs that worked on my version 1 don't work on the version 2.  Aand this after I followed instructions for once!

 

I got it running with Openelec though.

 

Thanks E14 for the free Raspi2!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 10 years ago

    If you had followed directions you would have known that micro SDs from version 1 don't work on version 2.

     

    Even though you got it working, you will benefit from reading this (everyone needs to read it!):

     

    http://www.raspberrypi.org/forums/viewtopic.php?f=28&t=58151

     

     

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    But the components from other models can run on Raspberry 2 ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    Yes. The RPi 2 is the same footprint, size shape, fits the b+ case, can use the camera, has the same 40 pinouts uses the same usb options (wipi, etc) its compatible with the b+

     

    But, the SD card needs to be setup for the RPi 2. I recommend NOOBS (1.4... for the RPi 2) and load Raspbian. Don't try to use your RPi b+ SD card in the RPi 2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    The issue is simply that Linux distros (E.g. Raspbian) tend to update the file system mounted at / with hardware information.  That is why you should save your critical personal files on to a USB stick, rebuild the MicroSD, and re-install.  You can even rebuild  on Pi 2 from an old img file using `dd`, just like you did originally.

     

    Think of it this way: Would you ever plug an existing HDD or SSD into a new computer as-is and expect it to work?  Same idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    The issue is simply that Linux distros (E.g. Raspbian) tend to update the file system mounted at / with hardware information.  That is why you should save your critical personal files on to a USB stick, rebuild the MicroSD, and re-install.  You can even rebuild  on Pi 2 from an old img file using `dd`, just like you did originally.

     

    Think of it this way: Would you ever plug an existing HDD or SSD into a new computer as-is and expect it to work?  Same idea.