Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum ad hoc Netzwerk mit Raspberry Pi Model B
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 676 subscribers
  • Views 2250 views
  • Users 0 members are here
  • adhoc
  • raspberry
  • arp
  • routing
  • manet
Related

ad hoc Netzwerk mit Raspberry Pi Model B

Former Member
Former Member over 10 years ago

Hallo

 

Ich versuche ein Ad-hoc Meshnetz mittels 4 Raspberry Pi's Model B aufzubauen. Hier sind die Hardware Eigenschaften:

  • 4x Raspberry Pi Model B ( Raspbian Debian Wheezy 3.18)
  • 4x Edimax EW-7811Un USB WiFi Adapter (RTL8188cus)
  • 1x Laptop mit Win 8.1 um auf die RPi's über SSH (PuTTY) zuzugreifen

 

 

ich habe die RPi Netzwerkeinstellungen wie folgend konfiguriert:

/etc/network/interfaces

RPi1

auto lo
iface lo inet loopback
iface eth0 inet dhcp

auto wlan0
allow-hotplug wlan0
iface wlan0 inet static
  address 192.168.1.21
  netmask 255.255.255.0
  wireless-channel 1
  wireless-essid RPiAdHocNetwork
  wireless-mode ad-hoc

 

RPi2

auto lo
iface lo inet loopback
iface eth0 inet dhcp

auto wlan0
allow-hotplug wlan0
iface wlan0 inet static
  address 192.168.1.22
  netmask 255.255.255.0
  wireless-channel 1
  wireless-essid RPiAdHocNetwork
  wireless-mode ad-hoc

 

RPi3

auto lo
iface lo inet loopback
iface eth0 inet dhcp

auto wlan0
allow-hotplug wlan0
iface wlan0 inet static
  address 192.168.1.23
  netmask 255.255.255.0
  wireless-channel 1
  wireless-essid RPiAdHocNetwork
  wireless-mode ad-hoc

 

RPi4

auto lo
iface lo inet loopback
iface eth0 inet dhcp

auto wlan0
allow-hotplug wlan0
iface wlan0 inet static
  address 192.168.1.24
  netmask 255.255.255.0
  wireless-channel 1
  wireless-essid RPiAdHocNetwork
  wireless-mode ad-hoc

 

Laptop

IP: 192.168.1.20
Subnet: 255.255.255.0
Mode: Ad-hoc

 


Das pingen vom Laptop --> RPi's funktioniert

C:\> ping 192.168.1.21

Ping wird ausgeführt für 192.168.1.21 mit 32 Bytes Daten:
Antwort von 192.168.1.21: Bytes=32 Zeit=1ms TTL=64
Antwort von 192.168.1.21: Bytes=32 Zeit=1ms TTL=64
Antwort von 192.168.1.21: Bytes=32 Zeit=2ms TTL=64
Antwort von 192.168.1.21: Bytes=32 Zeit=1ms TTL=64

Ping-Statistik für 192.168.1.21:
    Pakete: Gesendet = 4, Empfangen = 4, Verloren = 0
    (0% Verlust),
Ca. Zeitangaben in Millisek.:
    Minimum = 1ms, Maximum = 2ms, Mittelwert = 1ms

 

das Pingen vom RPi --> Laptop funktioniert auch

pi@rpi1 ~ $ ping 192.168.1.20
PING 192.168.1.20 (192.168.1.20) 56(84) bytes of data.
64 bytes from 192.168.1.20: icmp_req=1 ttl=128 time=1.37 ms
64 bytes from 192.168.1.20: icmp_req=2 ttl=128 time=1.24 ms
64 bytes from 192.168.1.20: icmp_req=3 ttl=128 time=1.25 ms
64 bytes from 192.168.1.20: icmp_req=4 ttl=128 time=15.6 ms
64 bytes from 192.168.1.20: icmp_req=5 ttl=128 time=1.42 ms
64 bytes from 192.168.1.20: icmp_req=6 ttl=128 time=1.28 ms
^C
--- 192.168.1.20 ping statistics ---
6 packets transmitted, 6 received, 0% packet loss, time 5007ms
rtt min/avg/max/mdev = 1.242/3.710/15.683/5.354 ms

 

Das Problem ist, dass ich von einem RPi zum anderen nicht direkt pingen kann.

pi@rpi1 ~ $ ping 192.168.1.22
PING 192.168.1.22 (192.168.1.22) 56(84) bytes of data.
From 192.168.1.21 icmp_seq=1 Destination Host Unreachable
From 192.168.1.21 icmp_seq=2 Destination Host Unreachable
From 192.168.1.21 icmp_seq=3 Destination Host Unreachable
From 192.168.1.21 icmp_seq=4 Destination Host Unreachable
From 192.168.1.21 icmp_seq=5 Destination Host Unreachable
From 192.168.1.21 icmp_seq=6 Destination Host Unreachable
^C
--- 192.168.1.22 ping statistics ---
7 packets transmitted, 0 received, +6 errors, 100% packet loss, time 6004ms
pipe 3

 

Hat jemand vielleicht eine Idee wie ich die RPi's mit einander zu kommunizieren bringen könnte? vielen dank im voraus


Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • clem57
    clem57 over 10 years ago

    Add to each RPi:

    gateway: 192.168.1.20

    Now that will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to clem57

    I appreciate your suggestion. but what if I would ping a Pi with another Pi in the same subnet without a defult gateway? isn't that the main task of a an adhoc network ?

    my goal is to build a mesh network with RPi's and make them able to transport packets through each other ( same as in mobile adhoc mesh network MANET) by multihop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to clem57

    I appreciate your suggestion. but what if I would ping a Pi with another Pi in the same subnet without a defult gateway? isn't that the main task of a an adhoc network ?

    my goal is to build a mesh network with RPi's and make them able to transport packets through each other ( same as in mobile adhoc mesh network MANET) by multihop.