Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Human body temperature sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 2194 views
  • Users 0 members are here
  • body_temperature
  • raspberry_pi
  • raspberry-pi
  • ds1624
  • temperature_measurement
  • temperature_sensor
Related

Human body temperature sensor

balearicdynamics
balearicdynamics over 11 years ago

Hello all!

 

I have a question, no idea if this is obvious or it is a complex one. I have to setup a temperature body measurement sensor, that will be based on the high precision with memory IC DS1624 (see attached datasheet).

The question is almost simple to explain: I need to find the way to convert this IC in a sensor. At the actual date I see a possible option but I am not sure if it is the best or there are other alternatives. The idea is explained below:

 

The probe itself includes the IC in a hosting container of the adequate characteristics; the idea is a good thermal transmission metallic end in contact in some way with the IC (maybe direct contact with the thermal conducting paste used for the CPU coolers?) So the entire probe has the cables reaching the processing device with a ground shielded cable of a length between 50 and 100 cm.

 

Some suggestion more reliable ?

 

Thanks in advance. Enrico

Attachments:
imageDS1624.pdf
  • Sign in to reply
  • Cancel
Parents
  • kas.lewis
    0 kas.lewis over 11 years ago

    Hello,

     

    If you look over the sudden impact challenge on here you should find a good few examples as all of those used the body temperature as part of their solution.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 11 years ago

    Hello,

     

    If you look over the sudden impact challenge on here you should find a good few examples as all of those used the body temperature as part of their solution.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to kas.lewis

    Kas, it is very difficult to find something in detail without reading the ton of posts there image