Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Use as a guitar pedal.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 2260 views
  • Users 0 members are here
  • logic
  • audio
  • guitar
  • cirrus
  • line
  • raspberry_pi
  • raspeberry_pi_accessories
  • noise
  • card
  • out
  • pedal
Related

Use as a guitar pedal.

e14 Contributor
e14 Contributor over 11 years ago

I was hoping to use the Cirrus board as a digital effects guitar pedal. I was planning on using line in and line out since the connections make things very simple. However, I have run into some problems with the line out to guitar amplifier connection. First of all, though, I tried recording through line in. When I played what I recorded through my computer speakers it sounded pretty good. When I connected the line out to my guitar amps (Vox AC15C1 / Marshall MG15FX) it had a significant amount of noise coming from the board. I then thought it might be the cord. I tested this by connecting my laptop to my amp with the same cord and playing the same file from my laptop, but this time there was no noise. I checked and the output impedance of the RPi and the Vox are both 15 ohms. One thing I was thinking might be a problem was the max capacitive load for the line out, which was 2 nF, but I haven't been able to find anything about that related to the Vox.

 

So does anyone know what could be causing noise from the line out only when it is connected to a guitar amplifier? And has anyone tried to use the Cirrus board with the RPi as a guitar pedal?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 11 years ago

    I'm a bit confused about the shared ground and ground loop comments.

     

    Isn't the Pi's power supply isolated - Not connected to your house's ground?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 11 years ago

    I'm a bit confused about the shared ground and ground loop comments.

     

    Isn't the Pi's power supply isolated - Not connected to your house's ground?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • sqkybeaver
    0 sqkybeaver over 11 years ago in reply to Jan Cumps

    when everything is grounded separate points, eg; amp at wall socket, rpi on another socket. there can be a potential(voltage) difference at between these points when they should be the same potential(ground in this case), this will cause current to flow between these points.


    the idea of the transformer is to isolate the grounds from each other to eliminate any ground current between these spots. this can be a deadly problem in certain situations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 11 years ago in reply to sqkybeaver

    But is that Pi grounded? Isn't Ryan using your typical isolated power supply for the Pi?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sqkybeaver
    0 sqkybeaver over 11 years ago in reply to Jan Cumps

    most wall-wart supply's are floating outputs. very very very few have one or the other output tied to mains ground(earth) the cheaper phone charger types are switching and are not guaranteed to be clean, or safe.

     

    Ryan, what power supply are you using?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to sqkybeaver

    I'm using this guy: http://www.mcmelectronics.com/product/DISTRIBUTED-BY-MCM-MWS158-0502200UC-MIC-/28-17985?t=2&utm_expid=8634549-27.0czCl7fSQamjILoiAH9mgA.1&utm_referrer=https%3A%2F%2Fwww.google.com%2F

     

    I'm a little confused about why the transformer would help. How would it isolate the grounds from each other, and, I might be reading it wrong, I feel like I want the grounds to be connected. Also I'm not exactly sure what I'm looking for. It seems that a suitable transformer may be over $50 or under $10 (suitable transformer for an audio isolation transformer?). Here is another one that seems more focused on guitars: GuitarCenter

     

    To Joey: if I'm able to get it working I would be very happy to post the info about what I did, however it seems like I have a lot of work to and I'm headed back to college tomorrow, so I'm not sure I'll have a ton of time to make significant progress over the next couple of months.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sqkybeaver
    0 sqkybeaver over 11 years ago in reply to e14 Contributor

    the power supply you are using is a switching(switch mode), while they are typically more efficient, and cheaper(smaller parts) than a linear type, but they follow the two out of three rule, they are going to be noisy compared to linear supplies. you can put a ferrite core around the end of the power supply cable, this may reduce some of the noise from the wall wart. http://www.newark.com/ferrites-split-core?searchRef=SearchLookAhead

     

    most all transformers do not have electrical connection between the primary and secondary windings. this is where the isolation comes from. as long as the two grounds are not connected together external to the transformer.

     

    can you tell what frequency the noise is?