Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Use as a guitar pedal.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 2264 views
  • Users 0 members are here
  • logic
  • audio
  • guitar
  • cirrus
  • line
  • raspberry_pi
  • raspeberry_pi_accessories
  • noise
  • card
  • out
  • pedal
Related

Use as a guitar pedal.

e14 Contributor
e14 Contributor over 11 years ago

I was hoping to use the Cirrus board as a digital effects guitar pedal. I was planning on using line in and line out since the connections make things very simple. However, I have run into some problems with the line out to guitar amplifier connection. First of all, though, I tried recording through line in. When I played what I recorded through my computer speakers it sounded pretty good. When I connected the line out to my guitar amps (Vox AC15C1 / Marshall MG15FX) it had a significant amount of noise coming from the board. I then thought it might be the cord. I tested this by connecting my laptop to my amp with the same cord and playing the same file from my laptop, but this time there was no noise. I checked and the output impedance of the RPi and the Vox are both 15 ohms. One thing I was thinking might be a problem was the max capacitive load for the line out, which was 2 nF, but I haven't been able to find anything about that related to the Vox.

 

So does anyone know what could be causing noise from the line out only when it is connected to a guitar amplifier? And has anyone tried to use the Cirrus board with the RPi as a guitar pedal?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi all, sorry I just moved back to college (junior year) and was without internet for a while.

     

    When I first was trying out the RPi it was powered from a PC and that was really noisy.

     

    Are there any suggestions for an audio isolating transformer? One of my friends has a Voodoo lab pedal power 2 plus for his

    pedal board (which I think includes the audio isolating transformer), but I don't have enough pedals to justify buying something like that (for now at least).

     

    Also, there is virtually no noise when I plug the RPi into the same power strip as my amp, so the noise isn't too much of a problem,

    I'm just nervous after hearing how potentially bad not having an audio isolating transformer can be.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi all, sorry I just moved back to college (junior year) and was without internet for a while.

     

    When I first was trying out the RPi it was powered from a PC and that was really noisy.

     

    Are there any suggestions for an audio isolating transformer? One of my friends has a Voodoo lab pedal power 2 plus for his

    pedal board (which I think includes the audio isolating transformer), but I don't have enough pedals to justify buying something like that (for now at least).

     

    Also, there is virtually no noise when I plug the RPi into the same power strip as my amp, so the noise isn't too much of a problem,

    I'm just nervous after hearing how potentially bad not having an audio isolating transformer can be.