Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Best device for Gigabit Ethernet traffic testing and WiFi Site Surveying
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 706 subscribers
  • Views 2741 views
  • Users 0 members are here
  • wifi
  • raspberry_pi
  • raspberry-pi
  • networking
Related

Best device for Gigabit Ethernet traffic testing and WiFi Site Surveying

bobalexander
bobalexander over 10 years ago

Hi everyone!

I am currently using a Raspberry Pi 2 running IPERF https://iperf.fr/ to test bandwidth on a WiFi/LAN network.

As the Pi is only 100Mbps I am only able to exercise tests up to the 100M mark (~96 Mbits/sec).

 

Is anyone aware of a better small platform that I could setup iperf on to run tests at a higher bandwidth?

Ideally, it could run at GigE speeds but my current needs only require ~450Mbps for 802.11n WiFi testing.

BTW, this is nothing permanent or attached to a production network so security is not a concern.

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • bobalexander
    0 bobalexander over 10 years ago

    In case anyone is interested, I have ran a few tests while connected to the AP at 5.8Ghz 802.11n (450Mbps)

    image

    I was able to average 133.125 Mbits/sec with a peak of 144 Mbits/sec with no tuning or tweaking:

     

     

    iperf-2.0.5-3-win32>iperf -c 192.168.0.7 -r

    ------------------------------------------------------------

    Server listening on TCP port 5001

    TCP window size: 63.0 KByte (default)

    ------------------------------------------------------------

    ------------------------------------------------------------

    Client connecting to 192.168.0.7, TCP port 5001

    TCP window size: 63.0 KByte (default)

    ------------------------------------------------------------

    [  4] local 192.168.0.6 port 49208 connected with 192.168.0.7 port 5001

    [ ID] Interval       Transfer     Bandwidth

    [  4]  0.0-10.0 sec   152 MBytes   128 Mbits/sec

    [  4] local 192.168.0.6 port 5001 connected with 192.168.0.7 port 41371

    [  4]  0.0-10.0 sec   172 MBytes   144 Mbits/sec

    ------------------------------------------------------------

    [  4] local 192.168.0.6 port 49209 connected with 192.168.0.7 port 5001

    [ ID] Interval       Transfer     Bandwidth

    [  4]  0.0-10.0 sec   163 MBytes   136 Mbits/sec

    [  4] local 192.168.0.6 port 5001 connected with 192.168.0.7 port 41372

    [  4]  0.0-10.0 sec   151 MBytes   127 Mbits/sec

    ------------------------------------------------------------

    [  4] local 192.168.0.6 port 49211 connected with 192.168.0.7 port 5001

    [ ID] Interval       Transfer     Bandwidth

    [  4]  0.0-10.0 sec   160 MBytes   134 Mbits/sec

    [  4] local 192.168.0.6 port 5001 connected with 192.168.0.7 port 41373

    [  4]  0.0-10.1 sec   142 MBytes   118 Mbits/sec

    ------------------------------------------------------------

    [  4] local 192.168.0.6 port 49212 connected with 192.168.0.7 port 5001

    [ ID] Interval       Transfer     Bandwidth

    [  4]  0.0-10.0 sec   165 MBytes   139 Mbits/sec

    [  4] local 192.168.0.6 port 5001 connected with 192.168.0.7 port 41374

    [  4]  0.0-10.0 sec   166 MBytes   139 Mbits/sec

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to bobalexander

    was the source on the WIFI as well or connected via copper?

     

    Also are you sure the USB WIFI adaptor is capable of using all that bandwidth offered..

    Personally I think that's very good either way getting a 1/3 of the max available bandwidth in real life!

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 10 years ago in reply to bobalexander

    was the source on the WIFI as well or connected via copper?

     

    Also are you sure the USB WIFI adaptor is capable of using all that bandwidth offered..

    Personally I think that's very good either way getting a 1/3 of the max available bandwidth in real life!

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bobalexander
    0 bobalexander over 10 years ago in reply to Problemchild

    The source (Banana Pi) in the WiFi test was connected to the AP (Cisco 2702i in autonomous mode) via GigE copper straight in.

    The WiFi adapter in my laptop is an internal PCI Express Half Mini Card (Intel - Centrino Ultimate-N 6300 AGN).