Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Server - Other Alternatives.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 42 replies
  • Answers 2 answers
  • Subscribers 713 subscribers
  • Views 6738 views
  • Users 0 members are here
  • raspberry
  • intel
  • helpme
  • servers
  • single_board_computer
  • single_board_computers
  • raspberrypi
  • server
  • arduino
Related

Raspberry Pi Server - Other Alternatives.

e14 Contributor
e14 Contributor over 10 years ago

Hi All,

 

I was just wondering if there are any other single board computers like the Raspberry Pi which would allow me to create a Storage/Cloud server by connecting a external hard drive. I am kind of new to this and would like to work with simple boards to help get me started. Has anyone has come across tutorials that would help me or done a similiar sort of project and if this is actaully do able.

 

I was thinking of using the Intel Galileo Gen 2 or the Arduino Uno

 

Any feedback and recommendations would be greatly appreciated.

 

Many Thanks in Advance.

 

Omar.

  • Sign in to reply
  • Cancel
Parents
  • eugenenine
    0 eugenenine over 10 years ago

    I have a Pi B and Pi2 B.  The Pi B ran into performance issues with Owncloud but the 2 runs it well.  I run Owncloud on the 2 with a dynamic DNS client and web exposed and we have 4 phones, two tablets and 6 computers syncing with it.  The Pi runs my internal server with a 1TB drive.  It holds all our other documents, pictures, music, etc that's not on Owncloud.  It's the older stuff that I don't keep synced.  It's also the backup server for the Owncloud pi2.  The internal shares all its data via samba for the windows clients and NFS for the Linux clients and minidlna allows standalone devices like a blueray player to access the media as well.

    The orange Pi, period, beaglebone, or small x86 systems such as miniityx boards are all alternatives but the Pi2 works well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • eugenenine
    0 eugenenine over 10 years ago

    I have a Pi B and Pi2 B.  The Pi B ran into performance issues with Owncloud but the 2 runs it well.  I run Owncloud on the 2 with a dynamic DNS client and web exposed and we have 4 phones, two tablets and 6 computers syncing with it.  The Pi runs my internal server with a 1TB drive.  It holds all our other documents, pictures, music, etc that's not on Owncloud.  It's the older stuff that I don't keep synced.  It's also the backup server for the Owncloud pi2.  The internal shares all its data via samba for the windows clients and NFS for the Linux clients and minidlna allows standalone devices like a blueray player to access the media as well.

    The orange Pi, period, beaglebone, or small x86 systems such as miniityx boards are all alternatives but the Pi2 works well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to eugenenine
    I have a Pi B and Pi2 B.  The Pi B ran into performance issues with Owncloud but the 2 runs it well.


    This is just the point. To make a project is more than acceptable to choose the better performances / prices hardware; but if the project should really work for a long time, maybe the worth to invest few more $ and buy a more reliable than super-cheap device anyway.

    To make a server IMHO it is different, especially when the server should serve image This is the reason that in cases like this I wait until there is not the right budget (or I induce a client) and make the better choice respect the absolute cheaper.


    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to balearicdynamics

    On the other hand, for someone gaining experience, first getting the cheapest option is a good way to learn "what is needed".

     

    Example: I had never owned a tablet. What use would I have for one??? Got one of the cheapest, found out what the thing is useful for, and that I need a bit more performance. You can argue that maybe I should have gotten the more performant one immediately. But that's not true: I didn't know what "extra performance" I needed. Better screen resolution? More RAM? More storage? Back then I didn't know, now I do.

     

    Similar case here. Getting the cheapest option first will allow you to learn where that option is lacking **in your case**. Of course if from the outset you can predict it won't satisfy the intended use-case, then it's no use. But if the use-case is vague, unpredictable or may expand in the future, then "maybe this will suffice" and getting the cheapest option is a good way to gain experience in figuring out what you need in the end.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to rew

    Almost correct Wolff, but first of all this is not an "unpredictable case" as the user explicitly asked suggestions on making a server.

     

    IMHO there are some braking lines where you can't go down in every case. Especially for newbies and there is a reason, supposing that the newbie is not lazying trying just for fun and just because he has nothing better to do (no good films, no friends to go with to the pub, bored of bowling image ); when a guy, a very young guy max 6-7 years ask to his parents to play guitar the most probable thing they do if decide to buy a guitar to him is to find a crap just-few-more-than-a-toy guitar. He start playing, study and discover that guitar has a so bad sound that it's no worth. But is the guitar playing bad also when the kid has a sufficient knowledge to play something well. The same is the tablet you never owned. sure it is not the worth you buy a super device investing 5-600$ but if you just try with a Android 2.3 25$ tablets it is very probable that you abandon because you are so far from what a tablet toady is that you continue without any idea.

     

    There is also another aspect, involving the budget. Suppose that you decide to make a server and buy a 177$ Gizmo2 or 79$ SBC like the last XU4. Then you add .... 40$ for a fast 500 Mb HDD USB3. You have spent an amount between 200 and 250$. You have a server, that is what you want, reliable and with good performances. Then you come happy and buy a second HDD and invest another 40$. You have again a server, based on a good SBC and better. And so on.

     

    Instead it is not rare that trying with several low cost devices, adding components, making tests with a platform not useful to reach the goal the expenses count at the end of the experiments result higher than what expected.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to balearicdynamics

    Agreed. Again: If you can easily predict that the "cheapest option" will be lacking in some respect, then you should immediately get the more advanced/expensive option.

     

    You're saying "server". You have an image with "server" that may not be the same as what the thread-starter wants/needs.

     

    If "server" means: "a system that can download movies in the background and then serve them on-demand to a media player on my network", then a $35 raspberry pi will suffice. Sure the raspberry pi has lousy disk-performance. But does that hinder the background downloading? No! Does it influence the media streaming at all? No! Of course the disk and ethernet performance come into play if you want to move big files between your PC and the "server", but if you never do that, why spend the extra money on that?


    Often you can get a $35 option and "twice as much" for a little extra, say $40. Then even if you don't know what it would be useful for, you might chose to get the bigger option. Now in this case the choice seems to be a $35 raspberry pi or a $70 XU4. You might think that this is quite a jump. But if you count all the extras, SD card, powersupply, harddisks the difference is much less than 50%. The small price-increase might be acceptable for some people even if they don't really know right now if it will be useful, but for others the difference is significant.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to eugenenine

    A small mini-ITX is around 20-30£ and the PSU is another 10£++ obviously this is somewhat more than a RPI but there is so much more computing power available than an RPI and so easy to use then often it should win hands down.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to rew
    You're saying "server". You have an image with "server" that may not be the same as what the thread-starter wants/needs.


    This maybe, I have considered this possibility but why not use the correct terms for the things?

    Anyway, in the case I have to build a media server (that is lightweight than a traditional server for sure), I should provide at least:

    • Good transfer speed because good videos and films today are streamed in MKV format that occupy some giga of space. Try to transfer on a 10/100 lan or with an external USB 2 HDD just only 10 films to put them on your media server ...
    • A reasonable external storage space, half or better 1 Tb just for the same reason, films and music
    • 90% of the users I know  expect that their media server is permanently downloading torrents, also when they are watching videos.
    • There is a good percentage of people that like media servers because gives the possibility to access different sources from different PCs.

     

    And more. Despite that there is a specific distribution for the Raspberry PI to make a good quality media server. With all the hardware imposed limitis.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eugenenine
    0 eugenenine over 10 years ago in reply to balearicdynamics

    Notice though I said the 2 works well.  Also Owncloud is going to take a little more power than just a file share because Owncloud is using a web server, SSL, database, etc.  It didn't run any better on an old laptop.  The RP 2 has been my Owncloud server since it early this year.  I sync all our services, our calendar, contacts, etc.  On our vacation our phones together uploaded several g of pictures and videos then my tablet downloaded them so we could review at the hotel room later.  So i've given it quite a work out.

    Also I still use the original Pi as the internal server, sharing files, music,video, etc that I don't have in ouwcloud.  It does the job without issues.  $50 investment in a pi, case, power supply isn't too much to try it.  I used the drive that wasnin the laptop with a cheap USB adapter since the data was already there.  I've seen people waste $500 on a Mac mini and have nothing more than my $50 server.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to eugenenine

    Eugene, here we are speaking of things that works, not things that cost! So exclude any Mac mini, mac tv and so on. Who buy a Mac has not idea that an entire world exists outside there image

     

    Then about your details and price vs performances it is correct. I remain of the idea that to make a server, including all it's the worth to use something more performing than a PI, while a small media server with acceptable (and accepted) network speed of 10/100 is perfect, in particular when the cost is a strategical aspect.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eugenenine
    0 eugenenine over 10 years ago in reply to balearicdynamics

    Thats why I've said I've seen people waste the $ when a Pi will do.

     

    Unless your really moving a lot of data around your home network then a Pi will do fine.  Wifi to your laptop will max out first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to balearicdynamics

    Just read some of the posts on the thread, but lots of good points - a RPI 2 performs functions of a server through the advantages of it running Linux.

    If price is not the most critical factor then many GigEth boards would be a good choice - especially if needs are expected to change.

    The Gizmo2 is pretty slick. I've not used it as a home server. But I did use it for GigEth, and got nice performance out of it (used it for uncompressed HD cam stream).

     

    I purchased some lowish-end Synology NAS boxes for home use in 2010, and they have been running near-non-stop for five years, so they are cost-effective. Permanently doing disk writes. Serving up files daily. They've only been down when the electricity fails (we need an open source UPS project here on Element14!). Never needed images to be rebuilt due to corruption. The only maintenance I will do is replace the spinning disks soon to pre-empt any failures (none so far) as they come to the end of their lives. I can't see a need to replace the NAS boxes themselves, they still run the latest OS and have GigEth, and run cool and extremely quiet. Very well-built too.

     

    Five year operational life so far basically, and still future-proof for the immediate years to come. Incredible value for money.