Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Server - Other Alternatives.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 42 replies
  • Answers 2 answers
  • Subscribers 713 subscribers
  • Views 6766 views
  • Users 0 members are here
  • raspberry
  • intel
  • helpme
  • servers
  • single_board_computer
  • single_board_computers
  • raspberrypi
  • server
  • arduino
Related

Raspberry Pi Server - Other Alternatives.

e14 Contributor
e14 Contributor over 10 years ago

Hi All,

 

I was just wondering if there are any other single board computers like the Raspberry Pi which would allow me to create a Storage/Cloud server by connecting a external hard drive. I am kind of new to this and would like to work with simple boards to help get me started. Has anyone has come across tutorials that would help me or done a similiar sort of project and if this is actaully do able.

 

I was thinking of using the Intel Galileo Gen 2 or the Arduino Uno

 

Any feedback and recommendations would be greatly appreciated.

 

Many Thanks in Advance.

 

Omar.

  • Sign in to reply
  • Cancel
Parents
  • ipv1
    0 ipv1 over 10 years ago

    HI Omar,

    Here is my take on the whole thing.

     

    If you need a solution for connecting a storage to the network and nothing more, I would suggest you get a NAS system which will save you stress medicine later image Those things are cheap and they are usually solid and no mater how much you may want to use that old PC for a NAS box, I think the power consumption on the readymade solution and the ergonomics are MUCH better.

     

    IF you feel you want something to tinker with, then you may move towards the likes of Rapsberry Pi, RPi2, Intel Galileo Or even a CubieTruck.

    The cubie truck has SATA interfaces to connect hard drives and can run linux and android as well.

     

    I am personally using an Intel Galileo for a home automation system running OpenHAB as a primary sink. All logs and swap file are disabled to prolong memcard life and data persistance is accomplished using google drive image

     

    I am using an old windows machine for a NAS system right now because it also functions as a test bed for some windows xp experiments hence the extra space is justified.

     

    If you are just interested in having an Android based system then my suggestion would be to buy the UTRA CHEAP tablets(I have a Datawind 7inch for less than 50 dollars) and root it. enable USB thumb drive support and run your android sharing apps from there.

     

    Hope this helps image

     

    Cheers,

    IP

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ipv1
    0 ipv1 over 10 years ago

    HI Omar,

    Here is my take on the whole thing.

     

    If you need a solution for connecting a storage to the network and nothing more, I would suggest you get a NAS system which will save you stress medicine later image Those things are cheap and they are usually solid and no mater how much you may want to use that old PC for a NAS box, I think the power consumption on the readymade solution and the ergonomics are MUCH better.

     

    IF you feel you want something to tinker with, then you may move towards the likes of Rapsberry Pi, RPi2, Intel Galileo Or even a CubieTruck.

    The cubie truck has SATA interfaces to connect hard drives and can run linux and android as well.

     

    I am personally using an Intel Galileo for a home automation system running OpenHAB as a primary sink. All logs and swap file are disabled to prolong memcard life and data persistance is accomplished using google drive image

     

    I am using an old windows machine for a NAS system right now because it also functions as a test bed for some windows xp experiments hence the extra space is justified.

     

    If you are just interested in having an Android based system then my suggestion would be to buy the UTRA CHEAP tablets(I have a Datawind 7inch for less than 50 dollars) and root it. enable USB thumb drive support and run your android sharing apps from there.

     

    Hope this helps image

     

    Cheers,

    IP

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Problemchild
    0 Problemchild over 10 years ago in reply to ipv1

    Sounds sensible Inderpreet!