Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Microstack GPS and Accelerometer on RaspberryPi 2 and Ubuntu Mate
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 705 subscribers
  • Views 2171 views
  • Users 0 members are here
  • Ubuntu
  • 2
  • rasberrypi
  • raspberry_pi
  • mate
  • microstack
Related

Microstack GPS and Accelerometer on RaspberryPi 2 and Ubuntu Mate

doubletop
doubletop over 10 years ago

I'm going round in circles trying to get this to work with Ubuntu Mate and its not clear which posts on any website are relevant and which are not.

 

Here's where I've got to.

 

$ sudo apt-get install python3-microstacknode

 

Doesn't work

 

sudo apt-get install python3-pip

 

works

 

sudo pip-3.2 install microstackcommon microstacknode

 

works if pip-3.2 is changed to pip. However it puts all the files into /usr/local/lib rather than /usr/lib and there are no example files. microstackcommon and microstacknode files have been moved to /usr/lib/ in the existing file structure for python 2.7 python3,4 and python3,5. I got the examples from GitHUb and placed them in a local folder.

 

As there is no Rasp-config available config.txt has been edited to add

 

sudo nano /boot/config.txt

 

and

 

dtparam=i2c_arm=on

dtparam=spi=on

 

sudo i2cdetect -y 1

 

works. However, no device is found

 

0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:      -- -- -- -- -- -- -- -- -- -- -- -- --

10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

70: -- -- -- -- -- -- -- --

 

Running the examples accelcat.py

 

Traceback (most recent call last):

  File "/home/pete/PythonTest/accelcat.py", line 11, in <module>

    with MMA8452Q() as accelerometer:

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 126, in __enter__

    self.init()

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 131, in init

    self.standby()

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 153, in standby

    self.ctrl_reg1.set(self._ctrl_reg1_value)

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 279, in set

    writing_bytes(self.device_address, self.register_address, v))

  File "/usr/lib/python3.4/dist-packages/microstackcommon/i2c.py", line 85, in transaction

    ioctl(self.fd, I2C_RDWR, ioctl_arg)

OSError: [Errno 5] Input/output error

 

and gpscat.py

 

Traceback (most recent call last):

  File "/home/pete/PythonTest/gpscat.py", line 3, in <module>

    import microstacknode.gps.l80gps

ImportError: No module named 'microstacknode.gps'

 

 

So clearly something is missing  from the pip install so rather than editing and juggling around files please where or how do I find the 'proper' install package that gets everything i need to make this work with Ubuntu Mate?

 

Pete

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 10 years ago

    Even though it looks as if the software installation might have been wrong or incomplete....

     

    you have clear indication that
    * You succeeded in enabling I2C: i2cdetect works!

    * Your PI does NOT have a connection to the I2C devices: I2cdetect does NOT report any devices.

     

    So: Check your hardware! (Both i2cdetect and python are trying to tell you: no i2c device found at that address).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • doubletop
    0 doubletop over 10 years ago in reply to rew

    Roger

     

    Thanks for taking the time to reply.

     

    I'd hope the hardware was fine Its a brand new RasPi 2, Microstack baseboard, accelerometer and GPS received form Element14 in the past week. The Ubuntu Mate was downloaded in the past week, installed on a new 32Gb class10 SDHC card and updates applied

     

    I'm keen to get a clean build that works properly and not subject to hacks and tweaks to make it work. Once I’ve got it going I plan to blow it all away and do a clean build

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to doubletop

    I haven't investigated what hardware you have. But the part "raspberry pi" I know what it is and it seems to be functioning. The other stuff seems to be "not connected to the pi" when viewed from the pi. If what you have is a simple board that plugs on the 'pi, make sure that it's correctly positioned and configured. Double check that your device is supposed to be on I2C. (I've had one of my clients complain that i2c-detect didn't see any devices, while he had an SPI device....). If you need wires to connect it check the wires. Or.... Post a picture.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to doubletop

    doubletop 

    Have you seen this http://www.microstack.org.uk/assets/gps/FormattedGPSgettingstarted.pdf?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to doubletop

    doubletop 

    Have you seen this http://www.microstack.org.uk/assets/gps/FormattedGPSgettingstarted.pdf?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • mconners
    0 mconners over 10 years ago in reply to clem57

    Reading that clem57 that looks like it should be communicating via the serial port and not I2C at all.

    But, I am not familiar with the setup he has.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to mconners

    Oh, I guess that  doc is only for the GPS. The accelerometer may very well use I2C.

     

    One issue to check is to make sure you have a power supply capable of running both the RaspberryPi and the microstack add on module and boards.

     

    You don't mention what type and rating of the power supply you are using.

     

    Mike