Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Inputs and Outputs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 822 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Inputs and Outputs

e14 Contributor
e14 Contributor over 10 years ago

I'm trying to use the Cirrus Logic Audio Card and RPi2 in a Software Defined Radio application.  Specifically the Softrock RXTX Ensemble:  WB5RVZ - Home Page

 

I was hoping I could use this card to do both RX and TX, but it's not clear how I can present the various inputs and outputs to the SDR software.  I'm working with Quisk right now (apt-get install quisk).

 

Normally I would present an audio device as hw:0 and hw:1 and so on.  This card only has hw:sndrpiwsp and I have to use the various scripts to activate inputs/outputs.

 

I only need to record and playback from one input and output at a time, but the trick is helping the software to switch between inputs and outputs when I push the transmit button.  Right now taking the Record_from_lineIn audio processing that in Quisk and then having the output from Quisk go to the headphone jack works like a champ.  I have to manually run the scripts and change to Record_from_DMIC and Playback_to_Lineout.sh which is rather clumsy.

 

So anyone know if I can use something more specific than a generic hw:sndrpiwsp device?

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    build python script like this pseudocode:

    loop forever until keyboard interrupt.

    test transmit button

       run transmit script for x time.

    else

       run receive script for x time.

    loop repeat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Quisk is actually python code so I suppose I could have it set the sound card i/o on the fly.  But that is no solution for other tools.  I need to switch inputs and outputs within a few milliseconds or it won't be practical.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    You need to assign higher priority to task/process running on Pi to make that happen under Linux!image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gonesurfing
    0 gonesurfing over 10 years ago

    Late reply, but I'm using Quisk with a softrock RXTX ensemble also. However I'm sending the IQ audio over the network with pulseaudio.  Pulseaudio is playing nicely with the Wolfson card for both line in and line out.

     

    I'm using usbsoftrock to key the radio. Here's some info under my old call sign.

     

    https://km4dsj.wordpress.com/