Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Inputs and Outputs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 824 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Inputs and Outputs

e14 Contributor
e14 Contributor over 10 years ago

I'm trying to use the Cirrus Logic Audio Card and RPi2 in a Software Defined Radio application.  Specifically the Softrock RXTX Ensemble:  WB5RVZ - Home Page

 

I was hoping I could use this card to do both RX and TX, but it's not clear how I can present the various inputs and outputs to the SDR software.  I'm working with Quisk right now (apt-get install quisk).

 

Normally I would present an audio device as hw:0 and hw:1 and so on.  This card only has hw:sndrpiwsp and I have to use the various scripts to activate inputs/outputs.

 

I only need to record and playback from one input and output at a time, but the trick is helping the software to switch between inputs and outputs when I push the transmit button.  Right now taking the Record_from_lineIn audio processing that in Quisk and then having the output from Quisk go to the headphone jack works like a champ.  I have to manually run the scripts and change to Record_from_DMIC and Playback_to_Lineout.sh which is rather clumsy.

 

So anyone know if I can use something more specific than a generic hw:sndrpiwsp device?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    build python script like this pseudocode:

    loop forever until keyboard interrupt.

    test transmit button

       run transmit script for x time.

    else

       run receive script for x time.

    loop repeat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Quisk is actually python code so I suppose I could have it set the sound card i/o on the fly.  But that is no solution for other tools.  I need to switch inputs and outputs within a few milliseconds or it won't be practical.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    You need to assign higher priority to task/process running on Pi to make that happen under Linux!image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    You need to assign higher priority to task/process running on Pi to make that happen under Linux!image

    Clem