Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cannot add Multimedia Widgets to Qt Creator C++ project for Raspberry Pi 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 3611 views
  • Users 0 members are here
  • raspberrypi.
  • qt5
  • raspberry_pi
  • c++
  • video player
Related

Cannot add Multimedia Widgets to Qt Creator C++ project for Raspberry Pi 2

e14 Contributor
e14 Contributor over 10 years ago

I am trying to compile and run the official Media Player Example in Qt: http://doc.qt.io/qt-5/qtmultimediawidgets-player-example.html for a Raspberry Pi running Raspbian Jessie. I still have no success: when I build the project, the following error appears.

:-1: error: Unknown module(s) in QT: multimedia multimediawidgets.

This is referred to the .pro code:

QT += network \
  xml \
  multimedia \
  multimediawidgets \
  widgets

 

I installed "sudo apt-get install qtmultimedia5-dev" but without success. Is it the right module to install?

My Qt should be up to date, and I don't know where the problem can be. Could anyone help please? Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The QtMultimedia module now resides in the QtMobility package. So you need to install QtMobility, which provides QtMultimediaKit :


    I have  tested and installed 5 seconds ago to check answer so it works on 12.04 It should be upwardly compatible fingers crossed  although even thats a misnomer these days  but there  you go

    This is how its  done see below

    sudo apt
    -get install qtmobility-dev

     

    When compiling, you must add the following flags :

     

    -I/usr/include/QtMultimediaKit -I/usr/include/QtMobility
    -lQtMultimediaKit

     

    It pays to do a quick search using Google Normally you will find some sensible people who will provide the correct answers 

     

    (How ever There are very few worth mentioning too these days   which is the norm )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    When compiling, you must add the following flags :

    -I/usr/include/QtMultimediaKit -I/usr/include/QtMobility
    -lQtMultimediaKit

    Ok, I added the flag in my Compilers environment in Qt, but the problem still remains. Since I cross-compile for Raspberry Pi, perhaps have I to "cross-compile" QtMultimedia for my RPi as well? How can I check if it is already done and how to do it in the case it is not? Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    When compiling, you must add the following flags :

    -I/usr/include/QtMultimediaKit -I/usr/include/QtMobility
    -lQtMultimediaKit

    Ok, I added the flag in my Compilers environment in Qt, but the problem still remains. Since I cross-compile for Raspberry Pi, perhaps have I to "cross-compile" QtMultimedia for my RPi as well? How can I check if it is already done and how to do it in the case it is not? Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    sudo apt-get install qtmobility-dev

    will load Pi version of code if the package exists.