Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum pi zero - which headers ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 872 views
  • Users 0 members are here
  • hats
  • headers
  • raspberry pi zero
  • robot
  • raspberry_pi_getting_started
Related

pi zero - which headers ?

perigalacticon
perigalacticon over 10 years ago

I have a new Pi zero, and I am new to the Pi world, this is my first Pi, and I have from some experience with Arduino.

 

What would you recommend for the header installation?  I noticed to use hats you want to use a male header pointing up from the Zero.  I was considering using female headers pointing up to use with breadboard jumper pins, and then use male-male header pins to adapt for when using a hat.  Would this arrangement work for hats?  I don't want to solder in the wrong one because switching seems it would be impossible.  What is the consensus for header type and orientation for the zero?  I hope to use the Zero for robot development.

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    perigalacticon

         Glad you score one since they are selling like hotcake's.  So before you solder away, what hat are you thinking of? Most hats will cover the old Pi's the size of a credit card. Do you want to do that with a smaller board? But if you still want this see https://learn.adafruit.com/introducing-the-raspberry-pi-zero/gpio-header-options .

    Clem

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • perigalacticon
    0 perigalacticon over 10 years ago in reply to clem57

    Oops!  The Adafruit GPIO cobbler cable doesn't fit in the zebra case image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • perigalacticon
    0 perigalacticon over 10 years ago in reply to clem57

    Oops!  The Adafruit GPIO cobbler cable doesn't fit in the zebra case image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • uscdadnyc
    0 uscdadnyc over 9 years ago in reply to perigalacticon

    I have: (a) RaspPi 1 B (w/26pin GPIO), (b) RaspPi 3 B (w/40pin GPIO) (c) RaspPI Zero (w/40pin GPIO). What I found useful is a PiFace Pi Rack, to interface "other" Cards. ALBEIT thru 26pin GPIO. But if you carefully "shave" (w/ a File) a 26pin Ribbon Cable you can get it to fit onto the 40pin GPIO.

    The PiFace Rack allows (1) Independent Power Supply for (interfaced) cards (2) can :"stack" Three Cards; and w/option (1) just power whatever card you are working with, (3) has jumpers for Daisy-chaining(?) of GPIO Pins 24 & 26. For what reason I have not figured out yet.

    Of course 40pins is better than 26pins, BUT I still have 40pins on my RaspPi 3B and Zero. Being only 26pins the Piface Rack might be MD'ed (Manufacturer Discontinued), so I say  buy one if you can, despite the fact that it is only 26pins. BTW it is thru the Piface Rack that I interface w/ my Gertduino which has only 26pins GPIO.

    USCDADNYC (NY NY USA)