Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Change capacitice touch screen sensitivity [Official display for Raspberry Pi]
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 706 subscribers
  • Views 1898 views
  • Users 0 members are here
  • driver
  • raspberry
  • touch
  • raspberry_pi_space
  • display
  • touchscreen
Related

Change capacitice touch screen sensitivity [Official display for Raspberry Pi]

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I would like to know if it is possible to change or modify the sensitivity of the capacitive touch screen for my Raspberry Pi.

My display is the Official 7" Raspberry touch display, and my OS is the latest Raspbian Jessie.

I need more sensitivity because in my application I have an additional glass lens above the display, so that the actual built-in drivers does not work well.

I guess one have to do little changes to the driver for the capacitive touch, but how and where? Does anybody has any idea?

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    Sorry no. But you can use a skin oil to improve the capacitance. I have a friend with dry cracked skin that does this. Warning the screen will get messy over time. But small price to get the screen to work if you need.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Clem Martins ha scritto:

     

    Sorry no. But you can use a skin oil to improve the capacitance. I have a friend with dry cracked skin that does this. Warning the screen will get messy over time. But small price to get the screen to work if you need.

    Clem

    Thanks! With your "Sorry no" you mean it is not possible at all or you don't know if it is possible or not?

    I think the oil solution wouldn't be suitable for my case image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    What is the details in your case if you do not mind?

    doug laser

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    I want to place the display inside a proper stainless steel vertical control panel. I would like to place a 3mm thick glass over it for increase protection from damages (the panel will be used by various people and the original 1 mm thick glass lens is too thin in my opinion).

    After a few attempts I saw that with the additional glass the touch screen doesn't work at all (the distance between the hand and the display is too much). This is the reason for which I wonder if there would be some chances to increase ore calibrate the touch response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Oh. The glass thickness can prevent finger capacitance. The field is electrically controlled and not a software parameter as explained in linked article. You may want to explore other types of touch screens. See  https://en.wikipedia.org/wiki/Capacitive_sensing explains types and suggest ares to explore. Bottom line is more glass is not a viable alternative for you.

    Clem