Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Zero Ethernet Problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 32 replies
  • Answers 5 answers
  • Subscribers 709 subscribers
  • Views 7639 views
  • Users 0 members are here
  • ethernet
  • raspberry pi
Related

Raspberry Pi Zero Ethernet Problem

e14 Contributor
e14 Contributor over 10 years ago

I'm having trouble connecting my Raspberry Pi zero to ethernet.

 

I have a Raspberry Pi 3 and four Raspberry Pi zeros. I'm a grad student in mathematics and I do a whole lot of parallel computing. I'm trying to set these up as a cluster to test my distributed code before I send it up to the university's very expensive computing cluster. I bought a handful of uxcell ethernet to micro USB adapters that you can find here: Amazon.com: uxcell Micro USB to RJ45 Network Card Adapter Converter for Windows 98SE Me: Computers & Accessories

 

When I plug ethernet into the Pi zero using this cable, the Pi zero is not being assigned an IP address. Is this adapter incorrect? I was hoping to use these cheap adapters as the grad student stipend isn't exactly CEO pay image.  As an additional note, plugging the ethernet directly into the Pi 3 works fine. The Pi 3 instantly recognizes the ethernet and has no problem connecting to the network.

 

I have tried using ip link and dhcpcd to get the network going on the Pi Zeros, but i'm stuck as I can't get them to recognize the LAN. I'm also positive that it isn't an issue with the router as I have used multiple routers (at home and at the university) and neither has worked. Thank you in advance for your replies.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Just a quick check is the otg  plugged to a powered hub with enough current? Mine was not because I needed more than 100 mA which was not provided as my picture setup showed.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Actually I am having a lot of trouble with my USB hub, and I'll be purchasing another one. However when I plug the ethernet into one of the Pi zero's ports and the power into the other, it still doesn't show up on the network. To be clear I plugged the ethernet straight from my router to the Pi zero and used the other port to power on the zero. With this setup I probed the network from my laptop and found no IP for the Raspberry Pi.

     

    That being said I wrote a little shell script to sleep 2m, then run the commands that you suggested I post the output of. Since I'm having trouble with the USB hub, I photographed the output of the three commands you suggested I try. They are as follows:

     

    imageimageimage

     

    A little unorthodox, I know, but it's the best I can think to do without the functional USB hub. Hopefully I'll have that new hub tomorrow or Monday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Problemchild

    Yes the reason that I'm doing things this way is because I already had the raspberry Pi's laying around, and have gotten into a little trouble "wasting resources" on the university cluster with trying to test my distributed code. All I had to purchase that I didn't already own for this were the Ethernet to Micro USB connectors. This project won't be doing any real "hefty" computation, I'm just hoping to test code on it so I no longer upset the people who run my university's cluster.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Problemchild

    Using your suggestions I was able to ssh into the Pi zero's. However, now that I'm able to ssh into them, I decided to try using my ethernet switch that has been laying around in my box of toys to get them all on the network. For some reason they are all being assigned the same IP address. I tried editing the /etc/network/interfaces file to manually assign different static IP addresses, but they are still all being assigned the IP address defined in /etc/network/interfaces of whichever Pi I boot first. When I'm ssh'ed into a Pi, after a few seconds I get an error message saying "Broken Pipe." I have to remove the IP address from my list of known hosts, and then I can ssh into a Pi zero again, but when I go back in it is often a different Pi zero. It seems that they are fighting for the IP address, even though they are different machines being connected from separate ports of the ethernet switch at the same time.

     

    For reference this is what I put in the /etc/network/interfaces file

     

    iface eth0 inet static

         address 10.0.0.XX

         netmask 255.255.255.0

         network 10.0.0.0

         broadcast 10.0.0.255

         gateway 10.0.0.1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    The Ethernet port is at the lower level(physical) and has not relation to IP address(at the TC/IP layer). See https://en.wikibooks.org/wiki/A-level_Computing/AQA/Computer_Components,_The_Stored_Program_Concept_and_the_Internet/Str…  &  https://en.wikipedia.org/wiki/OSI_model to understand.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    This doesn't make sense unfortunately.

    Get a single one working. No point experimenting with all 4 while you still have issues with a single one.

    Once you're at the stage that you can successfully use a single Pi plugged into your switch, then work on the second one.

     

    By "successfully use a single Pi" I mean you need to confirm that you can SSH into your Pi using your chosen IP address, see no unexpected behaviour like the broken pipe and see no issues with power supply fails/unintended reboots etc.

    Once all that works, add a second Pi, and take typical prudent engineering steps like using a separate power supply, confirming both function before adding a third, etc. After it all works, you can optimise to reduce supplies, etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    I should have been more specific in my last post. That is exactly what I'm doing. With any single pi plugged in I can successfully ssh into the Pi and stay logged in as long as I please. There are no reboots, and no "Broken Pipe" error messages. When I plug in a second Pi with a separate power source, it gets assigned the same IP address as the Pi that was already active and I had already been ssh'ed into. When the second Pi gets plugged in and assigned the same IP address as the first Pi, I get kicked out of ssh with the "Broken Pipe" error message, and when I attempt to ssh back in I get this message:

     

    @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@

    @    WARNING: REMOTE HOST IDENTIFICATION HAS CHANGED!     @

    @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@

    IT IS POSSIBLE THAT SOMEONE IS DOING SOMETHING NASTY!

    Someone could be eavesdropping on you right now (man-in-the-middle attack)!

    It is also possible that a host key has just been changed.

    The fingerprint for the ECDSA key sent by the remote host is

    SHA256:Zl9WWVSRwUpIGG0k+y7I6nMUTL7/DUviVuYdiW3kGy0.

    Please contact your system administrator.

    Add correct host key in /home/william/.ssh/known_hosts to get rid of this message.

    Offending ECDSA key in /home/william/.ssh/known_hosts:9

      remove with:

      ssh-keygen -f "/home/william/.ssh/known_hosts" -R 10.0.0.31

    ECDSA host key for 10.0.0.31 has changed and you have requested strict checking.

    Host key verification failed.

     

     

    After seeing this error message I remove 10.0.0.31 from my known hosts and try to ssh to the same IP. After deleting this from the known hosts and using the same IP for ssh, I can successfully access a Pi again but it's the second Pi that was plugged in. With both of them connected, I can't stay logged into either Pi very long, before I get kicked out by the "Broken Pipe" error message. Every time I get the broken pipe message I see the same "REMOTE HOST IDENTIFICATION HAS CHANGED" error message, and it alternates which Pi I can access by using "ssh pi@10.0.0.31"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Are you assigning a different ip address for each of the Pi's? If you clone them, then you must change each one before a reboot.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    Do you have a router connected? If so, unplug it, just to eliminate the possibility that DHCP is in (incorrect) operation.

    Just use the switch for now.

     

    Also, there is no way for a Linux box to look inside another Linux box to examine the IP addressing configuration and then self-configure with that configuration. No code or protocol exists to do that as far as I'm aware.

    Can you paste or attach the entire content of your /etc/network/interfaces file, for the first Pi, and for the second Pi? I get that just the IP address will be different, but it will be good to see it in detail.

     

    Also, a quick photo showing the router, Pi's etc would be great too. I can't see how it will help just yet, but I'm clutching at straws since your problem is bizarre.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    By the way, out of curiosity, please can you paste the output of:

    ifconfig -a 

     

    For the Pi before and after you plug the second one in, and when then second pi takes over as you say.

     

    Something like:

     

    Step 1. Only Pi A connected

     

    Step 2. Plug in Pi B

     

    Step 3. wait until broken pipe and then delete from known_hosts and then reconnect

     

    Step 4.  unplug pi A

     

     

    After each step, record the following:

    ssh pi@ip_address_A

    cat /etc/hostname    (so we can see exactly which Pi you're connected to)

    ifconfig -a

     

    ssh pi@ip_address_B

    cat /etc/hostname

    ifconfig -a

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Just so you know, for some reason the Pi that I'm trying to set to IP address 10.0.0.30 is for some reason getting assigned 10.0.0.31. Also I have an arris 2 in 1 modem/router, so there's no way to take my router out of the equation. But yes Clem I do have a router being used. That being said, here's all the output that you requested:

     

    The contents of /etc/network/interfaces on Pi number 1 (ssh pi@10.0.0.31 with cat /etc/hostname showing pizero1):

     

    # interfaces(5) file used by ifup(8) and ifdown(8)

     

     

    # Please note that this file is written to be used with dhcpcd

    # For static IP, consult /etc/dhcpcd.conf and 'man dhcpcd.conf'

     

     

    # Include files from /etc/network/interfaces.d:

    source-directory /etc/network/interfaces.d

     

     

    auto lo

    iface lo inet loopback

     

     

    iface eth0 inet static

      address 10.0.0.30

      netmask 255.255.255.0

      network 10.0.0.0

      broadcast 10.0.0.255

      gateway 10.0.0.1

     

     

    allow-hotplug wlan0

    iface wlan0 inet manual

        wpa-conf /etc/wpa_supplicant/wpa_supplicant.conf

     

     

    allow-hotplug wlan1

    iface wlan1 inet manual

        wpa-conf /etc/wpa_supplicant/wpa_supplicant.conf

     

    The contents of /etc/network/interfaces on Pi number 2 (ssh pi@10.0.0.31 with cat /etc/hostname showing raspberrypi):

     

    # interfaces(5) file used by ifup(8) and ifdown(8)

     

     

    # Please note that this file is written to be used with dhcpcd

    # For static IP, consult /etc/dhcpcd.conf and 'man dhcpcd.conf'

     

     

    # Include files from /etc/network/interfaces.d:

    source-directory /etc/network/interfaces.d

     

     

    auto lo

    iface lo inet loopback

     

     

    iface eth0 inet static

            address 10.0.0.31

            netmask 255.255.255.0

            network 10.0.0.0

            broadcast 10.0.0.255

            gateway 10.0.0.1

     

     

    allow-hotplug wlan0

    iface wlan0 inet manual

        wpa-conf /etc/wpa_supplicant/wpa_supplicant.conf

     

     

    allow-hotplug wlan1

    iface wlan1 inet manual

        wpa-conf /etc/wpa_supplicant/wpa_supplicant.conf

     

    The results of ifconfig -a with only Pi number 1 plugged in (ssh pi@10.0.0.31 with cat /etc/hostname showing pizero1):

     

    eth0      Link encap:Ethernet  HWaddr 00:e0:4c:53:44:58

              inet addr:10.0.0.31  Bcast:10.0.0.255  Mask:255.255.255.0

              inet6 addr: fe80::26a5:b629:f948:92c3/64 Scope:Link

              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

              RX packets:204 errors:1 dropped:1 overruns:1 frame:2

              TX packets:164 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:1000

              RX bytes:19673 (19.2 KiB)  TX bytes:23792 (23.2 KiB)

     

     

    lo        Link encap:Local Loopback

              inet addr:127.0.0.1  Mask:255.0.0.0

              inet6 addr: ::1/128 Scope:Host

              UP LOOPBACK RUNNING  MTU:65536  Metric:1

              RX packets:200 errors:0 dropped:0 overruns:0 frame:0

              TX packets:200 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:0

              RX bytes:16656 (16.2 KiB)  TX bytes:16656 (16.2 KiB)

     

    The output of ifconfig -a on Pi number 1 after plugging in Pi number 2 (ssh pi@10.0.0.31 with cat /etc/hostname showing pizero1):

     

    eth0      Link encap:Ethernet  HWaddr 00:e0:4c:53:44:58

              inet addr:10.0.0.31  Bcast:10.0.0.255  Mask:255.255.255.0

              inet6 addr: fe80::26a5:b629:f948:92c3/64 Scope:Link

              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

              RX packets:1134 errors:1 dropped:3 overruns:1 frame:2

              TX packets:329 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:1000

              RX bytes:96791 (94.5 KiB)  TX bytes:42976 (41.9 KiB)

     

     

    lo        Link encap:Local Loopback

              inet addr:127.0.0.1  Mask:255.0.0.0

              inet6 addr: ::1/128 Scope:Host

              UP LOOPBACK RUNNING  MTU:65536  Metric:1

              RX packets:200 errors:0 dropped:0 overruns:0 frame:0

              TX packets:200 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:0

              RX bytes:16656 (16.2 KiB)  TX bytes:16656 (16.2 KiB)

     

    The output of ifconfig -a on Pi number 2 after "taking over" with Pi number 1 still plugged in (ssh pi@10.0.0.31 with cat /etc/hostname showing raspberrypi):

     

    eth0      Link encap:Ethernet  HWaddr 00:e0:4c:53:44:58

              inet addr:10.0.0.31  Bcast:10.0.0.255  Mask:255.255.255.0

              inet6 addr: fe80::26a5:b629:f948:92c3/64 Scope:Link

              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

              RX packets:3566 errors:0 dropped:0 overruns:0 frame:0

              TX packets:767 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:1000

              RX bytes:239048 (233.4 KiB)  TX bytes:101124 (98.7 KiB)

     

     

    lo        Link encap:Local Loopback

              inet addr:127.0.0.1  Mask:255.0.0.0

              inet6 addr: ::1/128 Scope:Host

              UP LOOPBACK RUNNING  MTU:65536  Metric:1

              RX packets:200 errors:0 dropped:0 overruns:0 frame:0

              TX packets:200 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:0

              RX bytes:16656 (16.2 KiB)  TX bytes:16656 (16.2 KiB)

     

    The output of ifconfig -a on Pi number 2 after unplugging Pi number 1 (ssh pi@10.0.0.31 with cat /etc/hostname showing rasperrypi):

     

    eth0      Link encap:Ethernet  HWaddr 00:e0:4c:53:44:58

              inet addr:10.0.0.31  Bcast:10.0.0.255  Mask:255.255.255.0

              inet6 addr: fe80::26a5:b629:f948:92c3/64 Scope:Link

              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

              RX packets:3618 errors:0 dropped:0 overruns:0 frame:0

              TX packets:793 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:1000

              RX bytes:243745 (238.0 KiB)  TX bytes:105906 (103.4 KiB)

     

     

    lo        Link encap:Local Loopback

              inet addr:127.0.0.1  Mask:255.0.0.0

              inet6 addr: ::1/128 Scope:Host

              UP LOOPBACK RUNNING  MTU:65536  Metric:1

              RX packets:200 errors:0 dropped:0 overruns:0 frame:0

              TX packets:200 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:0

              RX bytes:16656 (16.2 KiB)  TX bytes:16656 (16.2 KiB)

     

    A picture of my setup:

     

    image

     

    Where the source of the blue ethernet cable to the ethernet switch is coming straight from the back of the modem/router unit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Oh my gosh, I see the problem: they all have the same mac address 00:e0:4c:53:44:58 from Amazon.com: uxcell Micro USB to RJ45 Network Card

    Which means the Chinese did not care to imprint unique ones for each adapter. I hope you can complain to where you got these.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Oh my gosh, I see the problem: they all have the same mac address 00:e0:4c:53:44:58 from Amazon.com: uxcell Micro USB to RJ45 Network Card

    Which means the Chinese did not care to imprint unique ones for each adapter. I hope you can complain to where you got these.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • bwelsby
    0 bwelsby over 10 years ago in reply to clem57

    You saw it too image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Wow you're right. I'll see what I can do about complaining to Amazon. They usually have excellent customer service.

     

    Thanks everybody for your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to clem57

    Um, yeah some rely on the fact it's unlikely that some one will have a load of these modules

    Any way before you rush off you can try setting the MAC manually which may be easier than sending the whole lot back

    Check the manuals but the command will be something like

    ifconfig eth0 hw ether <mac address>

    obviously as root

     

    set the MACs to different values and you should be OK

    Also you will need this to run each time you boot or insert the NIC

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Problemchild

    Problemchildis correct. Try to force the mac address read How to set the mac address from /etc/network/interfaces in Debian | YourITronics .

    When you load the network information the device should use the hwaddress. But be careful not to dupicate any address . I would change the last part from 01-ff range.

    Like:

    hwaddress ether 00:e0:4c:53:44:68 ### -> next one 00:e0:4c:53:44:78 etc.

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to clem57