El último modelo de RPi no tiene el enganche a Bayoneta para la SD.
Sólo funciona con SD de 16 gigas o se pueden utilizar de 8 gigas?
El último modelo de RPi no tiene el enganche a Bayoneta para la SD.
Sólo funciona con SD de 16 gigas o se pueden utilizar de 8 gigas?
First sentence makes no sense when translated.
The latest model of RPI has no hitch Bayonet for SD.
But 16GB better than 8 GB any way. See RPi Easy SD Card Setup - eLinux.org for great help.
Clem
Hi all.
Thank you for your reply.
The RPI until the version 2 had a locking system for the sd who also served as ejection system.
RPI 3 does not have this system?
Can I use the RPI with a Sd 8GB?
I tried to move the file from the SD 16GB to the 8GB one, but the system will not start.
Best regards.
Vittorio
You are correct. The PI3 has a push to insert and pull to remove SD card socket vs the earlier models that where push to insert, push to release. In my opinion the new version is better as there will be less chance to accidentally pop it out.
An 8GB SD card should work without problems but ensure it is Class 10 and as fast as you can afford. (Recommend Samsung EVO or PRO, or Sandisk ULTRA). You can also go bigger if so desired (32GB for instance). Very useful if your going to be logging data, Capturing video from camera or installing big games /
The size of the sd card needs to be big enough for the o/s you pick. I used 8GB for a fresh download of Rasbian Jessi full edition which was dated Feb 29, 2016 and the Pi 3 worked fine. Older version may not work unless properly updated with 3 commands.
Clem
Dear friends:
Thank you for your replies.
Only a question more: I have bought a original SD 16GB whit operative system for RPi 3 and with this SD RPi work.
How can I to pass this OS to a 8GB SD?
I have tried to copy the files but in this way RPi don’t start.
Thank you and best regards.
Vittorio.
I think you would be better off just starting from scratch by visiting https://www.raspberrypi.org/downloads/raspbian/ and downloading the latest image of raspian. then following this guide https://www.raspberrypi.org/documentation/installation/installing-images/README.md to install it onto the SD card.
Good Luck
You cannot copy. Two partitions must be fat for /boot and ext4 for rest..
So, how can I transport the Operative System from the original SD to the 8GB SD ?
Hola Vittorio! Eres tu el que estuvo en el INEM de Tortosa?
Un saludo!
Toni